Publications
  • Learn
  • More
Publications
Blog Controlling lightning with lasers
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 2 Apr 2012 6:21 PM Date Created
  • Views 578 views
  • Likes 1 like
  • Comments 1 comment
  • research
  • alternative_energy
  • test
  • nikola_tesla
  • tesla
  • industry
  • on_campus
  • weather
  • lightning
  • prototyping
  • university
  • energy
  • laser
  • earth
  • innovation
Related
Recommended

Controlling lightning with lasers

Catwell
Catwell
2 Apr 2012

image

Lightning strike in Paris, France (via Bertrand Kulik)

 

Possibly the greatest pioneer in the field of electrical engineering, Nikola Tesla, dreamed of one day controlling lightning. During lightning storms, he would sit and watch in amazement as nature demonstrated its powerful electrical discharges. He successfully simulated electrical discharges up to 7 meters in length using millions of volts produced by his infamous coils. However, controlling nature's powerful forces ended up being one of Tesla's unfulfilled dream.

 

 

During the 1970s, scientist first began finding ways to trigger lightning strikes. Their methods included shooting small rockets into storm clouds with spools of wire connected to the ground. This method worked only 50% of the time and was not cost-effective or efficient. Therefore, scientist began pondering new ways to trigger lightning strikes. Around this time, it was first suggested that lasers may be used to direct lightning strikes.

 

 

As laser technology advanced, the hypothosis of triggering lightning strikes started to become a reality. In 2008 André Mysyrowicz and a team of researchers from École Nationale Supérieure de

Techniques Avancées (ENSTA ParisTech) conducted experiments with promising results. The team used laser pulses to create beams of plasma filaments (ionized air molecules) that could possibly conduct electricity. Though they had the correct idea, the beams were too short to trigger lightning strikes to the ground despite generating electrical discharges within the clouds themselves.

 

 

Recently, the same team has conducted "breakthrough experiments." Using more powerful lasers and high-voltage discharges to simulate lightning, they are able to direct the discharge using a filament path. Additionally, directing a laser beam 5 to 20 centimeters from two oppositely charged electrodes over 50 meters, the team successfully intercepted the lightning and kept it from  jumping between the electrodes. Controlling the lightning without it touching electrodes demonstrates a more real-life situation (IE: no electronics are in natural strikes).

 

 

Lightning can be a powerful tool to understanding mechanisms underlying the natural phenomena. Triggered lightning strikes could help engineers perform sensitivity tests on air-planes and infrastructures such as power lines. Mastery over the planet is inevitable.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    Hi Cabe,

     

    I am not sure I would associate the term "infamous" to the Tesla coil.  Tesla's work is still far beyond most of us and we have not seen his equal in electromagnetic impelentations since his death.

     

    Lightning can also be a power source if we can use Lasers to lure the individual bolts onto a system where the electrical energy can be captured and converted into useful levels.

    I know that they had good success with electron beam lasers, so it would be interesting to see what lasers they are using in this case.

     

    The potential of lighting use is why I continue my research into its behavior in the open sky.  There is a lot of interesting physics going on during a lightning strike.

     

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    Hi Cabe,

     

    I am not sure I would associate the term "infamous" to the Tesla coil.  Tesla's work is still far beyond most of us and we have not seen his equal in electromagnetic impelentations since his death.

     

    Lightning can also be a power source if we can use Lasers to lure the individual bolts onto a system where the electrical energy can be captured and converted into useful levels.

    I know that they had good success with electron beam lasers, so it would be interesting to see what lasers they are using in this case.

     

    The potential of lighting use is why I continue my research into its behavior in the open sky.  There is a lot of interesting physics going on during a lightning strike.

     

    Thanks

    DAB