Publications
  • Learn
  • More
Publications
Blog Engineers design robotic tank to bring Wi-Fi to hazardous areas
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 10 Aug 2012 6:01 PM Date Created
  • Views 626 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • test
  • wifi
  • transportation
  • military
  • industry
  • hmi
  • robotics
  • robot
  • hazard
  • on_campus
  • Design
  • cabeatwell
  • prototyping
  • wireless
  • university
  • search_and_rescue
  • innovation
  • communication
Related
Recommended

Engineers design robotic tank to bring Wi-Fi to hazardous areas

Catwell
Catwell
10 Aug 2012

image

Node.js WiFi-Extending Robot (via Notheastern University)

 

Electrical and computer engineers from Northeastern University have collaborated on a robotic vehicle that’s designed to bring Wi-Fi into hazardous areas where getting a high-speed connection is next to impossible. Known as the Node.js WiFi-Extending Robot, the team designed the 150lbs mini-tank using a custom-built aluminum frame (using 3D CAD software, a CNC machine and water-jet cutter) with after-market treads that house a couple of 12V brushed DC motors powered by 9 14.8V lithium polymer batteries (45Ah total with a 12 hour run-time) that give it a top speed of 8-10 mph. The robots motor controls make use of an Arduino unit attached to a custom made H-bridge (electronic circuit) which out-puts PWM signals through a serial-port to the robots ASUS EEE PC brain (running Ubuntu) housed inside of a Pelican case (Pelican cases are designed to take a lot of punishment).

 

The robots Wi-Fi system makes use of a series of Linksys routers that have been adapted to use dd-wrt firmware and outfitted with long range antennas and power amplifiers (for greater range) all housed in their own Pelican cases for communication. One of the routers is used for command and control while the others are attached to aluminum skids that can be deployed (solenoid actuated) off of the robots tail-end and used as repeaters. The user controls the robot through a node.js web server from up to 1km away using any PC and navigates using the robots on-board camera system and is able to see real-time telemetry such as GPS coordinates, signal strength and interface connection status to name a few. Judging from the robots design (it can easily carry a 150lbs man), it’s easy to see why it would be invaluable in places such as battlefields or disaster areas where communication would be crucial in not only saving lives but to place an order for pizza delivery from the nearest FOB (Forward Operating Base).

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • gervasi
    gervasi over 13 years ago

    I wonder if they control the robot with Wi-Fi or a more narrow-band system.  A narrow-band system will buy you at least 20dB, maybe 30dB, lower noise floor than Wi-Fi.  They probably use Wi-Fi, since you need a Wi-Fi connect to the robot to have a useful reason for local clients to connect to the robot.  My concern would be driving into a deep fade and losing contact.  I'd want either a low-noise-floor narrow-band transceiver for control on the robot or loads of fade margin. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • gervasi
    gervasi over 13 years ago

    I wonder if they control the robot with Wi-Fi or a more narrow-band system.  A narrow-band system will buy you at least 20dB, maybe 30dB, lower noise floor than Wi-Fi.  They probably use Wi-Fi, since you need a Wi-Fi connect to the robot to have a useful reason for local clients to connect to the robot.  My concern would be driving into a deep fade and losing contact.  I'd want either a low-noise-floor narrow-band transceiver for control on the robot or loads of fade margin.