Publications
  • Learn
  • More
Publications
Blog iCraft robotic arm controlled by eye movement can help feed the disabled
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 11 Jun 2012 6:18 PM Date Created
  • Views 663 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • hmi
  • robotics
  • robot
  • on_campus
  • Design
  • cabeatwell
  • prototyping
  • university
  • technology_for_the_disabled
  • sensor
  • innovation
  • communication
Related
Recommended

iCraft robotic arm controlled by eye movement can help feed the disabled

Catwell
Catwell
11 Jun 2012

image

The Team: Ryan LaVoie, James Barron, Pedro Lopes, Nick Aquino, Basel Magfory, Mohammed Kante and advisor electrical and computer engineering professor Waleed Meleis (via Mary Knox Merrill & Northeastern University)

 

The disabled, as well as their caregivers, know that the simple act of trying to eat can be a daunting task in itself. People eat at different rates (speed) that caregivers have a difficult time trying to match those individual speeds so a team of engineers from Northeastern University in Boston designed a robotic arm that overcomes that problem and provides a personal sense of freedom.

 

The team, led by Mohamed Kante, designed the robotic arm so that the user can control it by eye movement alone. Called ‘iCRAFT’ (eye Controlled Robotic Arm Feeding Technology), the robot functions using color-coded boxes situated on a monitor which correlates with individual containers of food. A camera positioned next to the user follows the user’s pupil direction with specialized eye-tracking software and detects which colored box (4 in all with 3 associated with two bowls of food and a drinking bottle with the fourth being a pause feature) the subject is looking at and then sends a signal to the robotic arm to scoop up the food from the corresponding food container.

 

The robotic arm the team used to create iCRAFT (unknown at this time) looks to be a RobotShop M100RAK which features 4 Hitec HS785HB servo motors with four degrees of movement and operates with 4.8 to 6 volts of power depending on torque. Similar configurations of robotic assistive arms can cost around $3,500 US but the team states that building the iCRAFT set them back only $900 US which seems very affordable for the amount of freedom it gives the user. The design won the ECE Capstone Design Competition 2012.

 

See more about robotics in the element14 Robotics goup.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    I like the idea very much.

     

    Anything we can do to create a better life for the disabled the better.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Catwell
    Catwell over 13 years ago in reply to DAB

    DAB,

     

    I feel the same way, which is why I have added a tag to posts I feel show the progress in Technology For The Disabled.

     

    We all will need the benefits of such research eventually in life.

     

    Cabe

    http://twitter.com/Cabe_e14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Catwell
    Catwell over 13 years ago in reply to DAB

    DAB,

     

    I feel the same way, which is why I have added a tag to posts I feel show the progress in Technology For The Disabled.

     

    We all will need the benefits of such research eventually in life.

     

    Cabe

    http://twitter.com/Cabe_e14