Publications
  • Learn
  • More
Publications
Blog Light's magnetic properties, to generate "solar power"
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 19 Apr 2011 2:42 AM Date Created
  • Views 906 views
  • Likes 1 like
  • Comments 2 comments
  • alternative_energy
  • eavesdropper:dit
  • on_campus
  • light
  • magnetic_moment
  • university
  • energy
  • solar
  • innovation
Related
Recommended

Light's magnetic properties, to generate "solar power"

Eavesdropper
Eavesdropper
19 Apr 2011
image
William Fisher (via University of Michigan)
 
University of Michigan researchers have discovered a way to use a lesser property of light for the production of electricity. Light has weak electric and magnetic components that most have ignored as an important effect. But it was not passed over by Professor Stephen Rand of the school's engineering departments. Rand found that if the light is intense enough, while passing through a non-conductive material, will produce a magnetic field 100 millions time stronger than previously measured.
 
Doctoral Student William Fisher explains, "It turns out that the magnetic field starts curving the electrons into a C-shape and they move forward a little each time. That C-shape of charge motion generates both an electric dipole and a magnetic dipole. If we can set up many of these in a row in a long fiber, we can make a huge voltage and by extracting that voltage, we can use it as a power source."
 
Rand states, " This could lead to a new kind of solar cell without semiconductors and without absorption to produce charge separation." Current solar cells absorb light and produce electricity and heat, with only a maximum efficiency, at the moment, of 10%. Rand's magnetic solar effect is also producing a 10% efficiency, but only a small fraction of the heat, and with only glass focusing and fibre optic guides. In other words, no silicone.
 
Testing will be done with laser light at first, but later with sunlight. The university is seeking patent protection of the intellectual property this has created. Seems to be a lot of  rushing to the patent office these days.
 
Eavesdropper
 
pic via Webster's dictionary
  • Sign in to reply
Parents
  • DAB
    DAB over 15 years ago

    Hi E,

     

    An interesting discovery, but matching the right photon frequency to materials will be key.  Each photon at a given wavelength with be absorbed or emitted depending upon the energy levels between the electron bands of the material.  Still, with some study, there may be a way to predict which materials will respond best to each of the different energy levels.

     

    Thanks,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to DAB

    They are definitely hard at work to exploit this aspect of light. What I like about this idea is how it could be combined with standard solar panels. Not only would the visible light and infrared light get absorbed, but the magnetic solar could also be collected. Efficiency jumps to 20%. Pump water through the system to cool it, provide a solar photovoltaic boost, and collect the heated water from it. Overall, it would knock most alternative energy collection per square foot out of contention.

     

    E

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Eavesdropper
    Eavesdropper over 15 years ago in reply to DAB

    They are definitely hard at work to exploit this aspect of light. What I like about this idea is how it could be combined with standard solar panels. Not only would the visible light and infrared light get absorbed, but the magnetic solar could also be collected. Efficiency jumps to 20%. Pump water through the system to cool it, provide a solar photovoltaic boost, and collect the heated water from it. Overall, it would knock most alternative energy collection per square foot out of contention.

     

    E