Publications
  • Learn
  • More
Publications
Blog New resistive memory lasts longer than any current flash
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Eavesdropper
  • Date Created: 20 Jul 2011 6:57 PM Date Created
  • Views 753 views
  • Likes 1 like
  • Comments 2 comments
  • research
  • test
  • dit
  • eavesdropper:dit
  • industry
  • memory
  • resistive_memory
  • innovation
Related
Recommended

New resistive memory lasts longer than any current flash

Eavesdropper
Eavesdropper
20 Jul 2011
image
ReRam layers via Samsung
 
All flash memory has a finite number of guaranteed write/rewrite times. Some older and cheaper types are set at 100,000 and more advanced have 1,000,000. Using this type of memory as a solid state harddrive could push the memory to its breakdown phase fairly quickly with the constant disk access seen in most modern operating systems.
 
Researchers at the Samsung Advanced Institute of Technology are looking into creating non-volatile ReRam (resistive RAM) that is able to handle write cycles in the excess of 1,000,000,000,000 (1 trillion) at speeds (10ns) of up to a million times faster than current flash technology.
 
ReRam has dielectric properties. Normally insulating, but when energized it becomes conductive. Very much like a transistor gate, the memory element is a conductive path when its gate is closed. Apply the electrical spike and the gate opens, restricting current flow. Apply again, and the gate closes. Each bit of data holds its last state without power. Past ReRam was a tantalum film (Ta2O5 ). The Samsung researchers use a bi-layer structure of Ta2O5-x/TaO2-x filaments. This new bi-layer ReRam allows for more data to be set through the filament paths.
 
The IMEC consortium, a collection of the biggest technology companies, is behind this research. Member companies like HP, Intel, Panasonic, and, of course, Samsung want to explore and advance nano-electronics. Although this bi-layer ReRam looks promising, it is still several years away.
 
Eavesdropper
  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    It looks like an interesting approach, but didn't they have some issues with the old Tantalum capacitors that forced them off the market?

     

    Anyway, I agree that it will be a few years before we see these devices in a useable component.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    It looks like an interesting approach, but didn't they have some issues with the old Tantalum capacitors that forced them off the market?

     

    Anyway, I agree that it will be a few years before we see these devices in a useable component.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 14 years ago in reply to DAB

    Tantalum capacitors are the most used today. However, some older military surplus of wet-slug tantalum caps have a tendency to leak electrolyte or complete loss through the failing of the teflon seal.

     

    I would agree, we will not see the commercial use for many years.

     

    Cabe