Publications
  • Learn
  • More
Publications
Blog Stephen Hawking looks to use the iBrain as a new way of speaking
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 19 Jul 2012 7:37 PM Date Created
  • Views 826 views
  • Likes 2 likes
  • Comments 1 comment
  • research
  • industry
  • hmi
  • eeg
  • on_campus
  • Design
  • cabeatwell
  • prototyping
  • measurement
  • university
  • technology_for_the_disabled
  • sensor
  • brain
  • innovation
  • communication
Related
Recommended

Stephen Hawking looks to use the iBrain as a new way of speaking

Catwell
Catwell
19 Jul 2012

image

Stephen Hawking at Cambridge (via Hawking & Wikipedia)

 

A new device may give theoretical physicist Stephen Hawking the ability to speak using only his mind. Called the iBrain, the device was designed and developed by neuro-diagnostics company NeuroVigil to transform thought into speech. Actually the device is a portable EEG (Electroencephalography) machine that is attached to the head of the wearer and monitors brainwaves using two electrodes.

 

The headgear is capable of recording information for days without requiring a recharge and features a USB port for data transfers that can then be sent over the internet to health professionals for examination. The device is used in conjunction with a special algorithm, called SPEARS (Sleep Parametric EEG Automated Recognition System), which is capable of in-depth analysis and classification of both daytime and nighttime EEG patterns. These patterns can then be used to identify and diagnose sleep related medical conditions or, in the case of Stephen Hawking, central nervous system diseases such as Parkinson’s or amyotrophic lateral sclerosis (a form of motor neuron disease).

 

Professor Hawking was diagnosed with ALS during when he enrolled at the University of Cambridge and was not expected to live 2 or 3 years beyond his 21st birthday. As he became slowly paralyzed over time, it was necessary for him to incorporate technology that could help him speak such as his trademark voice synthesizer hardware. That device allows him to use his cheek muscle twitches which trigger an infrared sensor to write sentences (at approximately one word per minute) that are then ‘voiced’ by the computer hardware.

 

image

iBrain concept (via Neuro Vigil)

 

His system uses predictive text input software that can complete a word by typing the words first few letters much like texting with smartphones. However, as his ALS slowly paralyzes his body even his cheek movements will cease to function which is why he is testing the iBrain. Currently, it is being used to detect his brain patterns associated with speech.

 

The US military is also interested in the device and the company states that the US Navy had sent them an anonymous soldier’s iBrain EEG read-out to be analyzed using NeurVigil’s software. The Navy did not specify if that particular soldier was healthy or not. The company team responsible for the analysis found that the read-out showed that the subject suffered a traumatic brain injury as well as post-traumatic stress disorder. On top of their findings, they were even able to identify patterns associated with taking an antidepressant drug for anxiety!

 

The iBrain system has promising potential and could give the renowned physicist the capability of talking using way less hardware than he uses now, but the system is still being developed. As it stands, the company states that they are 35% done developing the iBrain 2 (which will also monitor heart-rates) and even have started the planning stages of the iBrain 3 which would be an available commercial version that could be connected to an iPhone or Android-based phone and cost around $100 US.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    I have been playing with the Neurosky mind wave device and so far I am impressed.

    I used it to monitor my pain levels and it was amazing.  I could watch my concentration levels drop as the pain increased and then my brain was able to mask the pain and let the concentration improve until the next pain wave repeated.

     

    So having tested this interface I feel confident that you will see a lot more implementations.  The age old dream of communicating with just your brain is becoming reality.  I hope someone goes around to all of the people trapped within their paralysed bodies and free their minds to communicate.  What they are experiencing would be of great value for the Medical field to find better ways to treat people who cannot consciously communicate.

     

    I look forward to the future developments of these devices.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    I have been playing with the Neurosky mind wave device and so far I am impressed.

    I used it to monitor my pain levels and it was amazing.  I could watch my concentration levels drop as the pain increased and then my brain was able to mask the pain and let the concentration improve until the next pain wave repeated.

     

    So having tested this interface I feel confident that you will see a lot more implementations.  The age old dream of communicating with just your brain is becoming reality.  I hope someone goes around to all of the people trapped within their paralysed bodies and free their minds to communicate.  What they are experiencing would be of great value for the Medical field to find better ways to treat people who cannot consciously communicate.

     

    I look forward to the future developments of these devices.

     

    DAB