Publications
  • Learn
  • More
Publications
Blog UWB Positioning System Helps Blind Navigate Indoors
  • Blog
  • Documents
  • Events
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Publications to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 9 Jul 2012 6:21 AM Date Created
  • Views 672 views
  • Likes 1 like
  • Comments 2 comments
  • android
  • research
  • transportation
  • industry
  • hmi
  • on_campus
  • embedded
  • cabeatwell
  • prototyping
  • measurement
  • university
  • technology_for_the_disabled
  • sensor
  • innovation
  • communication
Related
Recommended

UWB Positioning System Helps Blind Navigate Indoors

Catwell
Catwell
9 Jul 2012

image

Navigation network for the blind concept (via Fujitsu)

 

As technology becomes more readily accessible and integrated into the home, harnessing the connectivity can aid people with disabilities live an easier life. Blindness can be a crippling handicap, especially to those who were not born blind. Navigation through one's home should not be an accident waiting to happen. Japan’s National Institute of Information and Communications Technology along with the company Fujitsu  are developing a system based on Ultra Wideband Network (UWN) that will allow the blind to navigate around their homes using sound.

 

The indoor support system ties a UWB network and a smartphone with a Fujitsu developed app to direct the user with audible directions. The impulse radio UWB transceivers, called base stations, are able to measure distances and create a digital map of the indoor environment. A smartphone for the user and other bases located at critical destinations make up the mobile stations. A PC control station analyzes all of the positioning data in real time and transmits directions to the user’s smartphone using 12 o’clock directional signals and specifying distances. The system is accurate to within 30 centimeters. One catch, the system requires Android 2.3 or newer.

 

Future work includes adding sensors and developing software that can detect obstacles. This particular prototype network is intended as an aid for the blind, but other application for indoor navigation are in the works. This UWB system could be used for guidance through museums, government buildings, hospitals etc. The system was demonstrated at Wireless Technology Park 2012, July 5-6 at Pacifico Yokohama.

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • DAB
    DAB over 13 years ago

    It might be more effective given a normal noise background.

     

    Whatever the reason, it is good to see the improvement for those who need the assistance.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gervasi
    gervasi over 13 years ago

    This is the first UWB application I've heeard of that actually uses Gaussian monopoles (impulse radio) instead of just a really wideband version of conventional modulation.  I'm unclear though why they needed to impulse radio.  Couldn't they have embedded the timing info on conventional modulation? 

     

    I like this research b/c I always felt like impulse radio is a neat idea that desperately needs a killer app.  It's a neat idea, but someone needs to think of a way to make it actually do something.  Maybe this is one such app.