Member and Staff Blogs Great Prize - Multicomp Pro MP720105
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 21 Dec 2022 3:20 AM Date Created
  • Views 1551 views
  • Likes 10 likes
  • Comments 4 comments
  • dougw
  • mystery card
  • Multicomp Pro MP720105
Related
Recommended

Great Prize - Multicomp Pro MP720105

dougw
dougw
21 Dec 2022

This is a quick video about the Multicomp Pro MP720105 which was a prize for guessing a mystery circuit card:

 Now, Can You Guess where this FULL PCB came from? (If so you could Win an oscilloscope!) [CLOSED] 

It is a phenomenal prize for such a contest - thank you element14 and baldengineer  

It is another instrument that is well suited to use in blogs because it is very thin and doesn't hog the bench, allowing room for the project apparatus.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Relevant Links:

 Now, Can You Guess where this FULL PCB came from? (If so you could Win an oscilloscope!) [CLOSED] 

  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 3 years ago +1
    Glad it arrived! I have a similar model that I kept because they are a good trade-off for the size, performance, and capability. I was poking at the SCPI command set recently. I was hoping to make…
Parents
  • baldengineer
    baldengineer over 3 years ago

    Glad it arrived!

    I have a similar model that I kept because they are a good trade-off for the size, performance, and capability. 

    I was poking at the SCPI command set recently. I was hoping to make a scottiebabe inspired script to capture multiple screenshots for an animated GIF.

    My hope was there would be a command to cause a screenshot save to a USB drive. I did not see one. But I think it is possible to get the bitmap with a SCPI command—just need to spend more time with it. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to baldengineer

    Aww, thanks for the shoutout! Scope gifs are the best!

    When you do, you can sell it for millions as an NFT on the blockchain Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • scottiebabe
    scottiebabe over 3 years ago in reply to baldengineer

    Aww, thanks for the shoutout! Scope gifs are the best!

    When you do, you can sell it for millions as an NFT on the blockchain Slight smile