Member and Staff Blogs How will GaN change the world of electronics design in the next decade?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 29 Aug 2019 8:40 PM Date Created
  • Views 1382 views
  • Likes 7 likes
  • Comments 9 comments
Related
Recommended

How will GaN change the world of electronics design in the next decade?

rscasny
rscasny
29 Aug 2019

Silicon has been the kingpin of the semiconductor industry for a long time. And it should be: it has an ideal crystal structure for use as a semiconductor, But in today's world where ultra-low power and an extremely small package are two important factors in electronics design, maybe silicon has sort of reached its limits. What's the alternative?

 

As a semiconductor material, gallium nitride (GaN) is getting the attention that silicon once had. GaN works will in high voltage and high temperature applications. Plus it has high switching frequencies than silicon and attractive for its high energy efficiency.

 

So, how will GaN change the world of electronics design in the next decade?

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 7 years ago +2
    I've been validating GaN power FETS for a few years now. Checking Out GaN Half-Bridge Power Stage: Texas Instruments LMG5200 - Part 1: Preview I think they have a place together with silicon, won't replace…
  • dougw
    dougw over 7 years ago +1
    I am looking forward to using GaN devices in the near future because of their lower on resistance. It looks like you could come up with something closer to an ideal diode than what can be done today. GaN…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to clem57 +1
    clem57 wrote: Well the cost factor may be a little overrated. This is due to the process not being as mature as silcon manufacturing. But take a look at this article and set me straight, Jan Cumps . Clem…
  • colporteur
    colporteur over 7 years ago +1
    Establish a panel of long tooths, those individuals around when glass transistor were the norm and silicon replacements were coming out of the wings, and ask them the same question regarding silicon? As…
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to colporteur +1
    I also think it's a great technology. From germanium/glass to silicon was a clearer case though - except where a low forward drop is important and germanium is still used. It's somewhat different with…
  • colporteur
    colporteur over 7 years ago in reply to Jan Cumps +1
    I put my hands up and surrender. I haven't investigated the properties of GaN in comparison. Your commentary caused me to recall germanium diodes lower voltage drop compared to silicon. I seem to think…
Parents
  • shabaz
    shabaz over 7 years ago

    I'm not too clued-up on the physics of it all, but I'm especially interested in GaN LEDs. Some manufacturers concentrated on that, presumably because they'd invested in GaN technology for power applications too, and it takes years to refine their processes. Whereas other manufacturers might have started with a different technology (e.g. Silicon Carbide) and are expanding into that. Apparently there's many variants too, like GaN devices grown on SiC, or grown on sapphire, and again the manufacturers have to spend years /decades refining things, not knowing for sure if the research will bear fruit, or if an alternative technology will take over (especially if the processes to work with it end up cheaper or more reliable for instance).

    So, it's very exciting, continually seeing the improvements in light quality and efficiency that they're achieving.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago

    I'm not too clued-up on the physics of it all, but I'm especially interested in GaN LEDs. Some manufacturers concentrated on that, presumably because they'd invested in GaN technology for power applications too, and it takes years to refine their processes. Whereas other manufacturers might have started with a different technology (e.g. Silicon Carbide) and are expanding into that. Apparently there's many variants too, like GaN devices grown on SiC, or grown on sapphire, and again the manufacturers have to spend years /decades refining things, not knowing for sure if the research will bear fruit, or if an alternative technology will take over (especially if the processes to work with it end up cheaper or more reliable for instance).

    So, it's very exciting, continually seeing the improvements in light quality and efficiency that they're achieving.