Member and Staff Blogs NASA’s new space suit design features increased protection and maneuverability
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 2 May 2014 7:53 PM Date Created
  • Views 971 views
  • Likes 0 likes
  • Comments 3 comments
  • vote
  • hmi
  • nasa
  • droud_sourcing
  • Design
  • cabeatwell
  • space_suit
  • croud
Related
Recommended

NASA’s new space suit design features increased protection and maneuverability

Catwell
Catwell
2 May 2014

image

ILC Dover’s New Z-2 space suit protects against micrometeor strikes and features fashionable shorts. (via NASA)


NASA has had roughly nine spacesuits designed for astronauts to travel into space with since Alan Shepard was chucked into orbit during the Project Mercury back in the early 60s. The current suit used by American astronauts is the Enhanced Mobility Unit (EMU) designed by ILC Dover and has been the ‘go-to’ suit for space-faring humans since 1981. That suit however, is nearing its end and really isn’t sufficient for otherworldly ventures, such as the exploration of Mars. In an effort to get up to date with a better, modern spacesuit that can handle the rigors of kicking rocks on other planets as well as taking a beating while floating in space, NASA recently held a $4.4-million design challenge for a replacement.


Three suits made the finals and the general public was invited to vote for the winner, with 63% of the vote going to ILC Dover and their peculiar-looking Z-2 Spacesuit. A slight upgrade from the prototype Z-1, dubbed the ‘Buzz Lightyear’ suit because of the fluorescent green stripping used for identification. The cleverly named Z-2 features a hard-shell composite torso section (over the Z-1’s soft-shell) that’s comparable to body armor in that it will protect against micrometeor impacts, extreme temperatures and radiation when performing EVAs (Extravehicular Activities). The shoulder and hip joints have been redesigned for increased mobility and the boots have been reengineered for increased performance in the vacuum of space and ruggedized for the rocky surfaces found on the moon and Mars. The suit will sport some functional fashionable identifiers, such as light-emitting panels and Luminex wiring to help locate astronauts if trouble arises. It will also feature ‘classic’ connections to interface with existing airlocks and suit-ports. A prototype is expected to be delivered to NASA by November of this year and human-rated vacuum tested with an included PLSS (Portable Life Supporting System) by 2020.


C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    It looks like they have improved a number of features, but I would have to try one on to see how flexible it would be. image

     

    Going forward I think we need easy to put on suits, rugged materials without being so constrictive to prevent the type of outer space working environments or potential lunar and mars surface activity.

    I do like the greater visibility, but I wonder how much thermal gain would occur in sunlight.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    It looks like they have improved a number of features, but I would have to try one on to see how flexible it would be. image

     

    Going forward I think we need easy to put on suits, rugged materials without being so constrictive to prevent the type of outer space working environments or potential lunar and mars surface activity.

    I do like the greater visibility, but I wonder how much thermal gain would occur in sunlight.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Catwell
    Catwell over 12 years ago in reply to DAB

    How long until we see this on another planet? Maybe not even in my lifetime...

     

    C