Member and Staff Blogs What's new in fairy tech?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scottiebabe
  • Date Created: 16 Nov 2023 1:35 AM Date Created
  • Views 2602 views
  • Likes 11 likes
  • Comments 19 comments
Related
Recommended

What's new in fairy tech?

scottiebabe
scottiebabe
16 Nov 2023

The first set of fairy lights I purchased a few years ago had a very rudimentary embodiment. Just two AA batteries, an on/off switch, and a string of miniature LEDs on enamel wire.

image

I love the simplicity of the design... The design works well enough with disposable alkaline batteries. However recharge cells don't work very well on their own, as their combided state of charge voltage very quickly drops below the forward voltage of the white LEDs.

Fairy Tech 2.0

Browsing at the dollar store today, I found some new fairy lights which included some circuitry on a PCB. What could it be?

image image

Same general look and feel as before.

image

Now included is a three position switch!

image

The mysterious PCB

image

No sign of an inductor anywhere Disappointed. Just a

- 8-pin MCU?

- Watch crystal

- SPDT Slide switch

image

Fairy Tech 3.0

I can upgrade this new set of fairy lights with a boost converter module capable of operating of a single alkaline/Ni-MH cell

image

Module based on ME2188 https://file.elecfans.com/web2/M00/64/78/poYBAGMHOg-APsG0AAge4TQOpd0961.pdf 

I bought a value pack awhile back thinking I would receive a selection of different output voltages. Nope, I got a bag of identical modules and each has a nominal output voltage of 5V. So, I added an additional 50 Ohm series resistor to limit the current to approximately 40 mA.

image

I am taking a bit of a gamble assuming the MCU is 5V rated. If it gives up the ghost, I'll replace it too.

image

All for now.

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 2 years ago in reply to scottiebabe +1
    Out of the box they can also sometimes be a bit too bright for fast lenses with wide open apertures. Arducam do a low-cost F1.6 C-Mount lens which can be used with the likes of a R-Pi HQ camera for bokeh…
  • scottiebabe
    scottiebabe over 2 years ago

    Other Fairy Tech

    An IC specifically designed for Fairy Lights Heart 

    https://www.shiningic.com/zh/productdetail.aspx?detailid=281&classid1=0101&classid2=010111 

    I bought a set of solar powered fairy lights in the spring and found that IC inside.

    image

    image

    image

    image

    image

    image

    Hasn't given up the ghost yet...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago in reply to dougw

    The LEDs are being low side switched by an output pin. There isn't any PWM modulation. The limited drive strength of the MCU output is adding some additional series resistance between the batteries and the LEDs. This would result in a slightly longer runtime when lit. 

    The only new function I can see, is the 6hr timer. Where the MCU switches the LEDs on for 6 hours then off for 18 hours, before the cycle repeats. Just like in many LED candles. Though most of those use three batteries in series, which has a greater output voltage than the forward voltage of white LEDs even when the batteries are depleted.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • electronicbiker
    electronicbiker over 2 years ago

    I bought one of these a few years ago. A simple device, no electronics (apart from the LEDs), just an on/off switch. The lights were quite Christmassy. The main problem was that the springs used for the battery contacts were far too strong. This resulted in the eventual bending-backwards of the end of the case furthest from the switch end, which took about three weeks. Upon close examination, there was a crack in both corners where the back panel meets the sides of the main body at almost 90 degrees. Verdict - Poor mechanical design of the case.

    As I don't work in The Repair Shop I bodged it with an elastic band and some Sellotape, which does not stretch as much as PVC tape. Scottiebabe might do better with only the one cell trying to push the case apart. I did think of replacing both cells using rechargeable 2/3rds AA's with solder tags, arranged so that the cells have to be disconnected while charging. One of those little jumpers would do, like the ones scattered about on PC mother-boards etc, in series with a solder tag. But then I decided that as these lights would only be used for a few days of the year and that not many visitors would be interested in the contents of the battery box, I'd stick with the Sellotape and the rubber band. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago

    So what does the original PCB do? Modulate the power to prevent LED over-current and extend battery life?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<