Engineering Life
  • Community Hub
  • More
Engineering Life
Forum Dimmer repair
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Engineering Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 77 replies
  • Subscribers 41 subscribers
  • Views 14587 views
  • Users 0 members are here
Related

Dimmer repair

wal_e
wal_e over 5 years ago

Hello everyone,

First of all I would like to apologize, I might certainly be in the wrong section, but I have been sent here by the Farnell technical assistance and to be honnest this place is a real maze for me image

So, I have been trying to fix a dimmer that went working only as a simple switch : OFF to ON max light directly. Following my researches it seems that the origin of my problem is a faulty triac and also - maybe - a capacitor ; I have tested both of the 2 fuses and they are ok.

The two original component are labeled:

- BTB04-600A

- CBB62B X2 0.033µF (250-280VAC) dimensions 40/110/56/C

My problem is that I can't find any of the exact two components and I have no idea what I can use to replace them as equivalent.

Any help is really appreciated

Thank you - very much - in advance.

 

W

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 5 years ago +5
    Hi, If rotating the dimmer makes it turn the light on and off, then why do you think the triac is faulty? Couldn't it be the rotary potentiometer? (I don't know - I'm speculating). I'm not sure it is good…
  • jw0752
    jw0752 over 5 years ago +4
    Hi Walid, If you only have off and on and when the dimmer is in the on position it is always at full brightness then the most likely problem is the Triac. You can test this with a continuity tester when…
  • wal_e
    wal_e over 5 years ago in reply to shabaz +4
    Hello Shabaz, Thank you for taking the time to answer. I found this diagnostic on the internet, it says that if the dimmer only works from OFF to ON max power it's a triac issue. As you can imagine this…
Parents
  • jw0752
    jw0752 over 5 years ago

    Hi Walid,

     

    If you only have off and on and when the dimmer is in the on position it is always at full brightness then the most likely problem is the Triac. You can test this with a continuity tester when the dimmer is removed from power by checking the continuity between A1 and A2 terminals. It should be open under normal circumstances. If it is shorted then the triac is bad. The other components are probably OK. The BTB 04-600A is a 4 Amp 600 Volt triac and can be replaced with pretty much any triac that has ratings of more than 4 amps and 600 volts. I have some BTB 06-600 which would be 6 amps and 600 volts. If you are inside the USA I will send one to you. If you are looking at the triac with the pins down and the label facing you the A1 and A2 terminal are the left pin and the center pin. The right pin is the gate and should be attached to a DB3 trigger diode if you have a standard design.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Hi John,

    Thank you for your help I really appreciate your kind answer but I am too far from you that would make this triac very expensive image So, I am experiencing exactly what you described and already replaced the old triac with a new one labeled BTB08-600BW (the only "equivalent" triac I found in the neiborhood) which didn'ty solve the problem. So I just tested both of them and both of their A1 and A2 show no continuity....does that mean they're both open and ok ? When I tested the capacitor I got a 0.0µF instead of 0.033µF...is it possible that my tester is not sensitive enough or is my capacitor is dead ? In that case could he be the origin of the problem ?

    Best regards,

     

    W

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    The Trigger diode or DIAC is a critical part of the dimmer circuit. It is designed to show a very high resistance to AC current until the voltage exceeds its thresh hold at which time it conducts.

     

    https://en.wikipedia.org/wiki/DIAC

     

    In the dimmer circuit the control (probably 500K Ohms) in series with a current limiting resistor( probably 10K) and the capacitor form an RC timing circuit. The setting of the control causes the voltage on the capacitor to rise at different rates. As soon as the voltage on the capacitor exceeds the threshold of the DIAC it fires and turns on the Triac which remains on until the AC current in the circuit passes through the zero point. The period for 60 Hz line voltage is 1/60th of a second and in this time the current passes through Zero twice. The AC line current will automatically turn off the Triac every 1/120 th of a second. If the Diac is shorted there will be no delay since the threshold of the diac will be zero volts and the triac will be triggered very early each 1/2 cycle which will give the appearance of full brightness regardless of control setting. If the DIAC is working properly the triac will not be triggered until much later in the half cycle and it will give the appearance of being dimmer.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Here is the Newark listing for the DIAC DB3 which is the most commonly used DIAC in the dimmer controls.

     

    https://www.newark.com/stmicroelectronics/db3/diac-28v-to-36v-do-35/dp/89K1258

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Hi John, thank you for these explanations I guess it is the last possible malfunctioning element ? How can I test the Diac knowing that my DMM can't do it ?

    Thank you in advance

     

    W

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Actually your meter should be able to test to see if it is shorted. Put the meter on Ohms and test across the DIAC. A short or very low ohms would be bad. Breaking the connection of one of the leads to the circuit should also cause the Triac to stay turned off. If the light no longer turns on with the switch when one of the diac leads is disconnected this would further confirm that the Triac is OK.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    It is too narrow for me to try disconnecting one of the leads it is a bedlight dimmer and everything is compacted. My DMM shows OL when testing de Diac in Ohm mode. I asked a friend for his professional DMM. I will test the db3 c531 and let you know but will most certainly replace it anyways...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Never thought to ask: What type of bulb are you using in the lamp?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Good question indeed, I am using a regular incandescent bulb.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Hi Walid,

     

    In order to do some experimenting I built a dimmer circuit on bread board.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    The first thing I learned from doing this is that my explanation of the circuit a few posts ago was at best simplistic and probably incorrect. My Experiments indicate that your Diac is likely OK. The capacitor value is fairly critical. Too much capacitance and the light stays on high. Too little capacitance and the light stays on high. No capacitance and the light stays off. Shorted Diac or one with parallel resistance and the light stays off. No Diac in circuit and the light stays off. I am sorry as this may not simplify or help much. If you have experiments that you would like me to run let me know. I will leave the bread board assembled for a few days.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Tonight I hooked up the oscilloscope as I wanted to see the change in the signal on the gate of the triac as the potentiometer was turned from a dim setting to a bright one. Channel one (Yellow) shows the source AC voltage and syncs the horizontal trace. Channel two (blue) is the gate of the triac and the trace on the Hantek Scope is across the bulb. Note the RMS voltage as we go from very dim to full brightness.

     

    imageimage

     

    Dim Setting

     

    imageimage

     

    Bright Setting

     

    Note of Caution. Taking readings of AC line voltage can be dangerous. I used an isolated bench AC source for this experiment and a portable secondary scope so than I would not have an Earth or Common ground conflict.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Hi John,

    I am really glad to see that here are persons like you whom put all that effort to help others. So, I changed the Diac and nothing changed still from Off to On full brightness. This, with your last message about the importance of capacitance lead me to think that, in fine, it's the capacitor that's dead or faulty and unfortunatly I couldn't find the exact same one to replace it. I took some photos of the controller and the DMM I borrowed from a friend so if you have any suggestions or ideas please let me know, I would be happy to explore further more.

    Best regards,

     

    Walid

    image

    image

    image

    image

    image

    image

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    Hi John,

    I am really glad to see that here are persons like you whom put all that effort to help others. So, I changed the Diac and nothing changed still from Off to On full brightness. This, with your last message about the importance of capacitance lead me to think that, in fine, it's the capacitor that's dead or faulty and unfortunatly I couldn't find the exact same one to replace it. I took some photos of the controller and the DMM I borrowed from a friend so if you have any suggestions or ideas please let me know, I would be happy to explore further more.

    Best regards,

     

    Walid

    image

    image

    image

    image

    image

    image

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to wal_e

    If you put the DMM in the 200 nF range,it should give a good measurement of that cacitor. : The value 33 - or something within 10% of that.

    You need to fit the capacitor legs into the 2 slots with capacitor symbol.

    Discharge the capacitor first.

     

    It's indeed a good DMM.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to Jan Cumps

    Hi Jan,

    I tested both: brown one on the PCB and the yellow - original one, they both read 00.0 µF :/ I am even starting to doubt the DMM....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to wal_e

    I found this page which I think is quite interesting and clear :

    https://www.astuces-pratiques.fr/electronique/variateur-a-triac-fonctionnement-et-schema

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to wal_e

    image

    Is this how you measured them? If yes, I think they are defect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    I would like to know if the lamp lights with the DIAC out of the circuit.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to Jan Cumps

    I couldn't put them in the dedicated slot since both have already been soldered and thus have short legs I used the DMM leads. BUT, I read an article about dimmers and how they work and can generate parasites and just figured out  that the capacitor I have been testing and changing the whole time is the one in charge of reducing these parasites along with the coil...and looking closer I saw a smaller capacitor that you can barely see on this photo behind the big one:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to jw0752

    No John, the light stays off whithout the DIAC...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to wal_e

    Thanks for running the experiment which confirms that the Triac is OK and that the Diac is also OK.  Verify that the resistors have the proper values and then the only thing left is the capacitor.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to wal_e

    wal_e  wrote:

     

    I couldn't put them in the dedicated slot since both have already been soldered and thus have short legs I used the DMM leads.

    I believe you have to use the two slots for capacity measurements.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • wal_e
    wal_e over 5 years ago in reply to Jan Cumps

    Well that would make perfectly sense....I will use wire extensions and let you know