Engineering Life
  • Community Hub
  • More
Engineering Life
Forum Magnetic Radiation
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Engineering Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 42 subscribers
  • Views 7535 views
  • Users 0 members are here
  • electro magnetic engineers
Related

Magnetic Radiation

lescolliershustoke@virginmedia.com
lescolliershustoke@virginmedia.com over 9 years ago

Hi

     a question :>

 

I have a solenoid and it has a certain range to it, i.e. the magnetic field does not go on fro ever for practical purposes.

 

I can adjust the design to gain more range, I can wind more turns on the armature but this won't extend the range if the core material saturates out. I can up the voltage and hence the current, but this creates more heat that I have to dissipate, and I want to power from a battery at the end of the day. So I am trying to get the longest range I can from 10 to 14 volts.

 

 

Does anyone have an answer on which parameter to try moving first assuming the range I have is not good enough.

 

regards

 

 

Les C

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp +2
    Can you draw a diagram of what you are trying to do, or at least explain it better. Generally speaking magnetism is not a long range phenomenon (ie it's pretty weak once you are separated from the source…
  • jw0752
    jw0752 over 9 years ago in reply to lescolliershustoke@virginmedia.com +2
    Hi Les, The magnetic field lines, that are being generated by a specific amount of power (Amps times Volts), are part of a magnetic circuit that by convention comes out of the north pole and loops around…
  • D_Hersey
    D_Hersey over 9 years ago +2
    Frequently Used Equations – The Physics Hypertextbook Radiation – The Physics Hypertextbook
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi Les,

     

    I got the impression from your question that you are using an open coil and that you are not talking about the travel of a plunger but rather the extent that the magnetic field extends radially from the coil. Is this so?

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lescolliershustoke@virginmedia.com
    lescolliershustoke@virginmedia.com over 9 years ago in reply to jw0752

    Hello yes this is the case i.e. from a coil and core how do I achieve the maximum range ?  Given I have limited power i.e. a 12V battery.

     

    I think, but don't know, If I pick the right core material it will help, not sure about geometric shape.

     

    regards

     

    Les C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp

    Can you draw a diagram of what you are trying to do, or at least explain it better. Generally speaking magnetism is not a long range phenomenon (ie it's pretty weak once you are separated from the source by a distance equivalent to the size of the source, eg the flux from a solenoid is pretty low once you are 1 solenoid length away from the end.) - if we understood what you are trying to do it might be possible to help a bit better.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to lescolliershustoke@virginmedia.com

    Hi Les,

    The magnetic field lines, that are being generated by a specific amount of power (Amps times Volts), are part of a magnetic circuit that by convention comes out of the north pole and loops around to enter at the south pole of the field. As with all things in nature this path is path of least resistance. Each line of magnetic force is repelled by the adjacent lines of force while simultaneously being attracted by the opposing pole of the magnet. This is why we get the characteristic field shape of a bar magnet or a solenoid.

     

    image

     

    Mathematically the line of force that comes out of the center of the magnetic field extends to infinity before looping back to the other pole but as D_Hersey correctly pointed out we have some form of inverse square law to deal with with respect to the intensity of the field as we go out. This makes the extension of the strength field dependent on the length of the magnet or solenoid to some extent and also the power that we put into the generation of the field. If you are looking for some way to focus the power of your solenoid's magnetic field so that you can project the magnetic effect an extended distance with a limited power source you have a very difficult engineering problem. The nature of the magnetic field is not amenable to this type of manipulation. I do not think that the converter will be of much help. For any specific coil resistance increasing the voltage will increase the current and thus increase the strength of the field but it will also create a commensurate increase in current draw from your battery. What I mean is that there will be no magic free increase in field intensity without paying for it with additional power input.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 9 years ago in reply to jw0752

    Bravo John!

     

    So often in physics, if we are dealing with a polynomial it is a second-order one.

     

    I saw a product called a 'magnetic lens' once.  It was a radially symmetrical piece of ferrite that was fat on one and skinny on the other.  The intention IIRC, was to put the fat end near the sensed and the skinny end by a Hall-effect sensor.  But you are right, there isn't much going on in this dimension

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to D_Hersey

    Hi Don,

    Yes the use of magnetic interactive materials can shape a field. Extending the core material of the solenoid can extend the field and there are diamagnetic materials that repel a magnetic field but in all of these cases the materials have to cover the distance. I get the impression that Les is hoping to project the magnetic field without material field shaping materials.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 9 years ago in reply to jw0752

    Wow, John you are all over this!  Sorry if I was being pedantic

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to D_Hersey

    That is what is so great about you being involved in a conversation. I always learn something as you push the limits and have such a great way of bringing in related ideas and topics.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • lescolliershustoke@virginmedia.com
    lescolliershustoke@virginmedia.com over 9 years ago in reply to jw0752

    Mathematically the line of force that comes out of the center of the magnetic field extends to infinity before looping back to the other pole but as D_Hersey correctly pointed out we have some form of inverse square law to deal with with respect to the intensity of the field as we go out. This makes the extension of the strength field dependent on the length of the magnet or solenoid to some extent and also the power that we put into the generation of the field. If you are looking for some way to focus the power of your solenoid's magnetic field so that you can project the magnetic effect an extended distance with a limited power source you have a very difficult engineering problem. The nature of the magnetic field is not amenable to this type of manipulation. I do not think that the converter will be of much help. For any specific coil resistance increasing the voltage will increase the current and thus increase the strength of the field but it will also create a commensurate increase in current draw from your battery. What I mean is that there will be no magic free increase in field intensity without paying for it with additional power input.

     

     

    John you have the problem nailed correctly, what you have explained is exactly what I am trying to do.  Thanks by the way to all of the other contributors I have read them all and there are far more than I expected thank you so much.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lescolliershustoke@virginmedia.com
    lescolliershustoke@virginmedia.com over 9 years ago in reply to lescolliershustoke@virginmedia.com

    Sufficient  to say,  If I can get this product off the ground sufficient to say it will save lives quite literally.

     

     

     

    .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to lescolliershustoke@virginmedia.com

    As John points out, the magnetic field can be channeled by appropriate materials.

    In solenoids these pole pieces can for example turn a linear solenoid into a horseshoe magnet, concentrating the field between the poles. This might allow you to have a much stronger field further from a pole than you would get with a linear solenoid.

    If you describe your geometry requirements we might be able to suggest a more appropriate solution.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 9 years ago in reply to rachaelp

    "Air doesn't saturate."  Ferrite does. This may limit the utility of this approach 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 9 years ago in reply to rachaelp

    "Air doesn't saturate."  Ferrite does. This may limit the utility of this approach