Engineering Life
  • Community Hub
  • More
Engineering Life
Forum Magnetic Radiation
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Engineering Life to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 42 subscribers
  • Views 7527 views
  • Users 0 members are here
  • electro magnetic engineers
Related

Magnetic Radiation

lescolliershustoke@virginmedia.com
lescolliershustoke@virginmedia.com over 9 years ago

Hi

     a question :>

 

I have a solenoid and it has a certain range to it, i.e. the magnetic field does not go on fro ever for practical purposes.

 

I can adjust the design to gain more range, I can wind more turns on the armature but this won't extend the range if the core material saturates out. I can up the voltage and hence the current, but this creates more heat that I have to dissipate, and I want to power from a battery at the end of the day. So I am trying to get the longest range I can from 10 to 14 volts.

 

 

Does anyone have an answer on which parameter to try moving first assuming the range I have is not good enough.

 

regards

 

 

Les C

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp +2
    Can you draw a diagram of what you are trying to do, or at least explain it better. Generally speaking magnetism is not a long range phenomenon (ie it's pretty weak once you are separated from the source…
  • jw0752
    jw0752 over 9 years ago in reply to lescolliershustoke@virginmedia.com +2
    Hi Les, The magnetic field lines, that are being generated by a specific amount of power (Amps times Volts), are part of a magnetic circuit that by convention comes out of the north pole and loops around…
  • D_Hersey
    D_Hersey over 9 years ago +2
    Frequently Used Equations – The Physics Hypertextbook Radiation – The Physics Hypertextbook
Parents
  • D_Hersey
    D_Hersey over 9 years ago

    Frequently Used Equations – The Physics Hypertextbook

     

    Radiation – The Physics Hypertextbook

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 9 years ago in reply to D_Hersey

    Hi Don,

     

    Just be aware that Planck's constant and radiation law are not correct over the range indicated in the current physics domain.

     

    I am still working out details, but the idea of temperature related to photon wavelength is incorrect.

     

    Yes there is a correlation, but each photon represents a specific kinetic energy based upon its mass and charge.

     

    If you use Planck's radiation law, you get the wrong values for any photon outside a limited domain of 1 to 3 microns.

     

    Even there, he was wrong as his experimental apparatus and sensors were providing the wrong information over the ranges of temperatures he used to create his fudge factor.

     

    DAB

     

    PS to all, magnetism is a field, not a radiation.  Radiation occurs via photon flow where as a field is created by the movement of electric charge.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 9 years ago in reply to DAB

    " Radiation occurs via photon flow where as a field is created by the movement of electric charge."

     

    Which creates/generates a magnetic field, hence the term electroMAGNETIC radiation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 9 years ago in reply to gdstew

    The jury is still out if electromagnetic waves can be called radiation or just energy transfer.

     

    The emission of photons is explicitly defined as "radiation" as the mass and energy is transferred via discrete objects.

     

    Long wave RF signals tend to use molecules to transfer energy, but not necessarily mass, so I think there is some doubt about using radiation with those frequencies.

     

    Magnetic force/field is just a component of the photon vibration.  It is the mass of the photon that carries the energy.

     

    I know this view is controversial, but it better fits the data and explains why there are still unresolved issues at this level of physics.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 9 years ago in reply to DAB

    The emission of photons is explicitly defined as "radiation" as the mass and energy is transferred via discrete objects.

     

    So is the emission of protons, and neutrons. At least they do actually have mass. But they never travel at the speed of light like photons/electromagnetic waves do.

     

    "Long wave RF signals tend to use molecules to transfer energy, but not necessarily mass, so I think there is some doubt about using radiation with those frequencies."

     

    I'm sorry but OMG are you serious ? They travel through "empty" space as well as as any electromagnetic wave/particle at any frequency does. Please supply all

    data from any experiment that says this is not so or that molecules are required for LW RF to propagate.

     

    "Magnetic force/field is just a component of the photon vibration."

     

    Citation ? And it still "radiates" with the photon.

     

    "It is the mass of the photon that carries the energy"

     

    There is absolutely no experimental data that shows that photons have mass. NONE. That is why they are able to travel at the speed of light. No particle with mass

    has ever been found to do that. They can get close, but no cigar.

     

    "I know this view is controversial, but it better fits the data and explains why there are still unresolved issues at this level of physics."

     

    After well over one hundred years of data from intense scientific experimentation with electromagnetic radiation and particle radiation of all forms that says it doesn't,

    perhaps you could share the "data" you say this hypothesis fits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • lescolliershustoke@virginmedia.com
    lescolliershustoke@virginmedia.com over 9 years ago in reply to gdstew

    Chaps Chaps Chaps, stick to the point I am not interested in what the hell you call it radiation, propagation, distribution, self perpetuation or any other term.

     

    What I want to know is which parameters to adjust to extend the range of a electromagnetic device i.e. a coil with a core.

     

    I would suggest that the permeability of the material would play a big part but none of you have suggested using a material with a higher / better permeability. Is this because I am wrong ??

     

     

    regards

     

     

    Les Collier

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to lescolliershustoke@virginmedia.com

    You can increase power or channel the field.

    To channel the field you need to stay below material saturation.

    We cannot suggest a suitable channeling solution unless we know what the target geometry is.

    What field strength do you need and at what distance?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 9 years ago in reply to lescolliershustoke@virginmedia.com

    You can increase power or channel the field.

    To channel the field you need to stay below material saturation.

    We cannot suggest a suitable channeling solution unless we know what the target geometry is.

    What field strength do you need and at what distance?