Member's Forum How can you manage to damage a soldering iron like this?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 632 subscribers
  • Views 3930 views
  • Users 0 members are here
  • soldering tips
  • soldering iron
  • soldering
Related

How can you manage to damage a soldering iron like this?

cstanton
cstanton over 7 years ago

image

My first thought is, perhaps it's corrosion, from high or excess heat, these are disposable parts after all, but what really contributes to this kind of wear, and is there anything that can be done to prevent it being so sudden or so soon?

 

Often I find the soldering tips in the workstation to be bent, or the end of the tip looking like it's snapped off.

 

What're your thoughts?

How long do tips last for you or how often do you replace them?

What do you use to take care of your soldering iron?

  • Sign in to reply
  • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to cstanton

    Did someone switch it with their worn home tip? You’d need a grinder to get it worn like that in a few months.

    It would also explain why it’s actually a tip with a different profile (also spotted by others in this chat) even though you mounted two identical ones.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to 14rhb

    Only that they were used in my local Hackspace over the period of about a month at least, a few months at most. No idea how they were being used, or who particularly.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to 14rhb

    Looks like it would fit in the chuck of my electric drill OK which would reduce the stress of using it with the soldering iron for a handle  image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to fmilburn

    For fixings like this when you can't find the proper driver?

     

    image

    PS: I do know the real answer but will leave it to dougw as it is his soldering iron selection image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to dougw

    What is the strange tip with two bumps on the edges used for?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago in reply to cstanton

    Does this mean you know a bit more history on where they were both used and by who? I'd be interested to hear the end users' stories on this.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to rsc

    > That tip may have started out that short

    It's the same tip.. I know, because I bought them both and fitted them D:

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to dougw

    dougw  wrote:

     

    ...

    Some of the tips have a worn spot that doesn't "wet" with solder well but I don't throw them out ...

    For those cases, I use these two:

    image

    As you can see, I don't use it often. Only when I create spots that don't wet (typically when melting a connector away with the iron because "it needs to go" image )

    The polish bar and activator are not to be used when the tip is OK. They are not maintenance utilities, but repair. They have downsides.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago

    Pictures really tell a lot in a thread like this so here are my irons and a collection of old tips:

    image

    The Aoyue is the iron part of my hot air rework station - I don't use the iron part much, because it isn't as good as the Hakko I use most of the time (I didn't bring the whole Hakko over for the picture).

    The blue tip in the middle is the one I am currently using in the Hakko.

    The Tenma is new, courtesy of element14 - only used in my camera area so far.

    The Yong Feng looks unused because it is - I bought it for $12 - it might see some use for mobile work since the temperature control is in the handle, eliminating the big controller block.

    Some of the tips have a worn spot that doesn't "wet" with solder well but I don't throw them out in case I want to use them for melting PLA or hot glue or some other application that would mess up a nice tip.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to shabaz

    Here's a customer action photo of my irons.

     

    The top one is unregulated, bought when I was at school (I guess '83). It's only be used with leaded solder. Has seen a lot of use.

    The lower one is 2 years old, regulated. I use it with unleaded solder - 350-380 °C. Also seen a lot of use.

     

    image

    My very first iron, an Archer, suffered from tip damage (there was a hole eaten into that one - that actually happened very fast image). Since then I never had structural damage to an iron.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
<>