Member's Forum Switching with transistor versus relay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 632 subscribers
  • Views 2607 views
  • Users 0 members are here
  • halloween ideas
  • relays
  • transistors
  • halloween project
  • motion sensors
Related

Switching with transistor versus relay

jgrub
jgrub over 6 years ago

Element14 has a great YouTube vid on transistors, and I get that transistors are faster than relays and are better in low voltage situations. But I've been trying to custom build a motion sensor that remotely turns on the motor of an animatronic prop. It should be easy enough to activate that motor from the collector side of my transistor. 

 

But because the prop is a distance away (maybe 5-6 feet), it has it's own power supply and a separate ground. All I really need is something to close the circuit on the ground side of the prop motor. So it seems to me that two wires from the prop to a remote relay, NOT a transistor C/E connection, would make more sense. The activated motion sensor would send 3.3v to the relay. Then the relay connects the two wires together and that completes the motor circuit.

 

I've been trying to do this with a transistor switch for days and can not figure out what I should be connecting to the motor two wires.

 

Has anyone else tried to rig a simple remote switch like this? (Halloween props typically use foot pads that complete the circuit in a similar but highly mechanical way.)

  • Sign in to reply
  • Cancel
Parents
  • jgrub
    jgrub over 6 years ago

    Great input, guys! I worked on my diagrams this morning and here they are:

    image

    The left-hand image shows you my motion detector (with the project box drawn around it for placement of access holes). The sole purpose of the LED is to dimly light the interior of the box to show that the power is on. Hence the very high value resistor. Note that, at the bottom of the left-hand diagram, I have two wires coming out to the right-hand diagram. The left-hand model is my trigger (HC-SR501) and my switch (2N3904). I'm trying to use it like a simple relay to connect the right-hand circuit to ground.

     

    The right-hand image is what's inside my Halloween prop (a hanging zombie). The motor is weighted so as to vibrate the prop. Then I have two LEDs for lighting up its eyes. It's powered by a 6vdc adapter that plugs into 120vac. The slide switch is SPDT so that I can turn it ON (constant on), OFF, or set it to get its completed connection (to ground) from the trigger/switch on the left. All components of both halves of this project appear to work fine. My issue is how to connect them to each other to just create a simple grounding -- or circuit completion -- on the right side. I have a shipment of relays coming today, but would still like to solve the transistor issue, simply because it's an obvious gap in my knowledge.

     

    FRANK, I mentioned the foot pad just to indicate what these props usually use if they don't have an on-body sensor. My hope to replace the unreliable (and too small) foot pads with these little sensor boxes (left-hand diagram) that can simply plug into the foot pad socket of the prop and then be mounted strategically.

     

    BTW, this is an ongoing project for a haunted house that my son creates every year. Hoping to come up with some cool monsters to help him expand that. 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jgrub
    jgrub over 6 years ago

    Great input, guys! I worked on my diagrams this morning and here they are:

    image

    The left-hand image shows you my motion detector (with the project box drawn around it for placement of access holes). The sole purpose of the LED is to dimly light the interior of the box to show that the power is on. Hence the very high value resistor. Note that, at the bottom of the left-hand diagram, I have two wires coming out to the right-hand diagram. The left-hand model is my trigger (HC-SR501) and my switch (2N3904). I'm trying to use it like a simple relay to connect the right-hand circuit to ground.

     

    The right-hand image is what's inside my Halloween prop (a hanging zombie). The motor is weighted so as to vibrate the prop. Then I have two LEDs for lighting up its eyes. It's powered by a 6vdc adapter that plugs into 120vac. The slide switch is SPDT so that I can turn it ON (constant on), OFF, or set it to get its completed connection (to ground) from the trigger/switch on the left. All components of both halves of this project appear to work fine. My issue is how to connect them to each other to just create a simple grounding -- or circuit completion -- on the right side. I have a shipment of relays coming today, but would still like to solve the transistor issue, simply because it's an obvious gap in my knowledge.

     

    FRANK, I mentioned the foot pad just to indicate what these props usually use if they don't have an on-body sensor. My hope to replace the unreliable (and too small) foot pads with these little sensor boxes (left-hand diagram) that can simply plug into the foot pad socket of the prop and then be mounted strategically.

     

    BTW, this is an ongoing project for a haunted house that my son creates every year. Hoping to come up with some cool monsters to help him expand that. 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • genebren
    genebren over 6 years ago in reply to jgrub

    Joe,

     

    I would suspect that you need a more complete path for the Ibe current to flow.  At present the path from the PIR through the base-emitter junction is not complete.  There needs to be a path from the emitter to ground (common to the PIR output) in order for current to flow through the base-emitter junction, allowing current to flow through the collector-emitter junction.  By connecting the emitter of the transistor to the ground connected to the PIR sensor, you should be able to complete this path.

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to jgrub

    That looks like a fun project.  I am away from home and pecking on my tablet but a couple of thoughts...

     

    * you need the diode for sure

    * it may be better to use a logic level MOSFET - the transistor amplifies current and I don’t know what the PIR can deliver and there is a 1k resistor.  I have always read PIR output with a microcontroller.

    * a quick look at the 2N3904 in a TO-92 package indicates it is only good for 200 mA and your motor can draw 2 A.

    * what current are your LEDs rated for?  Don’t think they will work on the prop side as shown but I am unable to mark your schematic up.  100k is going to make a very dim LED on the other side.

     

    Hopefully shabaz or dougw can have another look otherwise I will look again when I get home

    • Cancel
    • Vote Up +7 Vote Down