• Products and Partners
    Products and Partners
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
Member's Forum Switching with transistor versus relay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 632 subscribers
  • Views 2645 views
  • Users 0 members are here
  • halloween ideas
  • relays
  • transistors
  • halloween project
  • motion sensors
Related

Switching with transistor versus relay

jgrub
jgrub over 7 years ago

Element14 has a great YouTube vid on transistors, and I get that transistors are faster than relays and are better in low voltage situations. But I've been trying to custom build a motion sensor that remotely turns on the motor of an animatronic prop. It should be easy enough to activate that motor from the collector side of my transistor. 

 

But because the prop is a distance away (maybe 5-6 feet), it has it's own power supply and a separate ground. All I really need is something to close the circuit on the ground side of the prop motor. So it seems to me that two wires from the prop to a remote relay, NOT a transistor C/E connection, would make more sense. The activated motion sensor would send 3.3v to the relay. Then the relay connects the two wires together and that completes the motor circuit.

 

I've been trying to do this with a transistor switch for days and can not figure out what I should be connecting to the motor two wires.

 

Has anyone else tried to rig a simple remote switch like this? (Halloween props typically use foot pads that complete the circuit in a similar but highly mechanical way.)

  • Sign in to reply
  • Cancel
Parents
  • jgrub
    jgrub over 7 years ago

    Once again, thanks to all for a great discussion about transistors versus relays, as well as specifics about how my circuitry needs to improve. I will still plow forward with the transistor method, but only as an exercise to broaden my knowledge. 14rhb made a great point about low periodicity, thus swaying my decision to the relay route. I received my relays the other day and saw no problem in eliminating(!) several components (including my ultra-dim ON-indicator LED, as the relay board has two such LEDs). In total, I now have just three components (sensor board, relay board and 9V battery) and several screw connections versus solder connections. As a mass-manufacturing exercise, this option is way more expensive than the transistor version. As a one-off "gadget" of which I will probably make about a dozen of them, the relay version is a quick, reliable and durable solution. I look forward to posting a short video here of the prop and sensor in action.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 7 years ago in reply to jgrub

    Joe,

     

    Good that you have a path forward (relay) and path for the future/knowledge (transistor).  I thinking more about your plans and the scale of the motor (small vibrator), another approach that you might want to consider is a small solid-state relay.  This is very similar to your transistor approach, but something that might eliminate some design variables.  Something like https://www.newark.com/clare/cpc1002n/relay-solid-state/dp/03M7309?st=CPC1002  would give you the ability to switch up to 700mA of load, with no mechanical contacts (less cost, wear, etc.).  This could be connected to the output of your PIR, with a current limiting resistor inline and the output side could be used to complete the current path (much like your relay), with no need to tie the ground together.

     

    Just a note, be careful that the PIR has sufficient current output to drive your relay.  If the relay requires a higher current than the PIR can provide, you might need a driver between the PIR and the relay.  Also, be sure to add a protection diode to avoid damaging you PIR with the high voltage spike associated with the magnetic field collapse as the relay is switched off.

     

    Good luck!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 7 years ago in reply to jgrub

    Joe,

     

    Good that you have a path forward (relay) and path for the future/knowledge (transistor).  I thinking more about your plans and the scale of the motor (small vibrator), another approach that you might want to consider is a small solid-state relay.  This is very similar to your transistor approach, but something that might eliminate some design variables.  Something like https://www.newark.com/clare/cpc1002n/relay-solid-state/dp/03M7309?st=CPC1002  would give you the ability to switch up to 700mA of load, with no mechanical contacts (less cost, wear, etc.).  This could be connected to the output of your PIR, with a current limiting resistor inline and the output side could be used to complete the current path (much like your relay), with no need to tie the ground together.

     

    Just a note, be careful that the PIR has sufficient current output to drive your relay.  If the relay requires a higher current than the PIR can provide, you might need a driver between the PIR and the relay.  Also, be sure to add a protection diode to avoid damaging you PIR with the high voltage spike associated with the magnetic field collapse as the relay is switched off.

     

    Good luck!

    Gene