Member's Forum Switching with transistor versus relay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 632 subscribers
  • Views 2591 views
  • Users 0 members are here
  • halloween ideas
  • relays
  • transistors
  • halloween project
  • motion sensors
Related

Switching with transistor versus relay

jgrub
jgrub over 6 years ago

Element14 has a great YouTube vid on transistors, and I get that transistors are faster than relays and are better in low voltage situations. But I've been trying to custom build a motion sensor that remotely turns on the motor of an animatronic prop. It should be easy enough to activate that motor from the collector side of my transistor. 

 

But because the prop is a distance away (maybe 5-6 feet), it has it's own power supply and a separate ground. All I really need is something to close the circuit on the ground side of the prop motor. So it seems to me that two wires from the prop to a remote relay, NOT a transistor C/E connection, would make more sense. The activated motion sensor would send 3.3v to the relay. Then the relay connects the two wires together and that completes the motor circuit.

 

I've been trying to do this with a transistor switch for days and can not figure out what I should be connecting to the motor two wires.

 

Has anyone else tried to rig a simple remote switch like this? (Halloween props typically use foot pads that complete the circuit in a similar but highly mechanical way.)

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 6 years ago

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jgrub
    jgrub over 6 years ago in reply to dougw

    Douglas,thanks for this. As I study the configuration, it looks a lot like what I already have (except for the protective diode, which I need to add), except that you've placed the transistor and resistor in the motor "assembly", whereas I've placed them in the sensor "assembly". But wiring looks essentially identical, i.e. current flows from the motor to the collector, while the emitter goes to the negative side of the power source (or ground).

     

    As I'm very rusty at this, can you verify my observation? Or maybe I'm not seeing something else? Thanks!

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jgrub
    jgrub over 6 years ago in reply to dougw

    Douglas,thanks for this. As I study the configuration, it looks a lot like what I already have (except for the protective diode, which I need to add), except that you've placed the transistor and resistor in the motor "assembly", whereas I've placed them in the sensor "assembly". But wiring looks essentially identical, i.e. current flows from the motor to the collector, while the emitter goes to the negative side of the power source (or ground).

     

    As I'm very rusty at this, can you verify my observation? Or maybe I'm not seeing something else? Thanks!

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jgrub
    jgrub over 6 years ago in reply to jw0752

    Well, at least you concur. image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 6 years ago in reply to jgrub

    Hi Joe,

    the big difference in your schematic and that of Doug was that you did not have the emitter of your transistor tied to the ground image of the PIR control module. Without this connection the emitter base circuit would not be able to produce a current flow and the transistor could not turn on.

     

    John

     

    EDIT> Seems that I should have read Gene's post before I jumped in.

     

    Shutting up now, with a red face.

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 6 years ago in reply to jgrub

    I just linked the first schematic that illustrates how a transistor can be hooked up to drive a motor. As fmilburn points out you need a transistor that can handle the load, maybe a TIP120 or a big FET like an IRL520 as Frank mentioned. If the power dissipated in the transistor is over about .3 Watts you will need a heatsink on the transistor.

    • Cancel
    • Vote Up +6 Vote Down