Member's Forum Switching with transistor versus relay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 632 subscribers
  • Views 2598 views
  • Users 0 members are here
  • halloween ideas
  • relays
  • transistors
  • halloween project
  • motion sensors
Related

Switching with transistor versus relay

jgrub
jgrub over 6 years ago

Element14 has a great YouTube vid on transistors, and I get that transistors are faster than relays and are better in low voltage situations. But I've been trying to custom build a motion sensor that remotely turns on the motor of an animatronic prop. It should be easy enough to activate that motor from the collector side of my transistor. 

 

But because the prop is a distance away (maybe 5-6 feet), it has it's own power supply and a separate ground. All I really need is something to close the circuit on the ground side of the prop motor. So it seems to me that two wires from the prop to a remote relay, NOT a transistor C/E connection, would make more sense. The activated motion sensor would send 3.3v to the relay. Then the relay connects the two wires together and that completes the motor circuit.

 

I've been trying to do this with a transistor switch for days and can not figure out what I should be connecting to the motor two wires.

 

Has anyone else tried to rig a simple remote switch like this? (Halloween props typically use foot pads that complete the circuit in a similar but highly mechanical way.)

  • Sign in to reply
  • Cancel
  • jgrub
    jgrub over 6 years ago

    Great input, guys! I worked on my diagrams this morning and here they are:

    image

    The left-hand image shows you my motion detector (with the project box drawn around it for placement of access holes). The sole purpose of the LED is to dimly light the interior of the box to show that the power is on. Hence the very high value resistor. Note that, at the bottom of the left-hand diagram, I have two wires coming out to the right-hand diagram. The left-hand model is my trigger (HC-SR501) and my switch (2N3904). I'm trying to use it like a simple relay to connect the right-hand circuit to ground.

     

    The right-hand image is what's inside my Halloween prop (a hanging zombie). The motor is weighted so as to vibrate the prop. Then I have two LEDs for lighting up its eyes. It's powered by a 6vdc adapter that plugs into 120vac. The slide switch is SPDT so that I can turn it ON (constant on), OFF, or set it to get its completed connection (to ground) from the trigger/switch on the left. All components of both halves of this project appear to work fine. My issue is how to connect them to each other to just create a simple grounding -- or circuit completion -- on the right side. I have a shipment of relays coming today, but would still like to solve the transistor issue, simply because it's an obvious gap in my knowledge.

     

    FRANK, I mentioned the foot pad just to indicate what these props usually use if they don't have an on-body sensor. My hope to replace the unreliable (and too small) foot pads with these little sensor boxes (left-hand diagram) that can simply plug into the foot pad socket of the prop and then be mounted strategically.

     

    BTW, this is an ongoing project for a haunted house that my son creates every year. Hoping to come up with some cool monsters to help him expand that. 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago

    Hi Joe,

     

    Also, really a transistor is not a switch, but consists of semiconductor junctions that have switch-like behavour, within certain parameters, from a birds-eye view. From a closer view, that switch-like behaviour might or might not be suitable for the application.

    One thing that could affect the choice, is the motor requirements (current consumption). If that is low, then you may be fine using the transistor, but as you can see in Frank's circuit, a diode is also needed, because the transistor switch is fragile in some ways too. Also, motors demand more current when loaded, so that needs to be considered too.

     

    If the current consumption is high, then you may need to use a relay, but that may entail using the transistor too, because the 3.3V output from the motion sensor may not have the current drive to directly control the relay. It depends on the sensor output.

    So basically some more information is needed, or will need to be checked (motion sensor output capability, motor current requirement and voltage.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • fmilburn
    fmilburn over 6 years ago

    Hi Joe,

     

    Can you post a simple schematic with the transistor part number and how you have wired it up?  For a simple example of a microcontroller controlling a DC motor with a transistor in a Halloween costume see this post:  LadyBug Girl and Rocket Boy .  The schematic with the motor is near the bottom of the post.  If a foot pad will be used for a switch then it is not clear that a relay or transistor is needed at all.

     

    Frank

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
<