• Products and Partners
    Products and Partners
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
Member's Forum Weather satellite images
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 632 subscribers
  • Views 2272 views
  • Users 0 members are here
Related

Weather satellite images

neuromodulator
neuromodulator over 7 years ago

There are a couple of weather satellites that continuously transmit unencrypted images and data back to earth. Some are geostationary like the GOES satellites, and some have polar orbits like the NOOA and Meteor satellites. With right equipment it is possible capture, demodulate and decode the data transmitted by these satellites. Meteor satellites are russian, and currently 2 of them are operational (Meteor M N2 (More info) and Meteor M N2-2 (More info)). As it can be seen in the links, these satellites transmit at different bands through different protocols/services, one of them is the Low-Rate Picture Transmission (LRPT), which is transmitted at 137.1 and 137.9 MHz (Wikipedia link). LRPT uses QPSK and OQPSK modulation (Wikipedia link) and Reed-Solomon (Wikipedia link) forward error correction. Forward error correction allows the receiver to the "fix" corrupted data, allowing in this way the reception of data at a lower SNR.

 

There are many hardware alternatives to receive the data, I used an Ettus B200 SDR with a hand-tracked rabbits ear antenna. I used HDSDR to record the signal, SDR# with a meteor demodulator plugin to demodulate it, Medet to decode it, and "Smooth Meteor" to "correct" the image (compensate for the distortion caused by the earth spherical form). Here is an example of what I was able to receive:

 

image

  • Sign in to reply
  • Cancel
Parents
  • 14rhb
    14rhb over 7 years ago

    That is awesome work neuromodulator such a clear and detailed image. I've got a cheap SDR that I might be able to use Software Defined Radio (SDR) - My First Design or do you think it is too low-specification?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • 14rhb
    14rhb over 7 years ago

    That is awesome work neuromodulator such a clear and detailed image. I've got a cheap SDR that I might be able to use Software Defined Radio (SDR) - My First Design or do you think it is too low-specification?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • neuromodulator
    neuromodulator over 7 years ago in reply to 14rhb

    It should be enough, what kind of antennas do you have? What you will also need is a satellite tracking app or webpage (check these links: Meteor M2, Meteor M2-2) to check the time when the sat will pass over your location and start capturing. These sats have a period of around 100 min and you got around 15 mins to capture their transmission. The higher the elevation the sat will reach when it passes, the better, try to look for elevations over 45°. You can also try to capture NOAA-15, 18 and 19 sats, they transmit at 137 Mhz too, the images are lower res and they require higher SNR to get crystal clear images, but considering the short time period you have to capture a sat signal, you can use those sats to tune your rig while you wait for Meteor sats. If you can, try to look for a place with low RF contamination and high visibility, cities are usually not the best place to capture these weak signals.

    • Cancel
    • Vote Up +5 Vote Down