• Products and Partners
    Products and Partners
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
Member's Forum Breadboarding a must
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 632 subscribers
  • Views 3316 views
  • Users 0 members are here
Related

Breadboarding a must

Andrew J
Andrew J over 6 years ago

Really, you gotta breadboard, right?

 

image

This is a logic-driven game of snap, but with dice rather than cards.  It uses a XNOR!  If I remember correctly, that sketch on the post-it was for detecting and determining a match on the two LED die, turning on a player's led if they pressed the button correctly before the other player (and not if they didn't.)  I'd post a circuit diagram but about 1/4 of this is Charles Platt's work not mine so I don't feel it would be right.  I just came across the photo today and thought it was quite impressive - I keep thinking of going back to it and actually building it up and encasing.  It actually drove one of my very first questions on Element14 - I'd used an open-drain XNOR and didn't understand why it wasn't working.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 6 years ago

    Hi Andrew,

     

    That's very cool. especially the offshoot breadboard that occurred halfway in the design : )

    At my first workplace, I too saw an entire product laid out like this, but on solder proto-boards and on pieces of copper-clad, in a long line that spanned a table : )

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 6 years ago in reply to shabaz

    Actually, the 'offshoot' is the start of the circuit - I laid the others out perpendicularly so that both players would sit opposite each other.  It regulates 9V/12V down to 5V and a 555 timer is used to rapidly cycle a signal through a number of logic chips to drive the two banks of LEDs from 1 to 6, so fast that they all look turned on.  Randomisation comes purely from speed and the fact that holding a button down for a duration is non-repeatable by a human.  The other boards have logic to determine whether the two banks match and who pressed the 'snap' button first and to lock the other player out.  I recall I was going to automatically increase the score if a player was correct but I ran out of hook up wire, so that bit is purely manual in the setup above!  I did work out how to debounce the button presses, to prevent multiple scores being registered, using a capacitor rather than a Schmitt trigger or other logic chip (I was running out of those too) image 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 6 years ago in reply to shabaz

    Actually, the 'offshoot' is the start of the circuit - I laid the others out perpendicularly so that both players would sit opposite each other.  It regulates 9V/12V down to 5V and a 555 timer is used to rapidly cycle a signal through a number of logic chips to drive the two banks of LEDs from 1 to 6, so fast that they all look turned on.  Randomisation comes purely from speed and the fact that holding a button down for a duration is non-repeatable by a human.  The other boards have logic to determine whether the two banks match and who pressed the 'snap' button first and to lock the other player out.  I recall I was going to automatically increase the score if a player was correct but I ran out of hook up wire, so that bit is purely manual in the setup above!  I did work out how to debounce the button presses, to prevent multiple scores being registered, using a capacitor rather than a Schmitt trigger or other logic chip (I was running out of those too) image 

    • Cancel
    • Vote Up +5 Vote Down