• Products and Partners
    Products and Partners
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
Member's Forum Breadboarding a must
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 632 subscribers
  • Views 3311 views
  • Users 0 members are here
Related

Breadboarding a must

Andrew J
Andrew J over 6 years ago

Really, you gotta breadboard, right?

 

image

This is a logic-driven game of snap, but with dice rather than cards.  It uses a XNOR!  If I remember correctly, that sketch on the post-it was for detecting and determining a match on the two LED die, turning on a player's led if they pressed the button correctly before the other player (and not if they didn't.)  I'd post a circuit diagram but about 1/4 of this is Charles Platt's work not mine so I don't feel it would be right.  I just came across the photo today and thought it was quite impressive - I keep thinking of going back to it and actually building it up and encasing.  It actually drove one of my very first questions on Element14 - I'd used an open-drain XNOR and didn't understand why it wasn't working.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 6 years ago

    I've never been a bread-boarder - don't even own one !

     

    In the past I've done a fair bit with Veroboard (strip-board if you prefer) and I still use that occasionally.

     

    Normally I do simulation (logic in VHDL which will end up on an FPGA and analogue in LTSpice ) and then straight to pcb.

     

    Stuff that will work on bread-board will usually simulate nicely. Fancy analogue and switching or high power analogue don't work well on bread-board (and can be tricky in simulation).

     

    BTW, if you don't like LTSpice then you can now get MicroCap for free - it was a quite well thought of paid for simulator - now it's a free download at http://www.spectrum-soft.com

     

    This is a typical bread-board unfriendly device - it's a 2ns pulse stretcher with adjustable input threshold - simulates OK and works on a pcb but would not be feasible in other formats.

     

    None of the chips I want to use come in DIP any more image

     

    image

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 6 years ago in reply to michaelkellett

    It does seem that more and more chips are SMD only and the adaptors to use aren’t particularly cheap - I’ve thought it would be useful to cram them into spare PCB space when getting one manufactured.  At the time I created the above, breadboards, hook up wire and DIP chips/TH parts were all I had.  And a 9V/12V wall wart to drive them.

     

    I downloaded Microcap a week or so ago but haven’t had chance to play with it yet.  I find LTSpice “OK” but the UI leaves a lot to be desired on the mac.  There’s nothing intuitive about it so I’ve found features purely through serendipity than active knowledge.

     

    Where I am in my knowledge, I think breadboarding is useful for just trying things out, measuring them and playing around.  Even simple things like an RC circuit.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    Even using SMD adapter/proto-boards is time-consuming, sometimes it's easier to go from simulating straight to a PCB. But occasionally for single-chip experiments, I'll use a proto-board, I did try to create a general one to save a bit of money, I'm not sure how useful it is to others since it is mostly personal preferences on the design, but I'm happy to put the gerber files somewhere if anyone wants it. The boards need cutting, there's no bite-marks or anything to split them.

    I'm running low on these layouts (ten of these boards lasted a few years), I need to re-order them too. It's not a great board on balance, because some of the layouts were not useful, e.g. the QFN one at the bottom row, is not helpful because there are so many variants of QFN that it's unlikely to be right for any occasion. Also the bottom-right one with USB and DC jack isn't that useful, it's cheaper to buy USB sockets pre-soldered on boards.

    The only ones I've used a lot, are the top left style (repeated on the bottom row too) which is SOIC up to 20 pins, and the one next to it which can handle SSOP, and the middle row (orange arrow) which handles SOT-23, or the larger SMD 3-pin regulators.

    What worked really well was that the layouts have a ground area (green arrow) underneath, so any pin on the IC can be connected to 0V by running uninsulated wire from a hole to the underside and folding it over into the ground area (there's no solder mask there). Also another thing that worked well was that there are long stretches on each pin with no solder mask (red arrow) where 0603 parts can be soldered across pins for instance.

    The top-right layout was intended for interfacing flat flex, I've used that layout rarely since for circuits with flat flex it is likely I may have a PCB anyway.

    image

    Here's an example of the top-left board with a SOIC-8 chip, you can see the straddled components etc. For series components, I'll cut the trace with a scalpel The centre is ground, connected to the underside. Wires held in place with araldite : )

    image

    An example, showing the SOT-23 and DC jack boards:

    image

    Underside of a few random boards, you can see how bare wires were run into the centre ground:

    image

    It's all a bit crude : ) A sheet of copper-clad can be handy too, as a base and ground plane.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 6 years ago in reply to shabaz

    There's some good ideas in there though, even if you don't use them so much - making multisize ones rather than footprint specific for example.  You've not had any issues with shorting the top and bottom layers when cutting them I guess otherwise you would have mentioned it.  I have gone straight from design/simulation to PCB but I've paid the price on a couple of occasions - it can turn out expensive, e.g. getting 4 layer PCBs fast delivered only to find the inductor footprint was completely wrong.  That was £60 or so I won't be seeing again!! 

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 6 years ago in reply to shabaz

    There's some good ideas in there though, even if you don't use them so much - making multisize ones rather than footprint specific for example.  You've not had any issues with shorting the top and bottom layers when cutting them I guess otherwise you would have mentioned it.  I have gone straight from design/simulation to PCB but I've paid the price on a couple of occasions - it can turn out expensive, e.g. getting 4 layer PCBs fast delivered only to find the inductor footprint was completely wrong.  That was £60 or so I won't be seeing again!! 

    • Cancel
    • Vote Up +5 Vote Down