• Products and Partners
    Products and Partners
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
Member's Forum Diagnosis: GameBoy Advance SP - No Audio
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 631 subscribers
  • Views 1323 views
  • Users 0 members are here
  • audio
  • gameboy advance sp
  • gameboy
  • advance sp
Related

Diagnosis: GameBoy Advance SP - No Audio

cstanton
cstanton over 6 years ago

imageimage

 

The GameBoy Advance SP works, however there's no audio from the speaker, the SP was different from the Advance in that there's no 3.5mm headphone jack either so I can't easily compare/check it.

 

What're the steps I can take to start diagnosing this and where the problem is? I'm not familiar with using an oscilloscope if necessary, though I have a bitscope one I could try to work out how to use. I'm not seeing any physical problems.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 6 years ago

    Hi Christopher,

     

    The speaker can be checked with a multimeter set to ohms, just to confirm it is ok (should be 100 ohm or lower resistance across the terminals of it) and just confirm it's still soldered or pressed fine onto the board (using the multimeter set to ohms and check the connections on the track if possible, or visually inspect that the speaker is still making good contact with the board).

    Is there a volume control/slider/switch or anything? If so, those can sometimes fail. There a post here which talks about four solder connections on switches could be the issue:

    https://gbatemp.net/threads/gba-sp-sound-not-working.468232/

     

    For a sound issue, a crystal earpiece is really handy, you can move it around various points on the board, with no risk of damaging anything because the earpiece has a very high resistance so it doesn't load the circuit.

    However, you might not need that, if the issue is solved by the other suggestions above. A 'scope can be used for that too but again I don't think it will be necessary initially.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 6 years ago in reply to shabaz

    Finally found batteries for my multimeter...

     

    7.6ohms across the speaker, appears to make good contact with the PCB (it's stuck to the board with weak glue and prongs make contact). No sound still.

     

    There's a volume slider, it has 6 solder points and those are very secure to the PCB.

     

    I don't have a crystal earpiece or another way of testing the speaker at the moment.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to cstanton

    Oh, hoped it would have been an easy thing with some failed contacts : (

    The analogue channel on the bitscope could be used, by powering up the unit with a game installed and if it is known that sound should be playing for the game.

    The contacts near the volume slider would need to be probed (with the bitscope ground connection connected to the battery negative contact), and the 'scope set to approx. 1 msec/division or thereabouts, and 0.5 or 1 V/div. Also, probing near any small chip or capacitors that may be part of the audio amplifier circuitry, it could be physically between the speaker and the volume control area, just to spot if the audio signal is detected. There appear to be lots of 3-pin SOT-23 sized parts and some capacitors in that area from the photo, so that might be the amplifier. Probing on the capacitors would be worth trying, and if audio does get spotted in that area, then maybe reheating some of the parts there could fix it (in case a solder joint has lifted due to button-presses flexing the board maybe.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 6 years ago in reply to cstanton

    Oh, hoped it would have been an easy thing with some failed contacts : (

    The analogue channel on the bitscope could be used, by powering up the unit with a game installed and if it is known that sound should be playing for the game.

    The contacts near the volume slider would need to be probed (with the bitscope ground connection connected to the battery negative contact), and the 'scope set to approx. 1 msec/division or thereabouts, and 0.5 or 1 V/div. Also, probing near any small chip or capacitors that may be part of the audio amplifier circuitry, it could be physically between the speaker and the volume control area, just to spot if the audio signal is detected. There appear to be lots of 3-pin SOT-23 sized parts and some capacitors in that area from the photo, so that might be the amplifier. Probing on the capacitors would be worth trying, and if audio does get spotted in that area, then maybe reheating some of the parts there could fix it (in case a solder joint has lifted due to button-presses flexing the board maybe.