The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.
The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.
I worked at Mostek maintaining the Fairchild Sentry testers used to test the Z80s when they first began to manufacturer them. The second computer I every
built (parts, pcb, solder) was the SDB-80 which was the Mostek Software Development Board for the Z80 with 16K bytes (8 - MK4116 16K bit) dynamic RAMs
which Mostek also made. The first wire wrap board I ever made was a 48K byte dynamic RAM board also using MK4116s that worked with the SDB-80. I can
tell you there were a bunch of happy technicians when we were told that Mostek would be second sourcing the Z-80 and even happier when we were told we
could buy SDB-80 kits and build them ourselves! Those were really fun days. I still have a Zilog Z80 in a ceramic package that says it was manufactured in
Dallas even though Mostek was actually in Carrollton a suburb in Dallas County just north of north-west Dallas.
Wow! that's amazing that you got such a large DRAM board working with Wire-wrap.
Do you still have any photos or schematics of it?
It was quite rare to come across Mostek parts in Australia. We usually got Zilog, SGS and Sharp.
And from memory the SGS parts didn't support the undocumented instructions.
Hi COMPACT and Doug,
While the PC-1600 just didn't take off in the second half of the eighties, Sharp out of the blue discontinued the whole PC-1500A line. Among the
large number of commercial users worldwide with business application programs, one company especially had a huge practical problem with that:
Allianz, Germany's largest insurance company. They had abt. 50.000 (no typo !) PC-1500A systems for their commercial field service - now to be
written off just like that !
An other, very small, German company, having invested heavily in a rather unique application, decided, they could perhaps ensure continuity by
purchasing several dozen used systems from Allianz. Thus in the aftermath of the PC-1500A era a remarkable opportunity presented itself for us
(i.e. me and my son). Weilekes also was a father & son operation, who had devised a corrosion testing system for oil and gas pipes, to be used
in Siberia. The PC-1500A system was choosen because of its virtual indestructability and reliability in harsh environments. If anything, the mate
to the pocket computer - in fact a tiny 4-color plotter with system I/F - had to be overhauled meticulously. And that's where we came in.
My son (15 at the time) had already done so with several of these cigarette-pack size little gems*. Next the NiCad pack had to be exchanged for
a 'real' Sanyo (ask any model 'copter builder !). PC-1500A got a new keyboard switch mat, and any worn-out keys were replaced**. Refurbishing
further included all connectors, scratched LCD windows - sometimes complete cases were replaced.
Together with the Weilekes custom unit, the pocket computer + plotter were built into a special sort of cradle that the user wore like a candy seller
in a movie theatre; except this one had to shield the equipment from Siberian climate ... Sensors connected to the cradle were used for the actual
measurements. I believe these were basically resistance measurements - not surprisingly, taking into account the prominent position of German
developpers in skin resistance measuring medical devices.
What puzzles me now (was'nt aware of this then): both the former Soviet Union, and Hungary produced their own PC-1500A clone at the time;
wasn't Gazprom aware, or didn't they care ...?
Cheers
Ray
*of the Japanese ALPS brand, these days famous a.o. for its high-end audio-grade potentiometers
**Sharp spare part sets with only the [SPACE] and [ENTER] keys came in very handy indeed
Thanks for your explanation and friendly comment, Doug !
I will certainly share my story in this blog, but hope you don't mind me waiting a bit for COMPACT to react ?
Btw, I've always been intrigued by the Friends-Amis story in connection with Matsushita Corp., leading to the development of the HHC.
Although based on the 6502 microprocessor, the resemblance to the design of the SHARP PC-1500 (including bay with peripheral) is
striking. The idea behind it may have been original, but just assuming that Matsushita had no knowledge of the earlier presented SHARP
pocket seems a case of blind faith.
Apart from that, European companies, Olivetti and Nixdorf, should be included in stories about the history of the development from calculators
to handhelds i.m.o.
Cheers
Ray
You can create your own blog on any topic just by clicking on the "Create" button at the top of the page.
Threads like this Z80 topic just fade from view unless members keep adding anecdotes, so I think it is great to add stories directly to the thread, even if they are only peripherally related.
Hi COMPACT,
May I add another PC-1500A project story in response to your earlier interest, and present that, assuming you have also read my posts to Shabaz ?
(It would be boring i.m.o. to tell intertwined stories to two forum members, as if they didn't read each others 'incoming' posts, wouldn't it ?)
This story unfolded in the aftermath of PC-1500A's demise - ending in the permafrost of Siberia ...
As the story hasn't anything to do per se with Z80, does it interest you, and would it be acceptable in this thread ?
Would appreciate hearing from you
Cheers
Ray
Hi Shabaz,
As Appendices at the end of the 276 page PC-1600 Tech Ref Manual I found mnemonics, op-codes, and what have you of both the SC- and the
LH-processor. Not my cup of thea, really ... But maybe someone else finds the clues, required to answer the question: was LH-5801/3 a Z80
derivative, or not ?
For me Chapter 7 is much more evocative, and it confirms my belief all along, that not only 'Ol Blue Eyes did everything "My Way" ...
It is quite impressive what Sharp has integrated on-chip*, next to the processor 'core' - this goes for the Z80A derivative, as well as for the LH.
I've called what they have packed into this pocketcomputer "no mean feat". If you look at the features, you can say that again:
- 3 microprocessors, two 8-bit main CPUs (one emulating the PC-1500A a.o.) + one 4-bit subprocessor (I/O)
- 3 x 36 kB ROM
- RS-232C I/F
- serial optical I/F, 38.4 kbaud
- analog input (ADC)
- automatic power off with external wake-up from peripheral
- floppy and RAM-disk options
- 60-pin fully programmable system/expansion bus output
- 2 memory module slots
Impressive ? Sure ! A joy to work with (as a programmer or a user) ? Not really ... And that's a shame.
PC-1600 has never been able to replace PC-1500A in the market, possibly because it became the victim of its own over-complexity ?
At the time (mid eighties and on) Sharp had already her organizer concept ready, later shared in the PDA concept with Apple (Newton),
and so probably didn't care too much ... (PC-12xx, 14xx, E200, and E500 series thriving)
Cheers
Ray
* a.o. the complete port processor, LH-5811, of PC-1500 in the SC main CPU
Hi Ray,
It could be derived from the Z80, I really cannot tell one way or another.
I used the Z80 a lot in the home 8-bit computer era with plenty of machine code (I had no assembler) but I cannot recall much apart from a few instructions and op-codes that won't seem to leave the brain : )
The embedded 8-bit stuff I encountered later was mostly Motorola based (6805 and 6811 particularly) and a few other manufacturers.
Hi Shabaz,
Further to the Z80 discussion in relation to the Sharp PC-1600: reading the Technical Reference Manual, answers to several questions can be
found: http://pockemul.com/Documents/PC1600/PC1600TechnicalReference.pdf .
First of all, the main CPU, SC-7852, is a Z80A-clone. Second: Sharp specifies LH-5801/3 for what they call the subprocessor; so early production
probably was equipped with the 'old' PC-1500A CPU, which was then later on replaced by an upgraded version, the LH-5803.
After that the LH-58xx series was obviously discontinued, in favour of their SC family of micrprocessors - maybe to improve Z80(A)-compatibility.
The best - most comprehensive yet concise - overview: https://sharppocketcomputers.com/index.htm#basic . As an aside: It is remarkable that
after the 4-bit SC dual processor in Sharp's first pocketcomputer, the PC-121x had been succeeded by the 8-bit LHs, 4-bit SC-processors were
used again in later models.
Where the master-slave operation in the PC-1211 worked flawlessly, cooperation between the SC-Z80A and the LH-subprocessor more often than
not led to system instability, up to complete crashes.
The main disappointment with the PC-1600 however was its substandard (for Sharp at least !) LCD. Cramming this 4 times bigger display plus an
extra full size PCB, etc. into the same case as the PC-1500 however, is of course no mean feat ...
Maybe taking a glance at mnemonics and opcodes in the PC-1600 Tech Ref Manual can bring our decission nearer as to the LH-5801 was a Z80
derivative, or not. Memory allocation of the SC-Z80 surely differs considerably from that of the LH-5801, yet addressing range is equal (512 kB),
thanks to the flipflop registers in the LH; the SC seems having to do a lot of bank switching in large applications ...
Cheers
Ray
Hi Shabaz,
Very interesting musings about Z80 and possible 'mimicry' ... And thank you for the literature suggestions.
I believe having gotten some idea of Sharp policy in the dozen or so years I've made a living out of their products in many applications.
Do share your viewpoint that a lot of Japanese manufacturers of the time had more than enough innovation capability of their own, in order
not having to rely on copying; they did however clever- and selectively enter into strategic alliances and joint ventures.
I was appalled to learn that the company was recently taken over by Foxconn, of all the lousy manufacturers of today ...
The Japanese goverment should be ashamed for not having done anything to prevent this - the company that produced the unique amber
EL-displays for the Space Shuttle and where Philips had to buy all their LCD patents !
Back to the good ol' eighties and Sharp policy: I still feel the only explanation that makes sense for the model number, (LH-)5801, is as follows.
Next to their OEM production of Z80 clones - LH080, etc. - they wanted a proprietary microprocessor design for their indeed innovative line of
pocket computers. However they did not want to isolate these products too much from the brands and models that had become well-known
market leaders, in order to reach the broadest possible acceptance. So they devised the number 5800, with a wink to the 6800; but in order
to prevent the impression that they would suggest to make a predecessor, or down-graded version, they made the number their own by changing
it into 5801. Speculative ? Sure, but have I "entered into the realms of phantasy" ?
There was btw a LH-5803, which was meant to emulate the 1500 in its successor, the PC-1600 in order to attain full SW-compatibility. (It didn't
work 100% - much like my XP Pro overlay on Windows 10; this was probably also the reason for the PC-1600 being a less stable system than the trustworthy 1500).
Cheers
Ray
Hi Shabaz,
Very interesting musings about Z80 and possible 'mimicry' ... And thank you for the literature suggestions.
I believe having gotten some idea of Sharp policy in the dozen or so years I've made a living out of their products in many applications.
Do share your viewpoint that a lot of Japanese manufacturers of the time had more than enough innovation capability of their own, in order
not having to rely on copying; they did however clever- and selectively enter into strategic alliances and joint ventures.
I was appalled to learn that the company was recently taken over by Foxconn, of all the lousy manufacturers of today ...
The Japanese goverment should be ashamed for not having done anything to prevent this - the company that produced the unique amber
EL-displays for the Space Shuttle and where Philips had to buy all their LCD patents !
Back to the good ol' eighties and Sharp policy: I still feel the only explanation that makes sense for the model number, (LH-)5801, is as follows.
Next to their OEM production of Z80 clones - LH080, etc. - they wanted a proprietary microprocessor design for their indeed innovative line of
pocket computers. However they did not want to isolate these products too much from the brands and models that had become well-known
market leaders, in order to reach the broadest possible acceptance. So they devised the number 5800, with a wink to the 6800; but in order
to prevent the impression that they would suggest to make a predecessor, or down-graded version, they made the number their own by changing
it into 5801. Speculative ? Sure, but have I "entered into the realms of phantasy" ?
There was btw a LH-5803, which was meant to emulate the 1500 in its successor, the PC-1600 in order to attain full SW-compatibility. (It didn't
work 100% - much like my XP Pro overlay on Windows 10; this was probably also the reason for the PC-1600 being a less stable system than the trustworthy 1500).
Cheers
Ray
Hi Shabaz,
As Appendices at the end of the 276 page PC-1600 Tech Ref Manual I found mnemonics, op-codes, and what have you of both the SC- and the
LH-processor. Not my cup of thea, really ... But maybe someone else finds the clues, required to answer the question: was LH-5801/3 a Z80
derivative, or not ?
For me Chapter 7 is much more evocative, and it confirms my belief all along, that not only 'Ol Blue Eyes did everything "My Way" ...
It is quite impressive what Sharp has integrated on-chip*, next to the processor 'core' - this goes for the Z80A derivative, as well as for the LH.
I've called what they have packed into this pocketcomputer "no mean feat". If you look at the features, you can say that again:
- 3 microprocessors, two 8-bit main CPUs (one emulating the PC-1500A a.o.) + one 4-bit subprocessor (I/O)
- 3 x 36 kB ROM
- RS-232C I/F
- serial optical I/F, 38.4 kbaud
- analog input (ADC)
- automatic power off with external wake-up from peripheral
- floppy and RAM-disk options
- 60-pin fully programmable system/expansion bus output
- 2 memory module slots
Impressive ? Sure ! A joy to work with (as a programmer or a user) ? Not really ... And that's a shame.
PC-1600 has never been able to replace PC-1500A in the market, possibly because it became the victim of its own over-complexity ?
At the time (mid eighties and on) Sharp had already her organizer concept ready, later shared in the PDA concept with Apple (Newton),
and so probably didn't care too much ... (PC-12xx, 14xx, E200, and E500 series thriving)
Cheers
Ray
* a.o. the complete port processor, LH-5811, of PC-1500 in the SC main CPU
Hi Ray,
It could be derived from the Z80, I really cannot tell one way or another.
I used the Z80 a lot in the home 8-bit computer era with plenty of machine code (I had no assembler) but I cannot recall much apart from a few instructions and op-codes that won't seem to leave the brain : )
The embedded 8-bit stuff I encountered later was mostly Motorola based (6805 and 6811 particularly) and a few other manufacturers.
Hi Shabaz,
Further to the Z80 discussion in relation to the Sharp PC-1600: reading the Technical Reference Manual, answers to several questions can be
found: http://pockemul.com/Documents/PC1600/PC1600TechnicalReference.pdf .
First of all, the main CPU, SC-7852, is a Z80A-clone. Second: Sharp specifies LH-5801/3 for what they call the subprocessor; so early production
probably was equipped with the 'old' PC-1500A CPU, which was then later on replaced by an upgraded version, the LH-5803.
After that the LH-58xx series was obviously discontinued, in favour of their SC family of micrprocessors - maybe to improve Z80(A)-compatibility.
The best - most comprehensive yet concise - overview: https://sharppocketcomputers.com/index.htm#basic . As an aside: It is remarkable that
after the 4-bit SC dual processor in Sharp's first pocketcomputer, the PC-121x had been succeeded by the 8-bit LHs, 4-bit SC-processors were
used again in later models.
Where the master-slave operation in the PC-1211 worked flawlessly, cooperation between the SC-Z80A and the LH-subprocessor more often than
not led to system instability, up to complete crashes.
The main disappointment with the PC-1600 however was its substandard (for Sharp at least !) LCD. Cramming this 4 times bigger display plus an
extra full size PCB, etc. into the same case as the PC-1500 however, is of course no mean feat ...
Maybe taking a glance at mnemonics and opcodes in the PC-1600 Tech Ref Manual can bring our decission nearer as to the LH-5801 was a Z80
derivative, or not. Memory allocation of the SC-Z80 surely differs considerably from that of the LH-5801, yet addressing range is equal (512 kB),
thanks to the flipflop registers in the LH; the SC seems having to do a lot of bank switching in large applications ...
Cheers
Ray