The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.
The Z80 is still manufactured today and I was wondering whether there is any interest for a community or discussion group.
I worked at Mostek maintaining the Fairchild Sentry testers used to test the Z80s when they first began to manufacturer them. The second computer I every
built (parts, pcb, solder) was the SDB-80 which was the Mostek Software Development Board for the Z80 with 16K bytes (8 - MK4116 16K bit) dynamic RAMs
which Mostek also made. The first wire wrap board I ever made was a 48K byte dynamic RAM board also using MK4116s that worked with the SDB-80. I can
tell you there were a bunch of happy technicians when we were told that Mostek would be second sourcing the Z-80 and even happier when we were told we
could buy SDB-80 kits and build them ourselves! Those were really fun days. I still have a Zilog Z80 in a ceramic package that says it was manufactured in
Dallas even though Mostek was actually in Carrollton a suburb in Dallas County just north of north-west Dallas.
Wow! that's amazing that you got such a large DRAM board working with Wire-wrap.
Do you still have any photos or schematics of it?
It was quite rare to come across Mostek parts in Australia. We usually got Zilog, SGS and Sharp.
And from memory the SGS parts didn't support the undocumented instructions.
Hi COMPACT,
My son has a binocular microscope for his cartridge repairs/mods - tried it, didn't work for me alas (btw: there's a not-so-steady-anymore hand
to take into account as well). Thanks anyway for the uplifting tip.
I've read enough disturbing reports by pro circuit designers to stay away from SPICE and the like. My WYSIWYG-like statement lacked nuance,
that's true, but transitional phenomena e.g. are difficult to be measured correctly, and consequently just as difficult to predict/calculate/simulate.
And my experiments were on so called linear PSUs; btw: there's practically nothing 'linear' really in the operation of these classic power supplies.
As a result they are noisy, and hard to tame. Your average designer, however thinks, an overkill of microFarads + 'tripods' will easily cure this ...
Audiots frequently spend big bucks on external power supply 'upgrades' - on top of the just mentioned cure, these contain big transformers
with rediculous VA specs. While this might make sense for a power amp with underrated internal PSU, such upgrade PSUs for phono-amps are
outrageous ! We have performed in-depth listening tests here, and concluded that the advertised pros - improved bass response and dynamics -
didn't make up for the apparent loss of overall-quality: the music seemed robbed of its liveliness. Some team members stated: "As if an elephant
is sitting on the sound".
If you would want to consider RCA's Dynagroove technology* as a kind of early dithering, I would be with you, but calling RIAA equalisation
distorting the signal ... Changing the tonal balance in no way fits the definition of distortion. It is in fact a perfectly rational adaptation to the medium.
Its primary objective was optimizing playing time - so maybe one could call it a form of (physical) compression. The second aim, however is to
diminish and limit distortion - i.e. tracking distortion ! The famous ADC XLM cartridge from the sixties arguably was one of the most agile ever,
but it was not free from tracking distortion, of course. Here the question arises, how one is to discern between distortion caused by the vinyl
registration process, and distortion from the cartridge tracking the groove with its needle.
My son has done quite a bit of research in improving suspension in phono cartridges; he was surprised to find, how much there still is to be
gained in terms of tracking distortion this way - the experiments were done with state-of-the-art commercial carts.
(to be continued)
Ray
* dynamics at the end of the Pink Panther theme by Mancini e.g. really are impressive, but ... sure, it's just an effect - no HiFi.
To the list of analog turntables (and vinyl records) problems vs CD you can add poor channel separation, lower signal to noise, far less dynamic range, low frequency limits,
groove wear, warping, inherent vulnerability to acoustic feedback, tracking problems, and less resistant to injury and corruption.
As for reproducing square waves, as far as I know, no instrument other than electronic synthesizers produce anything that approaches the fast rise/fall times of a square wave.
That said, there are several groups that I like that use(d) synthesizers.
Hi Andrew,
Reading your profile, several thoughts spring to mind:
- seems like a wonderfulfilling (language economy) job/passtime - educating people, in order to enrich nowdays' ict with an intriguing past
- visiting my wife's family in Canada years ago, we went to the Toronto Science Museum - I had the time of my life !
- your level denominator goes, well ... lovely with your 'job' -:) Women's role in technology is grossly underrated, and almost neglected
(ENIAC, NASA, etc).
Cheers
Ray
As for degrading eyesight I'm reliant upon my bench binocular microscope just to solder 1960's tech like DIP ICs and through hole.
My spare parts are so old that I have to remove the unwanted oxide layer from them (just like my brain).
I don't like too much SPICE in my food.
Analog turntables - Don't get me started! The analog signal is distorted prior to recording so it can be reverse distorted for playback to support the RIAA equalisation.
And also seem to also ignore other distortion influences such as wow and flutter, stylus/cartridge momentum and contact friction variations
Like oscilloscopes, sound should be sampled at about 5x or more than the desired maximum bandwidth.
And how does one get a speaker to playback perfect square waves?
All of this gives me the "jitters!"
Hi Clem (if that's alright with you ?),
Don't despair, I've become a 'grumpy old man' myself lately sometimes -:).
(My wife was born in the middle of WW II, glad I missed that period - if only just).
But writing about my experiences gives me the idea that it isn't all over, and of no use to anybody any more.
If I can fill in some white spots in other members' memories and/or knowledge, like they have done in mine,
that would make it worth my while (like they said in the old days). Just keeping readers amused is OK too, btw.
I had to stop my electronics experiments a few years ago because of deteriorating eyesight. SPICE for me is no alternative, as I believe it can not
reliably simulate a real novelty circuit. After all it stands to reason that you can't get out what has not been put in, can you ?
So the only thing left for me to do is devising new circuits ... mentally, and hoping I can get someone interested enough to put my ideas to the test.
Also rewarding is acting as a kind of sparring partner for my son, when he is figuring out, how to improve on existing vinyl cartridge cantilever
design e.g..
Hope I haven't annoyed you.
Cheers
Ray
Come to think of it: I've also been privileged to live in the era of:
- the dawn of music registration on vinyl
- the transition (soon after) from mono to stereo
- transistors displacing vacuum tubes (while becoming a swiftly expanding family)
- the invasion of digital technology in the art of music registration and reproduction, culminating in the CD, but :
x NO, don't feel privileged, having to witness music quality being slaughtered by ease-of-use driven technology,
like MP3, streaming, and what have you ? (Microsoft 'eliminated' prof. Johnsons's HDCD, the best digital format ever).
So, I feel privileged, being able to enjoy in the same lifetime:
- the unsurpassed vibrancy of shellac disc mechanical replay with horn reproduction (thank you Canned Heat for pointing that out, back stage !)
- the reappreciation of mono recordings and revival of mono music reproduction (even newly developed vinyl cartridges)
- the vacuum tube revival (thanks mainly to Russia, China, and Eastern Europe - with NOS running out)
- the reappreciation of pure Red Book, but moreover of analog audio in all its forms.
How come ?
Organizers gradually took over the pocket computer market, but mid nineties my son helped me realize, there was an end to this.
His expertise (my former hobby) was (still is) high quality audio. So we decided to start our own import company - later developping
proprietary products.
What's the point in all of this ?
In one word: digital ! While digital control of equipment functions is only remotely (pun intended) interesting, we focussed on DSP,
digital signal processing. At first I was somewhat puzzled by the notion of losses in file conversion and transition - never encountered
such problems while processing data files on a computer ! Admittedly, it took me some time to figure out the cause.
Anyway, let me end this 'chapter' with a cliff-hanging anecdote:
After we were asked frequently by the public, why we did not demonstrate with digital equipment at an audio show, we got tired of lengthy
answers, followed by ditto discussions. So we devised a 'cunning plan': a large poster of the Mona Lisa was fed through a shredder, which
we stopped just before the end was reached (if this seems familiar to you, having followed the news lately: we were fisrt !). Next we 'repaired'
the poster with transparent 'magic tape'; then with a felt pen we wrote under the picture: "NICE, ISN'T IT: DIGITAL ?". Problem solved ...
Cheers
Ray
Thank you, COMPACT and Andrew Johnson !
Think I'm just privileged, having lived (better still: mostly had my youth in) the era of:
- the birth of the micropocessor
- the development from calculators into hand-held computers
- the 'transistorizing' of electronics
- the chip revolution leading to "zero cost electronics" (Scientific American, 1975), and ultimately to hand-held communication devices
- the development of LCD and similar display technology
and so on ...
It all began when awed by a self-built X-tal receiver, while visiting a cousin - almost mystically fascinating !
Not only did I blend together one myself shortly after, but also began reading books on radio history from the school library (which didn't have
anything DIY). And I got pretty jealous of inquisitive people like myself, who had been lucky enough to live during the age of say Heinrich Hertz,
Marconi, and the like (unfortunately I discovered Tesla much later). So obviously, some people just cannot be pleased enough ... !
Cheers
Ray
P.S.: the excitement of listening to your self-built X-tal receiver is similar to watching your first program do what you envisioned;
in both cases, "you'll always remember your first time" ...
Hi Andrew,
Reading your profile, several thoughts spring to mind:
- seems like a wonderfulfilling (language economy) job/passtime - educating people, in order to enrich nowdays' ict with an intriguing past
- visiting my wife's family in Canada years ago, we went to the Toronto Science Museum - I had the time of my life !
- your level denominator goes, well ... lovely with your 'job' -:) Women's role in technology is grossly underrated, and almost neglected
(ENIAC, NASA, etc).
Cheers
Ray