Member's Forum Help with noise measurement and stability of regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 630 subscribers
  • Views 3278 views
  • Users 0 members are here
Related

Help with noise measurement and stability of regulator

Andrew J
Andrew J over 5 years ago

I'm looking for some help with resolving a noise and what I believe is stability problem of a -5V LDO regulator.  Here is the circuit:

image

and in case it's useful, the relevant part of the PCB:

image

 

The circuit section I'm having difficulty with is the top right (yellow ICs).  I have a 285Ohm resistor soldered across terminals of TP9 and it draws 17.5mA.  R22 and C34 are not populated.

 

The TC7662TC7662 DC-DC charge pump, is fed from a regulated 12V and outputs -11.8V to feed into a -5V LDO regulatorMC7905CDMC7905CD which is outputting -5.011V.

 

When I take measurements (AC coupled, BW 20MHz, 1xprobe with the pigtail rather than flying lead) of the charge pump output (at TP12) and -5V output (at TP9) I get:

image

CH3: Charge Pump output with HF reject on (matches what is expected in the datasheet).  I was expecting that the frequency of the output would be 35kHZ due to way I have pins 1 and 8 connected together.

 

image

CH4: -5 LDO output with LF reject on.

 

I think the LDO output looks like it is oscillating.  Looking at the circuit the input capacitor, C18, is too small and should be a 0.33uF tantalum for stability, according to the datasheet but I have used a 0.33 ceramic capacitor as I don't have any useable tantalums and my thinking was the ceramic should have a low ESR.  I've actually tried with 22uF and then a 68uF electrolytic capacitors, in parallel, but both have zero effect on the LDO output which remains steadfastly at 1.32V.  I've tried the circuit on a breadboard but unfortunately I only have a TI LM7905 - this seems to work ok even with the original capacitor value and doesn't oscillate.  I think the TI part behaves differently so it's not a great comparison.  Its output is slightly improved with a 22uF input capacitor.

 

I really thought that adding an electrolytic capacitor at the input would help (the ESR of the 22uF was around 2.2Ohm) but it makes no difference at all.  I'm out of ideas short of "it really needs a tantalum capacitor on the input", so I'm putting this out there to see if anyone can give me pointers or things to try.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 5 years ago

    I couldn't find any reference to it in data sheets but it may be that the 7905 does not like the 1uF ceramic output cap. Lots of older design monolithic regulators need some esr in the output cap to work.  Try a 10uF aluminium electrolytic output cap instead of the 1uF ceramic.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 5 years ago in reply to michaelkellett

    Thanks Michael.  I tried with a 22uF on the output but in parallel with the 1uF and further from the regulator (no effect). I’ll remove the 1uF and solder in a 10uF in the morning and see how that goes. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 5 years ago in reply to michaelkellett

    Thanks Michael.  I tried with a 22uF on the output but in parallel with the 1uF and further from the regulator (no effect). I’ll remove the 1uF and solder in a 10uF in the morning and see how that goes.