• Products and Partners
    Products and Partners
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
Member's Forum Help with noise measurement and stability of regulator
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 630 subscribers
  • Views 3334 views
  • Users 0 members are here
Related

Help with noise measurement and stability of regulator

Andrew J
Andrew J over 5 years ago

I'm looking for some help with resolving a noise and what I believe is stability problem of a -5V LDO regulator.  Here is the circuit:

image

and in case it's useful, the relevant part of the PCB:

image

 

The circuit section I'm having difficulty with is the top right (yellow ICs).  I have a 285Ohm resistor soldered across terminals of TP9 and it draws 17.5mA.  R22 and C34 are not populated.

 

The TC7662TC7662 DC-DC charge pump, is fed from a regulated 12V and outputs -11.8V to feed into a -5V LDO regulatorMC7905CDMC7905CD which is outputting -5.011V.

 

When I take measurements (AC coupled, BW 20MHz, 1xprobe with the pigtail rather than flying lead) of the charge pump output (at TP12) and -5V output (at TP9) I get:

image

CH3: Charge Pump output with HF reject on (matches what is expected in the datasheet).  I was expecting that the frequency of the output would be 35kHZ due to way I have pins 1 and 8 connected together.

 

image

CH4: -5 LDO output with LF reject on.

 

I think the LDO output looks like it is oscillating.  Looking at the circuit the input capacitor, C18, is too small and should be a 0.33uF tantalum for stability, according to the datasheet but I have used a 0.33 ceramic capacitor as I don't have any useable tantalums and my thinking was the ceramic should have a low ESR.  I've actually tried with 22uF and then a 68uF electrolytic capacitors, in parallel, but both have zero effect on the LDO output which remains steadfastly at 1.32V.  I've tried the circuit on a breadboard but unfortunately I only have a TI LM7905 - this seems to work ok even with the original capacitor value and doesn't oscillate.  I think the TI part behaves differently so it's not a great comparison.  Its output is slightly improved with a 22uF input capacitor.

 

I really thought that adding an electrolytic capacitor at the input would help (the ESR of the 22uF was around 2.2Ohm) but it makes no difference at all.  I'm out of ideas short of "it really needs a tantalum capacitor on the input", so I'm putting this out there to see if anyone can give me pointers or things to try.

  • Sign in to reply
  • Cancel
Parents
  • Andrew J
    Andrew J over 5 years ago

    Could I ask you guys a follow up question.

     

    Given a choice between an input/ouput capacitor of tantalum or electrolytic, which would be preferable?  I have a feeling it may be down

     

    I have stability and good noise management with an input cap 22uF electrolytic and output cap 10uF electrolytic.  The 22uF caps I have used have low ESR - I measured one that I have to hand at 0.6Ohms @ 100kHz so they're all likely to be of that order, including the one in-circuit.

    The datasheet has this to say (I couldn't find the references you made in the datasheet, John jw0752)

     

    In many low current applications, compensation capacitors are not required. However, it is recommended that the regulator input be bypassed with a capacitor if the regulator is connected to the power supply filter with long wire lengths, or if the output load capacitance is large. An input bypass capacitor should be selected to provide good high−frequency characteristics to insure stable operation under all load conditions. A 0.33 uF or larger tantalum, mylar, or other capacitor having low internal impedance at high frequencies should be chosen. The capacitor chosen should have an equivalent series resistance of less than 0.7 Ohms

     

    If I look for 0.33uF tantalum caps, I can't find any with that low an ESR, most are in the 20s Ohms (actually, I've found one with an ESR of 6 Ohms).  "High-frequency" is a rather relative phrase as well!  Part of the reason for asking is curiosity - I've read somewhere that each capacitor material is more suitable for different frequencies and I've seen plenty of attenuation charts that show this.  One answer could be "don't worry about it if your electrolytics work" but I was thinking of re-working the PCB and providing space for these caps.  The pads for typical tantalum cases are different to pads for electrolytics (SMD rather than TH.)

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to Andrew J

    Hi Andrew,

     

    I am not sure if it was a typo but the highlighted section refers to a 0.33 mF cap which is a 330 uF cap and you are talking about a 0.33 uF cap in your comments.

     

    The Data Sheet I quoted from is probably from a different company.

     

    If the caps you are using are working that is the best measure of functionality.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 5 years ago in reply to Andrew J

    Hi Andrew,

     

    I am not sure if it was a typo but the highlighted section refers to a 0.33 mF cap which is a 330 uF cap and you are talking about a 0.33 uF cap in your comments.

     

    The Data Sheet I quoted from is probably from a different company.

     

    If the caps you are using are working that is the best measure of functionality.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Andrew J
    Andrew J over 5 years ago in reply to jw0752

    It's a typo from pasting which I will fix - the uF was changed to a mF because in the datasheet its the actual Greek letter!  It is a 0.33uF tantalum that is required.  I picked up the change of 0.7 [Omega] to 0.7W on the paste though!!

     

    Tantalum Polymer caps start at 1uF but are the only ones capable of getting an ESR < 0.7 Ohms.  Ditto Aluminium Polymer caps.  Tantalum at 0.33uF have way, way larger ESRs than 0.7Ohms - I can go higher to say 3.3uF or larger and find caps with a low enough ESR and larger is ok;  Alu electrolytics may just make it.  

     

    It would seem that the output capacitor needs ESR so as long as I avoid MLCC and polymer it should be ok.

     

    Given whatever I do I have to buy them in and I have to change the PCB, I'm still curious about the advantages of using tantalum over electrolytics.