Member's Forum Experiences with Pre-Heater - I'm Looking to Buy
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 629 subscribers
  • Views 6510 views
  • Users 0 members are here
Related

Experiences with Pre-Heater - I'm Looking to Buy

Andrew J
Andrew J over 5 years ago

I'm looking to buy a pre-heater to help with SMD soldering and rework, although mostly the former, and I'm interested in others experiences with these.  A lot of the heaters at my end of the budget are IR based which seems to be ok but may be impacted by reflectivity of boards/parts (I wonder how well they work with white PCBs.)  So far, the PCBs I've had made up are 100mmx100mm although one has been 140mmx1  The choices seem to be to spend a fantastic amount on a 'known' brand or rather less on one of the fairly common cheaper Chinese brands. 

 

What I'm not interested in is:

  • any sort of DIY solution.
  • anything that has a reputation for needed fixing on arrival.
  • an oven.

 

I seem to be homing in on the following:

 

Metcal PCT-100Metcal PCT-100: well known brand and not overly expensive.  Doesn't specify board size but looks like it may allow for 200mm x 100mm based on product dimensions.  It does say it is a 'focussed' heater which implies to me that it targets a small part of the underside of a board placed directly above the heater element so I don't know how good it would be at heating the overall board without overheating one specific spot.  All the marketing blurb shows very small PCBs being used.  There was a 'review' on YouTube but it wasn't a particularly useful one.

 

The bigger brother, Metcal PCT-1000Metcal PCT-1000, looks very useful but is really expensive.  Could form part of a larger soldering solution with other Metcal devices but I don't really need them right now.  If Element14 want to donate in return for a review then I could manage that image image

 

Aoyue Int883: a cheaper brand that makes a number of different soldering stations but the quality may be a bit suspect - I saw a YouTube video about a different pre-heater of theirs that came damaged.  Hardly statistically relevant, Digikey sell it if that means anything, and it does have a number of different operating modes and looks like it would be well controlled with three thermocouples.  Would take any board size I have.

 

Quick 870ESD: again, a cheaper brand and this one purports to reflow as well (not too bothered about that.)  Same sort of brand as Aoyue, more expensive and seems less controllable.

 

I don't think I could leave this post without an honourable mention to Zephyrtronics for their retro-industrial air-baths and a website built in the 1990s!  These look like good units but verging on the too expensive but the compact size may be worth considering.

 

Others I've looked at have been stupidly expensive or have very small heating areas.  So I seem to be leaning towards the Aoyue model but if anyone has alternative suggestions or use the Metcal PCT-100 then I'd definitely want to hear about it.

  • Sign in to reply
  • Cancel
Parents
  • Jan Cumps
    Jan Cumps over 5 years ago

    If your goal is to use it as a pre-heater - to aid the hot-air gun, you don't need a lot.

    I use a Tenma Mini SMD Preheater. Kindly sent to me by Shabaz image.

    This is a small device but can pre-heat a decent board.

    image

     

    It makes a big difference if you have to get heat from 20° to 350, or from 120° to 350°. Everything works way smoother.

     

    How I work for pre-heating (I use lead-free):

    • I put the board above the heater, set it to 100°.
      Usually I prepare my work while it's warming up. If it gets to hot for my hands I switch it off for a little while.
    • When I'm ready to use the gun, I put it between 150 and 200.
    • When finished, I switch of the heater but leave the power on. The fan helps with cooling.

     

    When dealing with double sided, I usually keep it at 100 ° and deal with it. Still better than no pre-heat.

     

    When dealing with a difficult IC or FET, with big ground plane that needs to set:

    • I do the same as above, but with the heater outlet aimed at the location of the component.
    • When ready, I push up the temperature to what makes sense for the job, and attack the component with the gun at the same time.

     

    I mentioned this before on the forum: I practice a lot with scrap PCBs.

    You learn what works and not for you. At what temperature the PCB delaminates or loses pads. At what settings components spontaneously drop from the underside.

    You learn the sounds and smells.

     

    Once you have been in a situation where placing or removing an IC took uncomfortably long time, you'll notice that having a pre-heater is a great asset.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 5 years ago in reply to Jan Cumps

    Thanks Jan.  Do you have a model number for that, or a picture of the top.  How do you think it compares, size-wise and outlet-wise, to the PCT-100 I mention above?  What's the biggest boards have you pre-heated with it?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Andrew J

    TENMA 2064552, no longer made, but the Aoyue 853 is virtually identical.

     

    Foto of the top. On an A4 page for scale:

    image

    Measurements:

    image

     

    I don't know the exact measures of the biggest board. Approx: 1/3 of the height of an A4 page, width of an A4 page.

    edit: it says: 540 W

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Andrew J

    Andrew J  wrote:

     

    I see that was some time ago now.  ...

    Yes, I designed most of the board at the time that Brussels was in the grip of the terror attacks and its aftermath. It's linked to that era in my memories.

    I'd like to use it in this month's project 14, as the output stage of a class-D amp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 5 years ago in reply to Jan Cumps

    I see that was some time ago now.  You'll be glad to know that JLCPCB will manufacture five 4-layer PCBs up to 100mmx100mm for £5.85 (€6.59) + delivery.  Crazy cheap.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 5 years ago in reply to Jan Cumps

    I see that was some time ago now.  You'll be glad to know that JLCPCB will manufacture five 4-layer PCBs up to 100mmx100mm for £5.85 (€6.59) + delivery.  Crazy cheap.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Andrew J

    Andrew J  wrote:

     

    I see that was some time ago now.  ...

    Yes, I designed most of the board at the time that Brussels was in the grip of the terror attacks and its aftermath. It's linked to that era in my memories.

    I'd like to use it in this month's project 14, as the output stage of a class-D amp.