Member's Forum Solder Reflow Oven Build
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 630 subscribers
  • Views 1800 views
  • Users 0 members are here
  • reflow
  • solder
  • msp430
  • oven
Related

Solder Reflow Oven Build

joe
joe over 12 years ago

I was watching the episode of Ben Heck's show here on element14 where he build a solder reflow oven out of a toaster oven and I thought this might make a nice project.  If you'd like to check out Ben's build, you can check out the link below:

Episode 116: Ben's Home-Brew Solder Reflow Oven 2.0 Episode

 

I have started work on this project and will post additional details if I make any progress.  To get going, I have chosen the MSP430G2955 to be the controller and will be interfacing it with the EA DOGS102-6 102x64 dot matrix display. 

  • Sign in to reply
  • Cancel
Parents
  • joe
    joe over 12 years ago

    At first glance, it appeared that measuring a negative temperature would be a bit more difficult because of the way in which the MAX31855 handled these values.  Basically, the chip works backwards for negative, so a temperature of -0.25°C would be represented as 1111 1111 1111 11 and a temperature of -0.50°C would be represented as 1111 1111 1111 10 and so on.  Since this is basically the opposite of the positive temperatures, I found that if I just XOR'ed the result with 1111 1111 1111 11 (0x3FFF)and added 1, I could use the same method as I used for the positive results.  Here's a piece of my test code used to obtain positive or negative temperatures in Celsius:

     

     

       extern uint8_t volatile temp[4];  \\ temp[0] contains the top 8 bits and temp[1] contains the bottom 6 bits plus two unused bits which will be shifted out

       uint16_t volatile temp_result;


    // Move the binary temperature result into temp_result using only the lower 14 bits

     

      temp_result = temp[0];

     

      temp_result = temp_result << 8;

     

      temp_result |= temp[1];

     

      temp_result = temp_result >> 2;

     

    // The if statement checks the 14th bit.  Assuming there is no fault condition, this bit will be 1 if the result is negative.

       if ( (temp_result & 0x2000) == 0){

           sprintf(buffer, "Result is: \n%d.%d%cC",temp_result >> 2, (temp_result & 0x03) * 25, 0x7F);

     

           Dogs102x6_stringDraw(1, 0, buffer, DOGS102x6_DRAW_NORMAL);

    }

       else{

      temp_result = (temp_result ^ 0x3FFF) + 1;

           sprintf(buffer, "Result is: \n-%d.%d%cC",temp_result >> 2, (temp_result & 0x03) * 25, 0x7F);

           Dogs102x6_stringDraw(1, 0, buffer, DOGS102x6_DRAW_NORMAL);    

    }

     

    Additional code would need to be added to check for faults prior to making the temperature measurement. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • joe
    joe over 12 years ago

    At first glance, it appeared that measuring a negative temperature would be a bit more difficult because of the way in which the MAX31855 handled these values.  Basically, the chip works backwards for negative, so a temperature of -0.25°C would be represented as 1111 1111 1111 11 and a temperature of -0.50°C would be represented as 1111 1111 1111 10 and so on.  Since this is basically the opposite of the positive temperatures, I found that if I just XOR'ed the result with 1111 1111 1111 11 (0x3FFF)and added 1, I could use the same method as I used for the positive results.  Here's a piece of my test code used to obtain positive or negative temperatures in Celsius:

     

     

       extern uint8_t volatile temp[4];  \\ temp[0] contains the top 8 bits and temp[1] contains the bottom 6 bits plus two unused bits which will be shifted out

       uint16_t volatile temp_result;


    // Move the binary temperature result into temp_result using only the lower 14 bits

     

      temp_result = temp[0];

     

      temp_result = temp_result << 8;

     

      temp_result |= temp[1];

     

      temp_result = temp_result >> 2;

     

    // The if statement checks the 14th bit.  Assuming there is no fault condition, this bit will be 1 if the result is negative.

       if ( (temp_result & 0x2000) == 0){

           sprintf(buffer, "Result is: \n%d.%d%cC",temp_result >> 2, (temp_result & 0x03) * 25, 0x7F);

     

           Dogs102x6_stringDraw(1, 0, buffer, DOGS102x6_DRAW_NORMAL);

    }

       else{

      temp_result = (temp_result ^ 0x3FFF) + 1;

           sprintf(buffer, "Result is: \n-%d.%d%cC",temp_result >> 2, (temp_result & 0x03) * 25, 0x7F);

           Dogs102x6_stringDraw(1, 0, buffer, DOGS102x6_DRAW_NORMAL);    

    }

     

    Additional code would need to be added to check for faults prior to making the temperature measurement.