Member's Forum Which Microcontroller you "Like the Most?" & Which Microcontroller you "Want to work on but don't have it right now?"
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 633 subscribers
  • Views 884 views
  • Users 0 members are here
  • microcontrollers
  • processors
Related

Which Microcontroller you "Like the Most?" & Which Microcontroller you "Want to work on but don't have it right now?"

mudz
mudz over 11 years ago

So, as clearly mentioned in title, Which is your best microcontroller till date? i.e The Micro Controller you like most and love to start working on it anytime. Let it be as simple as ATMEL AT89S51 or PIC or AVR or ARM based Microcontroller.. and If possible do mention why?
It Doesn't ends here.. image
Also mention which microcontroller/processor you want(desire) to work on but  you haven't got your hands on it yet?
For me :

1> Personally, whenever I have to start or try a new module I start with TI MSP430G2553  If it's unable to provide me with enough horsepower I move to TI lm4f120, because they both are easy to program and have in-built features like adc, pwm etc.. which are enough to drive simple modules.

2> I really wish to work on Freescale IMX6Q6 Processor. I already have figured it out how to get it and soon it will be in my hands. image


What about you?

  • Sign in to reply
  • Cancel
  • dougw
    dougw over 11 years ago

    I like Cypress PSoC4 because it provides the most power for the lowest cost with the best development tools.

    I would also like to try a PIC32 Pinguino - powerful MCU, free development tools and no programmer needed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 11 years ago

    I follow microcontrollers closely, but haven't used one in an actual design in a long time.  That's because my main project needs a full-sized 32-bit processor SoC with off-chip memory.  But here are my favorite microcontrollers:

     

    1.  I like the TI MSP430 series.  This is largely nostalgia because the 16-bit instruction set is based on the PDP-11, which I programmed extensively and joyfully in my undergrad days.  The MSP430 even has chips with FRAM to mimic magnetic core memory image  I'd love to play with the MSP430 some day.

     

    2.  The STM32 ARM Cortex-M0/M0+/M3/M4 offerings are very nice.  You can get cheap Discovery boards that bring out all the pins, and you can program them over JTAG/SWD and not be stuck with closed-source software.  You'll be able to get Cortex-M7 soon.

     

    3.  I really like the Cypress PSoC 4 and PSoC 5LP hardware.  Unfortunately, you have to use their closed-source software on a Windows PC, which I see as a huge disadvantage.  I keep advocating for Cypress to release the small amount of information needed to create open-source tools.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 11 years ago in reply to kas.lewis

    Sometimes we wish, they all should be 5v chips and most of the times, they should stay like 3.3v.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 11 years ago in reply to Robert Peter Oakes

    I have already used Stellaris launchpad Lm4f120(now this series is re-branded as Tiva c), it is good for some heavy tasks(while maintaining low power usage) but as we know technology changes everyday, now my pick will be FRDM-K64F(http://in.element14.com/jsp/search/productdetail.jsp?sku=2406741). This boards supports many features like it's mbed enabled, onboard ethernet controller, sdhc socket, Accelerometer, magnetometer etc. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kas.lewis
    kas.lewis over 11 years ago in reply to supper_slash

    Freescale has 5V chips I'm working with the KEA64 and that is 5V, actually for me its a bit annoying as all the sensors I sues are 3.3V and the board does not easily give 3.3V but Its a nifty little guy to play around with and comes in a nice case and has the programer built onto the board. It also comes with some tutorials to get you started.

     

    Kas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to supper_slash

    more horsepower can be realized by simply going to a tiva C or better but still within the TI stable

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • supper_slash
    supper_slash over 11 years ago in reply to mudz

    Well, as i am already familiar with the mps 430 line, i have been using it lot.

    And if i need more i/o, or horse power, i run two together. lol.

    I no its not the right way to do it, but, until i decide to breakdown and buy some programmers for pic, or atmel, that's what i will haft to do.

    I only wish they were 5v chips.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 11 years ago in reply to supper_slash

    Wow these are small and cheap. I will buy 1 or 2 of them soon but I am more into powerful Microcontrollers. image I love to work on such powerful things to squeeze all the power out of them, to take them to extreme that's what i like.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • supper_slash
    supper_slash over 11 years ago

    i love the TI MSP430G2553 also.

    I am looking forward to working more with pic's and atmel.

    But i think my next purchase will be some $4 PSoC 4 boards 

    I never herd of them till a week or so ago, and so i want a few to try out.

    I have several projects on the back burner that i think these will be good for.