Member's Forum Which Microcontroller you "Like the Most?" & Which Microcontroller you "Want to work on but don't have it right now?"
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 633 subscribers
  • Views 886 views
  • Users 0 members are here
  • microcontrollers
  • processors
Related

Which Microcontroller you "Like the Most?" & Which Microcontroller you "Want to work on but don't have it right now?"

mudz
mudz over 11 years ago

So, as clearly mentioned in title, Which is your best microcontroller till date? i.e The Micro Controller you like most and love to start working on it anytime. Let it be as simple as ATMEL AT89S51 or PIC or AVR or ARM based Microcontroller.. and If possible do mention why?
It Doesn't ends here.. image
Also mention which microcontroller/processor you want(desire) to work on but  you haven't got your hands on it yet?
For me :

1> Personally, whenever I have to start or try a new module I start with TI MSP430G2553  If it's unable to provide me with enough horsepower I move to TI lm4f120, because they both are easy to program and have in-built features like adc, pwm etc.. which are enough to drive simple modules.

2> I really wish to work on Freescale IMX6Q6 Processor. I already have figured it out how to get it and soon it will be in my hands. image


What about you?

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    I follow microcontrollers closely, but haven't used one in an actual design in a long time.  That's because my main project needs a full-sized 32-bit processor SoC with off-chip memory.  But here are my favorite microcontrollers:

     

    1.  I like the TI MSP430 series.  This is largely nostalgia because the 16-bit instruction set is based on the PDP-11, which I programmed extensively and joyfully in my undergrad days.  The MSP430 even has chips with FRAM to mimic magnetic core memory image  I'd love to play with the MSP430 some day.

     

    2.  The STM32 ARM Cortex-M0/M0+/M3/M4 offerings are very nice.  You can get cheap Discovery boards that bring out all the pins, and you can program them over JTAG/SWD and not be stuck with closed-source software.  You'll be able to get Cortex-M7 soon.

     

    3.  I really like the Cypress PSoC 4 and PSoC 5LP hardware.  Unfortunately, you have to use their closed-source software on a Windows PC, which I see as a huge disadvantage.  I keep advocating for Cypress to release the small amount of information needed to create open-source tools.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 11 years ago

    I follow microcontrollers closely, but haven't used one in an actual design in a long time.  That's because my main project needs a full-sized 32-bit processor SoC with off-chip memory.  But here are my favorite microcontrollers:

     

    1.  I like the TI MSP430 series.  This is largely nostalgia because the 16-bit instruction set is based on the PDP-11, which I programmed extensively and joyfully in my undergrad days.  The MSP430 even has chips with FRAM to mimic magnetic core memory image  I'd love to play with the MSP430 some day.

     

    2.  The STM32 ARM Cortex-M0/M0+/M3/M4 offerings are very nice.  You can get cheap Discovery boards that bring out all the pins, and you can program them over JTAG/SWD and not be stuck with closed-source software.  You'll be able to get Cortex-M7 soon.

     

    3.  I really like the Cypress PSoC 4 and PSoC 5LP hardware.  Unfortunately, you have to use their closed-source software on a Windows PC, which I see as a huge disadvantage.  I keep advocating for Cypress to release the small amount of information needed to create open-source tools.