Member's Forum Nostalgia: *** Smith Electronics Fun Way into Electronics
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 635 subscribers
  • Views 3019 views
  • Users 0 members are here
  • fundamental
  • beginners
  • nostalgia
  • fun
Related

Nostalgia: *** Smith Electronics Fun Way into Electronics

Gough Lui
Gough Lui over 11 years ago

A little while back, I did a little blogging about *** Smith Electronics Fun Way into Electronics series. This was arguably one of the main things which got me into the whole electronics hobby, so I thought some of you might also enjoy looking back at *** Smith when it was more than just a consumer electronics shop. If you remember these, or have any thoughts to share, I'd love to hear them image.

 

  • Tech Flashback: *** Smith’s Fun Way into Electronics Vol. 1
  • Tech Flashback: *** Smith’s Fun Way into Electronics Vol. 2 and 3
  • Sign in to reply
  • Cancel
Parents
  • supper_slash
    supper_slash over 11 years ago

    I remember having a "Boy Scout" book that got me started. I was not a scout, but i would buy there books, and there was a plan for a "Generator" made out of a spool of tread.

    There was more projects in there that i did, but i wore several of them generators out.image

    After that was Forest mimms. Like others.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to supper_slash

    Hi Lupe, You brought back a memory for me, also of a Boy Scout manual with a crystal radio in it. This was before they had nice kits made up.  I wound and shelacced a coil on a paper tube, used tin foil and paper to make a capacitor, and the crystal was a small piece of germainium that a bent pin was placed against. A small set of earphones was attached and there was the local radio station. It was very exciting to have someting like that really work.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to jw0752

    Wow, awesome that you actually built the diode!!

    My crystal radio attempts used the popular OA91 that was (is still) available from surplus stores. Like you I used a paper tube with the coil on it. The wire is really expensive now (Litz wire) which is a shame.

    Then I tried this one, so frustrating it never worked for me, I spent days on it ; ) using parts from the Tandy (Radio Shack) which were not quite the exact parts since the book was so old.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild

    I forgot to say that SOLDER SMOKE is a great old school pod cast done by this American guy out in Rome.

    I think it's the same chap who formulated the WSPR stuff correct me if I'm wrong?!?!?

     

    BTW Shabaz he has a bit on those SI5351 synthesizers Cool components had!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    Just had an idea I could use some plastic cogs to form a reduction gear to improve the tuning ..couldn't say the acrylic wasn't a good insulator ...probably good Permitivity  as well image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    Great video!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    Ah! Good point. I've only seen the relay switched inductor/capacitor ones, for about 20W or so. The motor method would be way higher.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    No way!!!

    This is great! A shame the video cannot be found on the BATC site. I wonder why they don't make use of youtube, for greater visibility of all the amazing material they probably have.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    You have the kit  no real excuses and you can even involve the Nephews. get them running the wire down the garden.

    Get a reel of enamelled wire from say Maplin or something and job done

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild

    Rev Dobbs  famous enough to have YouTube groupies image

    https://www.youtube.com/watch?v=8-KDpQd1s1k

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    You can use these for some moderate power RF. The continuous ones are useful if you want to do some automatic Tuning .

    A mate of mine uses a remote arduino type thing with a motor to turn one of these caps to tune up a large loop antenna in the garden.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    :-) great thread. This conversation has made me want to build a radio now : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to jw0752

    They are in better condition than I thought. The smaller one I don't know much about (but has a geared drive - very cool) and the longer one is a Jackson Brothers one, with continuous rotation so would need some end-stops or cord drive I guess. It looks silver-plated, and is unused, so I've put it back in the bag in the box - I want a _really_ nice radio project to use that : )

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 11 years ago in reply to jw0752

    They are in better condition than I thought. The smaller one I don't know much about (but has a geared drive - very cool) and the longer one is a Jackson Brothers one, with continuous rotation so would need some end-stops or cord drive I guess. It looks silver-plated, and is unused, so I've put it back in the bag in the box - I want a _really_ nice radio project to use that : )

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Problemchild
    Problemchild over 11 years ago in reply to Problemchild

    I forgot to say that SOLDER SMOKE is a great old school pod cast done by this American guy out in Rome.

    I think it's the same chap who formulated the WSPR stuff correct me if I'm wrong?!?!?

     

    BTW Shabaz he has a bit on those SI5351 synthesizers Cool components had!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    Just had an idea I could use some plastic cogs to form a reduction gear to improve the tuning ..couldn't say the acrylic wasn't a good insulator ...probably good Permitivity  as well image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to Problemchild

    Ah! Good point. I've only seen the relay switched inductor/capacitor ones, for about 20W or so. The motor method would be way higher.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to shabaz

    You can use these for some moderate power RF. The continuous ones are useful if you want to do some automatic Tuning .

    A mate of mine uses a remote arduino type thing with a motor to turn one of these caps to tune up a large loop antenna in the garden.