Member's Forum Webasto make
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 631 subscribers
  • Views 904 views
  • Users 0 members are here
Related

Webasto make

e14 Contributor
e14 Contributor over 11 years ago

HI there

i whant to make something similar with a webasto sistem. Webasto is an auxiliary heating for cars. In my case i need 2 wather sensors and 2 relays or contacts. My sistem works like that ( in my imagination). I have from another car some incandescent plugs, that fits perfectly on heating pipes. From this plugs i have 2 wires, negative and positive for power and 2 relays for command. My point is: can i build, using arduino, one sistem that can start the plugs when is below 7 degres and stop them when are more than 40 degress ( celsius) ? What do i need?

THank you very much

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 11 years ago

    Could you simply use 2 bimetallic thermostat switches in series, one would open all temperatures above 40 and the other would open at all temperatures below 7 degrees - so both would only be closed between 7 and 40?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 11 years ago

    Could you simply use 2 bimetallic thermostat switches in series, one would open all temperatures above 40 and the other would open at all temperatures below 7 degrees - so both would only be closed between 7 and 40?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to dougw

    Thank you Paul and Douglas for your reply. On the car i have 4 plugs and 2 relays. i need that this plugs to light up when the outside temperature is below 7 and to close them when it reaches 40( inside wather temperature). This will help wather worm faster. In theory i need two temperature sensors, one outside and one in wather. on the arduino board can i use normal temperature sensors? My plan is to connect the board at car sensors. I have one sensor that displays outside temperature in dashboard, and second one displays the cooling sistem temperature. Do you think that i can do this with Arduino?

    THank you