Member's Forum Having sketch problems.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 630 subscribers
  • Views 747 views
  • Users 0 members are here
  • new_member_introduction
Related

Having sketch problems.

e14 Contributor
e14 Contributor over 11 years ago

I am having trouble with my sketch.  I am using an ultrasonic distance to activate relay.  Relay stays on all the time.

 

 

 

 

#define trigPin 12

#define echoPin 13

int relay2 = 2;

int i = 1000;

 

 

void setup() {

Serial.begin (9600);

pinMode(trigPin, OUTPUT);

pinMode(echoPin, INPUT);

pinMode(relay2, OUTPUT);

}

 

 

void loop() {

long duration, distance;

digitalWrite(trigPin, LOW);

delayMicroseconds(2);

digitalWrite(trigPin, HIGH);

delayMicroseconds(10);

digitalWrite(trigPin, LOW);

duration = pulseIn(echoPin, HIGH);

distance = (duration/2) / 29.1;

digitalWrite(2, LOW);

if (distance >= 25 || distance <= 2){

   Serial.println("Out of range");

}

if (i >= 4){

delay(i);

(distance >= 10);

(distance <= 8);

 

 

 

 

 

 

i = i/2;

}

  else {

   digitalWrite(2, HIGH);

   digitalWrite(2, LOW);

   Serial.print(distance);

   Serial.println(" in");

    delay(i);

  digitalWrite(2, LOW);

  delay(i);

digitalWrite(2, HIGH);

 

 

i = i/2;

}

delay(2000);

}

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    I dont understand why you have all the DigitalWrite(2, low) and (2,high) statements the way you do, the relay if it is mechanical will never responsd that quickly

     

    these two statements seem obsolete as they do nothing

    (distance >= 10);

    (distance <= 8);

     

    and your comparison to i starts out with i=1000 and will not execute the relay pulse untill i<=4 so that means i/2 +2000ms delay each time as I goes from 1000 to 3 so thats about

    (1000, 500, 250, 125, 62, 31, 16, 8, 4) 9*2000 = 20 or more seconds before the relay will do anything

     

    Then your delays get so small due to using i and never resetting it once it gets to almost zero from 1000 that the relay will apear to sit energised or not depending what a High value on the output does

     

    So now we know the issues, what is it you really want the code to so, use a flow chart or plain english description (Not Code)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    I Want the sonic distance to activate relay when distance is greater than 8" and  shut off relay when distance is 7".

    thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    So what the deal with the ever decreasing i variable then ??, can you explain what your doing with your code

     

    also there is a library for ultrasonic transducers that may make your life alot easier

    http://playground.arduino.cc/Code/NewPing

    http://forum.arduino.cc/index.php?topic=106043.0

     

    hope this helps

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    So what the deal with the ever decreasing i variable then ??, can you explain what your doing with your code

     

    also there is a library for ultrasonic transducers that may make your life alot easier

    http://playground.arduino.cc/Code/NewPing

    http://forum.arduino.cc/index.php?topic=106043.0

     

    hope this helps

     

    Peter