Member's Forum Doorbell Circuit Help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 634 subscribers
  • Views 1661 views
  • Users 0 members are here
  • monostable
  • reed_switches
  • bell
Related

Doorbell Circuit Help

pathfider1998
pathfider1998 over 10 years ago

Hello, I am quite new here, so don't be too harsh.

If this is in the wrong community, tell me where to move this post to so I can get appropriate help.

-------------------------------------------

 

This specific problem has been bugging me for a long time.

*UPDATED*

 

So I have this little old doorbell which uses 3V battery and a generic Normally-open switch of any type to operate.

The doorbell rings when two wires coming from the unit is shorted (connected together).

Minimal duration for the activation is about 0.1ms.

When the switch is closed and held, it rings continuously (ding-dong, 0.5 second delay, ding-dong, delay again...)

 

I was using reed switch (normally-closed) to on a sliding automatic door so the bell rings when the door is opened.

The problem is, the door closes quite slowly because of the safety function (it has been installed so the door doesn't trap hands or other objects), so the doorbell rings 5~6 times constantly while the door closes.

I do not want to annoy people nor I want to drain the battery too fast.

 

I needed something to pulse the transistor or a relay for a brief moment (so the bell rings) and stays off until the door is closed.

So I searched for the monostable circuit that uses 3V or less as a power source. It returned none. (Or, they didn't work as desired)

I tried using some generic 555 timers, but they drew too much power (4.5V) and was not qualified.

I want to avoid using Arduino or ATTiny (or LSxxxx) because they cost a lot here.

 

UPDATE: Here's the explanation:

1. The reed switch is connected parallel to the power in (Vcc) of the control circuit we are trying to build.

So when the magnet is taken away and the reed switch closes, the control circuit kicks in, and when the door closes and reed switch opens, only the control circuit shuts off.

2. The pulse should be sent only once no matter how slow the door closes or where the door is at. There must be no second ringer.

 

It doesn't need to be tiny, just small enough to fit inside the credit card when built on a breadboard (ignore the heights).

Could anyone help?

 

p.s. E14 really needs some sort of "Without Code", "Newcomer Friendly", "Not-a-Coder" or "Logic Gates Only" group.

Somewhere where people like me can ask about the most cost-effective/fool-proof way to make things happen without programming PICs or using ready-made solutions.

Or for people without access to advanced components like ATTiny or LS74xx.

 

Or just make it easier for people to look for communities without having to scroll down 940 miles just to find the end of the list.

(Or maybe I am just silly. Tell me about communities or groups I can join too)

 

Here's the circuit board. Maybe you guys can understand this better.

image

image

Plus: Pin 1 of IC marked, and components are highlighted.

image

  • Sign in to reply
  • Cancel
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    Hi Phil

     

    Welcome to the Element14 community. image

    Does your reed switch go open or closed circuit when the door is opened?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 10 years ago

    Hi Phil

     

    Welcome to the Element14 community. image

    Does your reed switch go open or closed circuit when the door is opened?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • pathfider1998
    0 pathfider1998 over 10 years ago in reply to gadget.iom

    It needs to go closed circuit (so it turns on the "single bleep" circuit until the door closes).

    It only needs to send ONE pulse to whatever electronically controlled switch I got so it rings the bell, then STOP sending the pulses so it stops ringing.