• Products and Partners
    Products and Partners
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
Member's Forum Very low powered light help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 12 answers
  • Subscribers 635 subscribers
  • Views 3260 views
  • Users 0 members are here
  • boost converter
  • light
Related

Very low powered light help

pathfider1998
pathfider1998 over 10 years ago

Hello again,
Here's a thing: I need to build something that takes generic 3V LEDs of (almost) any color, running at half+quarter (3/4) of its brightness, which uses generic components anyone can find in electronics components seller (like NPN transistor), takes 0.7V~1.5V, and lights LED until the sun comes up, which is about 6~10 hours.

It does not have to be using rechargeable batteries (it'll be great if they do however) but it must sense light so it turns off when the sun shines.

(Nobody likes to change batteries daily just to enjoy teeny tiny light)

 

It'll be almost mass-produced (~100 units, hand-assembled) so it needs to be very simple.

Its circuit will be based on matrix type breadboards (not Veroboard, which has strips of copper running along the rows) and it does not need to be very small.

 

Battery types will vary from generic AAA size cells to LR42/AG13 batteries.

Colors: Green / Blue / White / Warm White, 2.7V~3.3V <- This is not the voltage the boost converter should output! This is for reference only!

Since it will be running at half of its maximum brightness, the voltage could be lower.

 

More information:

The output of the boost converter ("joule thief") should be just enough to light a generic 3V LED just enough to be visible in a dark room (illuminating small area around it), as mentioned earlier.

It uses high intensity LEDs with clear lens (instead of diffused one). You know, those LEDs used in toys such as spinning tops.

The LEDs are running in limitless mode. (there are no current-limiting resistors)

The circuit could be very tiny in some cases. (1.3cm in diameter, excluding batteries)

It needs no smoothing. (30Hz~)

Manufacturing cost should be minimal as I can't order ready-made ICs now.

 

Updated: There were some misleading lines. They're fixed now. Sorry for the confusion!

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 10 years ago

    You have an unclear (to me anyway) goal, and you've already specified a few tight technical requirements and restrictions.

     

    This makes it hard to suggest any off-the-shelf design that will immediately suit all your requirements and restrictions, hence why people are suggesting you read around the subject of efficient LED lighting circuits, and low voltage lighting circuits.

     

    Generally if you have tightly defined restrictions in some areas (e.g. that specific voltage range) then you're going to need to design and experiment yourself, but you could use some existing web resources for ideas (even if it helps eliminate some ideas or helps you relax some of the tighter restrictions).

     

    By the way, no such thing as a generic 3V LED of almost any color, some colors (including some that you suggested) need a higher voltage than 3V. That difference matters significantly for voltage multiplying/boost type circuits if you're working with such low supply voltages as you suggest.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago

    You have an unclear (to me anyway) goal, and you've already specified a few tight technical requirements and restrictions.

     

    This makes it hard to suggest any off-the-shelf design that will immediately suit all your requirements and restrictions, hence why people are suggesting you read around the subject of efficient LED lighting circuits, and low voltage lighting circuits.

     

    Generally if you have tightly defined restrictions in some areas (e.g. that specific voltage range) then you're going to need to design and experiment yourself, but you could use some existing web resources for ideas (even if it helps eliminate some ideas or helps you relax some of the tighter restrictions).

     

    By the way, no such thing as a generic 3V LED of almost any color, some colors (including some that you suggested) need a higher voltage than 3V. That difference matters significantly for voltage multiplying/boost type circuits if you're working with such low supply voltages as you suggest.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • pathfider1998
    0 pathfider1998 over 10 years ago in reply to shabaz

    The post has been updated as it did not convey what I intended. Sorry for the confusion!

     

    p.s. The voltages and specs can be changed to minimum possible spec. Maybe I can make them work too.