• Products and Partners
    Products and Partners
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
Member's Forum Very low powered light help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 12 answers
  • Subscribers 635 subscribers
  • Views 3260 views
  • Users 0 members are here
  • boost converter
  • light
Related

Very low powered light help

pathfider1998
pathfider1998 over 10 years ago

Hello again,
Here's a thing: I need to build something that takes generic 3V LEDs of (almost) any color, running at half+quarter (3/4) of its brightness, which uses generic components anyone can find in electronics components seller (like NPN transistor), takes 0.7V~1.5V, and lights LED until the sun comes up, which is about 6~10 hours.

It does not have to be using rechargeable batteries (it'll be great if they do however) but it must sense light so it turns off when the sun shines.

(Nobody likes to change batteries daily just to enjoy teeny tiny light)

 

It'll be almost mass-produced (~100 units, hand-assembled) so it needs to be very simple.

Its circuit will be based on matrix type breadboards (not Veroboard, which has strips of copper running along the rows) and it does not need to be very small.

 

Battery types will vary from generic AAA size cells to LR42/AG13 batteries.

Colors: Green / Blue / White / Warm White, 2.7V~3.3V <- This is not the voltage the boost converter should output! This is for reference only!

Since it will be running at half of its maximum brightness, the voltage could be lower.

 

More information:

The output of the boost converter ("joule thief") should be just enough to light a generic 3V LED just enough to be visible in a dark room (illuminating small area around it), as mentioned earlier.

It uses high intensity LEDs with clear lens (instead of diffused one). You know, those LEDs used in toys such as spinning tops.

The LEDs are running in limitless mode. (there are no current-limiting resistors)

The circuit could be very tiny in some cases. (1.3cm in diameter, excluding batteries)

It needs no smoothing. (30Hz~)

Manufacturing cost should be minimal as I can't order ready-made ICs now.

 

Updated: There were some misleading lines. They're fixed now. Sorry for the confusion!

  • Sign in to reply
  • Cancel
Parents
  • gihu
    0 gihu over 10 years ago

    Hi

     

    There are many LED ic driver, for different currents, fixed or adjustable, with different topologies buck, boost... depending on input voltage, and how you connect LEDs in the output (single LEDs, or a string of several LEDs). If your power supply has lower voltage than the LEDs in the output, then chose a boost topology. Also, very important to know the current you want through the LED, as D_Hersey suggest, LED are typcally controlled by current.

     

    Hope that helps,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gihu
    0 gihu over 10 years ago

    Hi

     

    There are many LED ic driver, for different currents, fixed or adjustable, with different topologies buck, boost... depending on input voltage, and how you connect LEDs in the output (single LEDs, or a string of several LEDs). If your power supply has lower voltage than the LEDs in the output, then chose a boost topology. Also, very important to know the current you want through the LED, as D_Hersey suggest, LED are typcally controlled by current.

     

    Hope that helps,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer