• Products and Partners
    Products and Partners
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
Member's Forum Very low powered light help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 12 answers
  • Subscribers 635 subscribers
  • Views 3255 views
  • Users 0 members are here
  • boost converter
  • light
Related

Very low powered light help

pathfider1998
pathfider1998 over 10 years ago

Hello again,
Here's a thing: I need to build something that takes generic 3V LEDs of (almost) any color, running at half+quarter (3/4) of its brightness, which uses generic components anyone can find in electronics components seller (like NPN transistor), takes 0.7V~1.5V, and lights LED until the sun comes up, which is about 6~10 hours.

It does not have to be using rechargeable batteries (it'll be great if they do however) but it must sense light so it turns off when the sun shines.

(Nobody likes to change batteries daily just to enjoy teeny tiny light)

 

It'll be almost mass-produced (~100 units, hand-assembled) so it needs to be very simple.

Its circuit will be based on matrix type breadboards (not Veroboard, which has strips of copper running along the rows) and it does not need to be very small.

 

Battery types will vary from generic AAA size cells to LR42/AG13 batteries.

Colors: Green / Blue / White / Warm White, 2.7V~3.3V <- This is not the voltage the boost converter should output! This is for reference only!

Since it will be running at half of its maximum brightness, the voltage could be lower.

 

More information:

The output of the boost converter ("joule thief") should be just enough to light a generic 3V LED just enough to be visible in a dark room (illuminating small area around it), as mentioned earlier.

It uses high intensity LEDs with clear lens (instead of diffused one). You know, those LEDs used in toys such as spinning tops.

The LEDs are running in limitless mode. (there are no current-limiting resistors)

The circuit could be very tiny in some cases. (1.3cm in diameter, excluding batteries)

It needs no smoothing. (30Hz~)

Manufacturing cost should be minimal as I can't order ready-made ICs now.

 

Updated: There were some misleading lines. They're fixed now. Sorry for the confusion!

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 10 years ago

    The battery can be turned off during daylight with a cadmium sulfide sensor, resistor and a PFET.

    The LED can be driven from low voltage with an inductive relaxation oscillator, or any oscillator with an inductive flyback output. The circuit plus FET switch takes 2 or 3 transistors.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pathfider1998
    0 pathfider1998 over 10 years ago in reply to dougw

    Thanks for the info! Below is a slightly more detailed explanation for this project.

     

    I need to make a boost converter which outputs high voltage (relative to input voltage, of course) but with low amperes.

    This circuit is commonly known as "Joule Thief".

    I need to somehow make it shut off during daytime and work under batteries, which may or may not be rechargeable. (The circuit I am trying to build will have no support for charging, though)

     

    Agendas:

    • Make a high-V low-I boost converter, with minimal parts available basically anywhere
    • Make the circuit shut off during daytime and turn on during night
    • No microcontrollers allowed (due to its cost and possible hiccups during programming)
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 10 years ago in reply to pathfider1998

    What voltage do you need and what current?

    The LEDs mentioned wouldn't normally be classed as high voltage....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 10 years ago in reply to pathfider1998

    What voltage do you need and what current?

    The LEDs mentioned wouldn't normally be classed as high voltage....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • pathfider1998
    0 pathfider1998 over 10 years ago in reply to michaelkellett

    Could you explain why I can't use relaxation oscillator for this application? I am quite confused as many people out there were able to make RO run 3V LEDs, including those slightly high powered ones.

    Plus I am still a beginner. image

     

    p.s. The LED just needs to be lit dimly. Its minimum allowed current is 3/4 of "recommended driving current" of the LED I am going to use (as stated above).

    I am not saying I am going to run it with 3V 0.034mA output!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to pathfider1998

    Phil, you need to define the problem and then look for solutions that actually solve it. Never rule anything out until you have evidence.

     

    Your problem is not that you need an up converter - you want to get  a constant current into your LED and that may need more or less volts than the battery. You can't do that with a relaxation oscillator (I can't bring myself to call it a J**** T**** !!). I doubt very much if you can do it starting from 0.7V without using some quite pricey parts (you'll need a bought in boost converter that can start from about 0.5V (to give  a working margin from your spec of 0.7V) and then a second switcher to drive the LED efficiently. It may be that someone makes a chip that does all this in one part but I don't know of one.

     

    Often you start out with a spec and need to refine it because it has internal conflicts - I think that in your case the 0.7V and the constraints on the type of parts you want to use might be such a conflict - so you'll need to change soothing to get it any further.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pathfider1998
    0 pathfider1998 over 10 years ago in reply to dougw

    3V, generic white LED, 25mA(+/-10%, since no spec sheet was given).

    Input voltage ranges from 0.7V to 3V.

    The term "high voltage" is used very generously -- It means it's just higher voltage.