• Products and Partners
    Products and Partners
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
Member's Forum Problem with Honeywell ASDX Analog pressure sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 3 answers
  • Subscribers 632 subscribers
  • Views 2791 views
  • Users 0 members are here
  • pressure
  • pressure_sensor
  • honeywell
  • analog
  • sensor
Related

Problem with Honeywell ASDX Analog pressure sensor

e14 Contributor
e14 Contributor over 10 years ago

Dear friends

Few months ago I decide to built a multi channel pressure box, so I bought 16 Honeywell ASDX differential analog pressure sensor (Model: ASDX RRX005NDAA5). the datasheet of this type of sensor attached.

Base on datasheet, this sensor has 3 active pin, pin No.1 is for voltage supply, Pin No. 2 is Analog output and Pin No. 3 is GND.

image

I design a PCB board to mount all 16 sensors on a single board. I use a 5Vdc power supply device for PCB board, now when I TURN ON the device and there is no applied pressure on sensors (just ambient pressure), the output voltages are almost 2.47 - 2.49 Volt (I checked Pin 1 voltage for each sensors and all of them is same 5Vdc). the problems are here:

 

Problems:

1. I expect when there is no applied pressure, the output voltage be 2.5V but as i mentioned above it is a little less, what is the reason?  

2. when I applied an specific pressure (for example 300Pa) most sensors shows different voltage in their output and so it is impossible to calculate the Pressures. the datasheet said i can calculate pressure by below Eq.

 

image

 

3. by the changing of the pressure, change in output voltage of sensors are not equal. for example if I increase the Pressure 500Pa, the voltage change for one sensor is almost 1.5V but the voltage change for another sensor is 0.7V!!

I will be so appreciate if help me

Attachments:
imagehoneywell-sensing-asdx-series-analog-pressure-sensors-product sheet-008090-12-EN.pdf
  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 10 years ago

    Hi Ashkan,

     

    I noticed in the data sheet that the sensor is fairly linear between 10 inches of H2O as a minimum up to 100 psi as a maximum. I have done the conversions and the minimum of 10 inches of H2O is actually 2,500 Pa while the 100 psi corresponds to 689,000 Pa. Your 500 Pa is below the minimum level of pressure for the sensor to be in its linear range. If I misunderstood your experiment let me know. Otherwise I would try putting 10 kPa on the sensors to see if they are more consistent in their outputs. It will be important to stay between Pmin and Pmax for accurate output.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jw0752

    Dear John

    Thanks for your reply

    the sensor model that i use is -5\+5 inH2O

    And it is equal -1250/+1250 Pa

    i think the datasheet is for all ASDX series that contain ranges from 5inH2O to 100 PSI

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jw0752

    Dear John

    Thanks for your reply

    the sensor model that i use is -5\+5 inH2O

    And it is equal -1250/+1250 Pa

    i think the datasheet is for all ASDX series that contain ranges from 5inH2O to 100 PSI

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to e14 Contributor

    A few other things I can think of:

    1) are you using the correct voltage for the sensor (they do 5V and 3.3V parts)

    2) is the load > 5k

    3) have some been damaged - the damage pressure for a 5"H2O device is only 15" which is  a very low pressure.

    4) that capacitor as John mentioned already

     

    If it's none of these try posting your circuit and even some pictures.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi Ashkan,

     

    Sorry, I saw the spec. on the Data sheet and thought it might be the problem. I will keep thinking but you might be able to contact Honeywell for some tech support if nothing else. I see that they have some phone numbers at the end of the data sheet. Did you remember the external bypass capacitor between pins one and three?

     

    John