• Products and Partners
    Products and Partners
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
Member's Forum Problem with Honeywell ASDX Analog pressure sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 3 answers
  • Subscribers 632 subscribers
  • Views 2784 views
  • Users 0 members are here
  • pressure
  • pressure_sensor
  • honeywell
  • analog
  • sensor
Related

Problem with Honeywell ASDX Analog pressure sensor

e14 Contributor
e14 Contributor over 10 years ago

Dear friends

Few months ago I decide to built a multi channel pressure box, so I bought 16 Honeywell ASDX differential analog pressure sensor (Model: ASDX RRX005NDAA5). the datasheet of this type of sensor attached.

Base on datasheet, this sensor has 3 active pin, pin No.1 is for voltage supply, Pin No. 2 is Analog output and Pin No. 3 is GND.

image

I design a PCB board to mount all 16 sensors on a single board. I use a 5Vdc power supply device for PCB board, now when I TURN ON the device and there is no applied pressure on sensors (just ambient pressure), the output voltages are almost 2.47 - 2.49 Volt (I checked Pin 1 voltage for each sensors and all of them is same 5Vdc). the problems are here:

 

Problems:

1. I expect when there is no applied pressure, the output voltage be 2.5V but as i mentioned above it is a little less, what is the reason?  

2. when I applied an specific pressure (for example 300Pa) most sensors shows different voltage in their output and so it is impossible to calculate the Pressures. the datasheet said i can calculate pressure by below Eq.

 

image

 

3. by the changing of the pressure, change in output voltage of sensors are not equal. for example if I increase the Pressure 500Pa, the voltage change for one sensor is almost 1.5V but the voltage change for another sensor is 0.7V!!

I will be so appreciate if help me

Attachments:
imagehoneywell-sensing-asdx-series-analog-pressure-sensors-product sheet-008090-12-EN.pdf
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Dear John, Michael and Douglas

    thanks for your quick reply

     

    the below picture shows my device, sensors and board

    image

    let me answer your question one by one:

    1) are you using the correct voltage for the sensor (they do 5V and 3.3V parts)

         I use adjustable -+5 Vdc and set this power supply on 4.99V

    2) is the load > 5k

        dear Michael and Douglas, I don't use any resistance on pin 2

    3) have some been damaged - the damage pressure for a 5"H2O device is only 15" which is  a very low pressure.

        I use this sensor in a low speed wind tunnel (the MAX speed is around 45 m/s and it is equal to  1113.7 Pa), so I don't think sensors damaged

    4) Capacitor

         I use one 100nF before any Vss pin of each sensor

     

    do you think the problem may be caused for the way i connect sensor to pneumatic connector? (see below picture)

    actually I am a mechanical engineering graduate and not very familiar with electronic details, can i use a 10 Kohm resistor? and do I use this resistor on output (Pin 2)

      imageimageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi Ashkan,

    I believe that dougw and michaelkellett have solved your mystery. The minimum load of 5K would be necessary for proper operation. 10K would be outside of specifications and might not work properly just as no load does not seem to work properly. If you can't find 5K resistors to put between pin 2 and ground then perhaps the more common 4.7K will be available. Since this is a precision instrument is is probably a good idea to match the resistors or get 1% values. This may not make a big difference but it is good procedure. Keep in mind that whatever circuitry that you feed the outputs of the sensors into will also contribute to the load. Right now the only load is probably the 1 meg or so of load imposed by your meter.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to jw0752

    The way I read the data sheet is that the load resistance should not be less than 5k - so no load resistor should be OK.

     

    @ Ashkan - are your sensors the 5V type  (what's the part number written on them ).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to jw0752

    The way I read the data sheet is that the load resistance should not be less than 5k - so no load resistor should be OK.

     

    @ Ashkan - are your sensors the 5V type  (what's the part number written on them ).

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer