• Products and Partners
    Products and Partners
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
Member's Forum Problem with Honeywell ASDX Analog pressure sensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 3 answers
  • Subscribers 632 subscribers
  • Views 2791 views
  • Users 0 members are here
  • pressure
  • pressure_sensor
  • honeywell
  • analog
  • sensor
Related

Problem with Honeywell ASDX Analog pressure sensor

e14 Contributor
e14 Contributor over 10 years ago

Dear friends

Few months ago I decide to built a multi channel pressure box, so I bought 16 Honeywell ASDX differential analog pressure sensor (Model: ASDX RRX005NDAA5). the datasheet of this type of sensor attached.

Base on datasheet, this sensor has 3 active pin, pin No.1 is for voltage supply, Pin No. 2 is Analog output and Pin No. 3 is GND.

image

I design a PCB board to mount all 16 sensors on a single board. I use a 5Vdc power supply device for PCB board, now when I TURN ON the device and there is no applied pressure on sensors (just ambient pressure), the output voltages are almost 2.47 - 2.49 Volt (I checked Pin 1 voltage for each sensors and all of them is same 5Vdc). the problems are here:

 

Problems:

1. I expect when there is no applied pressure, the output voltage be 2.5V but as i mentioned above it is a little less, what is the reason?  

2. when I applied an specific pressure (for example 300Pa) most sensors shows different voltage in their output and so it is impossible to calculate the Pressures. the datasheet said i can calculate pressure by below Eq.

 

image

 

3. by the changing of the pressure, change in output voltage of sensors are not equal. for example if I increase the Pressure 500Pa, the voltage change for one sensor is almost 1.5V but the voltage change for another sensor is 0.7V!!

I will be so appreciate if help me

Attachments:
imagehoneywell-sensing-asdx-series-analog-pressure-sensors-product sheet-008090-12-EN.pdf
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Dear Friends

    thanks for your helps, your answer inspired me to solving this problem.

    i use a 4.7Kohm with 1% accuracy resistor but my problem not solved, so i decide to connect the tubes to sensor directly (I used to use Pneumatic connector for connecting tubes to sensor) and after that i saw it's worked. all the sensor shows same pressure.)

    i think because these sensors are ultra-Low pressure sensors (-1250/+1250 Pa) using usual pneumatic connection is not a good Idea.

    I learn a lot of your answers and thanks so Much for your answers and your time

     

    Best Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Dear Friends

    thanks for your helps, your answer inspired me to solving this problem.

    i use a 4.7Kohm with 1% accuracy resistor but my problem not solved, so i decide to connect the tubes to sensor directly (I used to use Pneumatic connector for connecting tubes to sensor) and after that i saw it's worked. all the sensor shows same pressure.)

    i think because these sensors are ultra-Low pressure sensors (-1250/+1250 Pa) using usual pneumatic connection is not a good Idea.

    I learn a lot of your answers and thanks so Much for your answers and your time

     

    Best Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer