• Products and Partners
    Products and Partners
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
Member's Forum in need of help lcd
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 633 subscribers
  • Views 683 views
  • Users 0 members are here
Related

in need of help lcd

e14 Contributor
e14 Contributor over 10 years ago

im in need of some help guys and girls

 

i have salvaged lcd from a epson sx420 scanner printer its a 1.6" screen and there are very few markings on it. I would love to use this for some of my arduino projects but i cant seem to find a data sheet for it so i have no idea of the pinout for the screen i have attached a couple of images to try to help any ideas guys would be great

http://imgur.com/XmG6iI4

http://imgur.com/11aegD4

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    LCD Screen    

    3.8 cm colour

    from http://www.auo.com/?sn=135&lang=en-US

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jack.chaney56
    0 jack.chaney56 over 10 years ago in reply to clem57

    I have a question related to LCD screens, and Clem seems to be one of the Go-To people (at least he responds in a helpful manner).

     

    I understand that the writing of interface software is part of the dark arts, and proper robing is needed to perform the activity, but, why is there always such a mystery about the interface registers for LCD drivers.  The spec sheets only go as far as the RGB pins for the LCD, but devices akin to the ST7735, that actually create the raster signals are always shrouded in mystery.  Most times whey I try to dissect instructions and messages getting transferred to the controller, I come across comments like "don't understand this one", or "this one works", or the best "what I was told to use".  I get that most of the information is coming from the manufacturer and needs at least three or four levels of translation, but if there are standards or real sources for spec sheets, I would find that extremely helpful.

     

    This is mostly because I get interface code from vendors, that provides a user level that kind of meets requirements as interpreted by their engineers (some people shouldn't write code), and like most engineer types, I think I can do better, if I had the information.

     

    Thanks,

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jack.chaney56
    0 jack.chaney56 over 10 years ago in reply to clem57

    I have a question related to LCD screens, and Clem seems to be one of the Go-To people (at least he responds in a helpful manner).

     

    I understand that the writing of interface software is part of the dark arts, and proper robing is needed to perform the activity, but, why is there always such a mystery about the interface registers for LCD drivers.  The spec sheets only go as far as the RGB pins for the LCD, but devices akin to the ST7735, that actually create the raster signals are always shrouded in mystery.  Most times whey I try to dissect instructions and messages getting transferred to the controller, I come across comments like "don't understand this one", or "this one works", or the best "what I was told to use".  I get that most of the information is coming from the manufacturer and needs at least three or four levels of translation, but if there are standards or real sources for spec sheets, I would find that extremely helpful.

     

    This is mostly because I get interface code from vendors, that provides a user level that kind of meets requirements as interpreted by their engineers (some people shouldn't write code), and like most engineer types, I think I can do better, if I had the information.

     

    Thanks,

     

    Jack

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jack.chaney56

    The "mystery" issues persist because there is very little standardization for hardware-interfacing, much less software (tail follows the donkey).  Each vendor is protecting its market niche.  Provide $$$ incentive and then the vendors will change behavior.  This is the same situation that we used to have with floppy disks in the 1970s until the MS-DOS/PC forced everyone to provide standardized connections if they (the vendors) wanted to play in the "standard" sand box, thus, providing financial incentive for all.  As a side-effect, the floppy (and other peripherals too) vendors costs were reduced over time through the standardization.  Consumer price tag was lower.  Win-win-win.

     

    So, today, LCD vendors are operating "on the frontier", looking over their shoulders, just like the other SoC peripheral makers.  Will history repeat itself?