Member's Forum Using 12v at base of transistor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 29 replies
  • Answers 10 answers
  • Subscribers 631 subscribers
  • Views 8146 views
  • Users 0 members are here
  • transistor
  • 12v
  • car
Related

Using 12v at base of transistor

ntewinkel
ntewinkel over 10 years ago

Hi all,

 

I'm thinking of using a transistor in a car circuit, to switch a light depending on the state of another light.

 

So it will be 12v as the signal at the base of the transistor.

 

I have a bunch of pn2222a transistors, and I can't figure out from the datasheet what the maximum means for that. It seems to be a reverse maximum (ie, don't let the output be more than 5v over the base voltage).

 

So the question is - is it possible to switch a transistor like that using 12v at the base?

 

Thanks!

-Nico

 

ps, I know I can easily do this using relays, but those take up more space, and I'd prefer to avoid the mechanical bits.

  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 10 years ago

    I'm not sure this state table is what you have, but once the states are populated, the logic to derive each state can be determined.

    It the table your vehicle controls (in blue) generate control signals (in green) and you want the output signals in yellow and red.

    The output signals must be derived from the green control signals. there are only 2 control signals, but they each have five states (off, on dim, on full, flashing off-on and flashing dim-on) The darker colours indicate flashing on-dim. If I have it right, there are 14 input states and 11 output states.

    This doesn't need a microcontroller to sort out as your yellow turn signals only have 2 states and your tail lights follow the green control signals, except when the yellow signals are flashing. The dim condition doesn't matter if you use the green signals as power rails for your tail lights. etc.

    Some states are not possible because, for instance, the left and right turn controls cannot indicate both at the same time.

    In order to figure out the state it is necessary to detect flashing. The two types of flashing don't matter, but it is harder to detect flashing because it isn't always the same.

           

    I-STATE 0124358910121113161716161717
    ControlsLightsOFFONOFFOFFONONOFFONOFFOFFONONOFFONOFFOFFONON
    ControlsLeft SignalOFFOFFONOFFONOFFOFFOFFONOFFONOFFOFFOFFONOFFONOFF
    ControlsRight SignalOFFOFFOFFONOFFONOFFOFFOFFONOFFONOFFOFFOFFONOFFON
    ControlsBrakesOFFOFFOFFOFFOFFOFFONONONONONONFLASHINGFLASHINGFLASHINGFLASHINGFLASHINGFLASHING
    InputsLeft WireOFFDIMFLASHINGOFFFLASHINGOFFONONFLASHINGOFFFLASHINGONFLASHINGFLASHINGFLASHINGFLASHINGFLASHINGFLASHING
    InputsRight WireOFFDIMOFFFLASHINGOFFFLASHINGONONONFLASHINGONFLASHINGFLASHINGFLASHINGFLASHINGFLASHINGFLASHINGFLASHING
    OutputsLeft TurnOFFOFFFLASHINGOFFFLASHINGOFFOFFOFFFLASHINGOFFFLASHINGOFFOFFOFFFLASHINGOFFFLASHINGOFF
    OutputsRight TurnOFFOFFOFFFLASHINGOFFFLASHINGOFFOFFOFFFLASHINGOFFFLASHINGOFFOFFOFFFLASHINGOFFFLASHING
    OutputsLeft TailOFFDIMOFFOFFDIMDIMONONONONONONFLASHINGFLASHINGFLASHINGFLASHINGFLASHINGFLASHING
    OutputsRight TailOFFDIMOFFOFFDIMDIMONONONONONONFLASHINGFLASHINGFLASHINGFLASHINGFLASHINGFLASHING
    O-STATE012345667878910991010

    Note the brakes can be flashing if you pump the brakes - you don't want this to cause turn signals to come on unless the turn signals are also on.

    I am not sure there is enough information in the control signals to know what is going on if you pump the brakes at the same rate as the turn signal flashes - while they are flashing.

    If you use a flashing detector, it will delay your turn signal activation.

    I hope this doesn't look too confusing and complicated - it is just trying to set up a way to document what you and Michael have been saying in words, and in translating to a circuit, it should simplify to something similar to what you and Michael have been designing.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to dougw

    Thanks for all that, Douglas!

     

    It's after midnight, so I'll keep it quick, and check in more detail later, but we can reduce the table a little bit: there is no "Dim" - the lights have a separate wire and separate bulbs/LEDs on the trailer, so we can ignore anything to do with night-lighting for the logic. The signals get a full 12v when on.

     

    Thanks!

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to dougw

    Thanks for all that, Douglas!

     

    It's after midnight, so I'll keep it quick, and check in more detail later, but we can reduce the table a little bit: there is no "Dim" - the lights have a separate wire and separate bulbs/LEDs on the trailer, so we can ignore anything to do with night-lighting for the logic. The signals get a full 12v when on.

     

    Thanks!

    -Nico