Member's Forum Triac not shutting off (24v AC sprinkler valve control)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 16 answers
  • Subscribers 631 subscribers
  • Views 7614 views
  • Users 0 members are here
  • valve
  • ac
  • triac
  • sprinkler
  • 24v
  • opensprinkler
Related

Triac not shutting off (24v AC sprinkler valve control)

ntewinkel
ntewinkel over 10 years ago

Hi All,

 

I'm working on replacing my aging and broken sprinkler controller, and found some open source software (OpenSprinkler) to run on a Raspberry Pi that handles the scheduling very nicely (plus it has an app for my phone).

With that software I'm able to control a couple of shift registers to turn LEDs on and off, simulating the sprinkling zones.

 

I'm not very familiar with TRIACs (read: not at all familiar, never used them before image), but recently I learned that the sprinkler valves use 24v AC and that TRIACs would be a good way to switch them, with relays generally being rather big once you get 16 of them lined up, and regular power transistors only being good for DC.

 

I bought some BRT12H "non-zero crossing" opto-isolating TRIACs (datasheet: http://www.vishay.com/docs/83689/83689.pdf), because they seemed to meet the desirements of opto-isolating and AC for 250mA.

 

I hooked them up (with 220ohm resistors from shift registers to TRIACs), and it all looked promising when I turned the first zone on (sprinklers worked, yay!), but then it wouldn't shut off (sprinklers still working, not yay!). It only shuts off if I remove the 24v power momentarily.

 

I've done some Googling around but have not yet found any solution, and to be honest it's not making a whole lot of sense to me (yet... hopefully yet).

 

I did find out that TRIACs (in general?) need to cross zero (volts?) to turn off. I'm not sure what this "non-zero crossing" bit means but I have a nagging suspicion that it's a key part of the issue.

Should I have bought "zero crossing" TRIACs instead?

 

Can anyone help shed some light?  ...and hopefully also shed a solution image

 

ps, I did see that I can buy a pre-built board for not too expensive (about $80 after shipping and taxes), but it's a cool DIY project and it would be far more satisfying (and educational) to build it myself.

 

edit: While doing more searching for answers I noticed that SSRs (solid state relays) do exist that are tiny chips, like this one, DIP-8: http://www.sharpsma.com/webfm_send/335  - very cool.

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    http://www.onsemi.com/pub_link/Collateral/AN1048-D.PDF

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 10 years ago

    http://www.onsemi.com/pub_link/Collateral/AN1048-D.PDF

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to D_Hersey

    So if I figured this out correctly, the "snubber" consists of a capacitor and resistor in series on the output (ie, triac output pin A to capacitor to resistor to output pin B).

     

    All the calculations make my eyes water and make me realize that I'm missing a few years of electrical engineering in order to figure this out completely image

     

    The closest I can figure out, assuming 250 mA for the solenoid and from what I think are the correct values from the BRT12H datasheet is this:

    capacitor = about 10 nF ( = 0.01uF = 103 ?)

    resistor = about 620 ohm

     

    Does that sound like it's in the ballpark?  Also, how big is the ballpark? are those values strict or can I swap in some other capacitor values? I have a neat arrangement of resistor values, but the capacitors are of the "grab bag" variety and specific values are kinda hard to find. image

     

    Also, do I need a separate snubber for each triac or can they all share one set? In my case, only 1 triac will ever be on at one time.

     

    Thanks,

    -Nico