Member's Forum Triac not shutting off (24v AC sprinkler valve control)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 16 answers
  • Subscribers 631 subscribers
  • Views 7601 views
  • Users 0 members are here
  • valve
  • ac
  • triac
  • sprinkler
  • 24v
  • opensprinkler
Related

Triac not shutting off (24v AC sprinkler valve control)

ntewinkel
ntewinkel over 10 years ago

Hi All,

 

I'm working on replacing my aging and broken sprinkler controller, and found some open source software (OpenSprinkler) to run on a Raspberry Pi that handles the scheduling very nicely (plus it has an app for my phone).

With that software I'm able to control a couple of shift registers to turn LEDs on and off, simulating the sprinkling zones.

 

I'm not very familiar with TRIACs (read: not at all familiar, never used them before image), but recently I learned that the sprinkler valves use 24v AC and that TRIACs would be a good way to switch them, with relays generally being rather big once you get 16 of them lined up, and regular power transistors only being good for DC.

 

I bought some BRT12H "non-zero crossing" opto-isolating TRIACs (datasheet: http://www.vishay.com/docs/83689/83689.pdf), because they seemed to meet the desirements of opto-isolating and AC for 250mA.

 

I hooked them up (with 220ohm resistors from shift registers to TRIACs), and it all looked promising when I turned the first zone on (sprinklers worked, yay!), but then it wouldn't shut off (sprinklers still working, not yay!). It only shuts off if I remove the 24v power momentarily.

 

I've done some Googling around but have not yet found any solution, and to be honest it's not making a whole lot of sense to me (yet... hopefully yet).

 

I did find out that TRIACs (in general?) need to cross zero (volts?) to turn off. I'm not sure what this "non-zero crossing" bit means but I have a nagging suspicion that it's a key part of the issue.

Should I have bought "zero crossing" TRIACs instead?

 

Can anyone help shed some light?  ...and hopefully also shed a solution image

 

ps, I did see that I can buy a pre-built board for not too expensive (about $80 after shipping and taxes), but it's a cool DIY project and it would be far more satisfying (and educational) to build it myself.

 

edit: While doing more searching for answers I noticed that SSRs (solid state relays) do exist that are tiny chips, like this one, DIP-8: http://www.sharpsma.com/webfm_send/335  - very cool.

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    Sometimes, snubbers are needed with relays as well.  The inductive spike can pit or weld the contacts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to D_Hersey

    Aww man! There's no getting away from this lesson on snubbers, is there?

     

    I was having no luck with the R(620ish)-C(10nF) attempt - the valve stayed on, so I'll have to revisit that math. I've also set it up on a separate little breadboard for easy testing.

     

    So to make sure I'm heading towards the right path, is the snubber designed based on the inductive load then (in my case the sprinkler valve) ? (as opposed to the triac ratings?)

     

    And what is the best way to figure out the values? My multimeter can check for inductance of the sprinkler valve coil. And I can get the Amps used. Or can it all be based on the general values that most 24v sprinkler valves have?

     

    Thanks,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to ntewinkel

    Personally I don't think the snubber is going to resolve your issues.

     

    The load size is not enough to generate large spikes that will overwhelm or damage the switching components.

    It is also not likely to cause EMC, as you're using solid state devices, rather than contacts.

    The frequency of switching is not high so again unlikely to cause EMC.

     

    One of our members of another club has been killing solenoids, and it seems it is due to DC.

    However he's switching AC so I'm not 100% on how he's getting a DC component in the solenoids.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to mcb1

    One of our members of another club has been killing solenoids, and it seems it is due to DC.

    However he's switching AC so I'm not 100% on how he's getting a DC component in the solenoids.

     

    I was reading about that on OpenSprinkler.com (Understanding 24VAC Sprinkler Valves « RAYSHOBBY.NET - paragraph at bottom) - seems that DC causes it to draw far more current. Apparently he was able to make the 24AC valves work well using 9v, by giving it a quick 12v burst to activate the solenoid and then using 9v dc to hold it.

     

    That's something I'm interested in trying at some point too, given that 9v adapters are smaller and easier to find, and work well with my favourite dev environments.

     

    OpenSprinkler has schematics available, and it looks like they just use triacs (not opto-isolated), and I don't see any snubber parts. The only other parts around the triacs are MOVs that they use for protection from outside issues: "Also solder the 10 metal oxide varistors (MOVs). Each MOV is a blue, disc-shaped component. It’s non-polar, and its main purpose is to absorb transient high voltage and protect the circuit from power surge or lightening."

    https://github.com/rayshobby/opensprinkler/tree/master/OpenSprinkler%20Controller/hardware/v2.2

     

    Which is why I'm thinking maybe the BRT12H was a bad choice.

     

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 10 years ago in reply to mcb1

    One of our members of another club has been killing solenoids, and it seems it is due to DC.

    However he's switching AC so I'm not 100% on how he's getting a DC component in the solenoids.

     

    I was reading about that on OpenSprinkler.com (Understanding 24VAC Sprinkler Valves « RAYSHOBBY.NET - paragraph at bottom) - seems that DC causes it to draw far more current. Apparently he was able to make the 24AC valves work well using 9v, by giving it a quick 12v burst to activate the solenoid and then using 9v dc to hold it.

     

    That's something I'm interested in trying at some point too, given that 9v adapters are smaller and easier to find, and work well with my favourite dev environments.

     

    OpenSprinkler has schematics available, and it looks like they just use triacs (not opto-isolated), and I don't see any snubber parts. The only other parts around the triacs are MOVs that they use for protection from outside issues: "Also solder the 10 metal oxide varistors (MOVs). Each MOV is a blue, disc-shaped component. It’s non-polar, and its main purpose is to absorb transient high voltage and protect the circuit from power surge or lightening."

    https://github.com/rayshobby/opensprinkler/tree/master/OpenSprinkler%20Controller/hardware/v2.2

     

    Which is why I'm thinking maybe the BRT12H was a bad choice.

     

    -Nico