• Products and Partners
    Products and Partners
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
Member's Forum Ellie tries to hack a Retron 5 controller into something that doesn't suck.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Answers 6 answers
  • Subscribers 631 subscribers
  • Views 4429 views
  • Users 0 members are here
  • controller
  • hack
  • retro
  • retron 5
  • video games
Related

Ellie tries to hack a Retron 5 controller into something that doesn't suck.

mistsonata
mistsonata over 9 years ago

(This post is very long and has lots of pictures. If you're here to help, but don't want the whole storytime thing feel free to skip to the summary at the end.)

 

So here's the thing, I'm basically a total amateur. I only started soldering earlier this year, and I still understand very little about electronics and how they work. But that's never stopped me from doing stupid things before.

 

Right now, the stupid thing I'm doing is trying to make a Retron 5 controller into something that doesn't suck. I love my Retron 5, but its wireless bluetooth controller is awful. It's clicky, it's got this weird pseudo-analog stick style d-pad, it feels light and cheap, and it's just all around uncomfortable to hold. I've got an 8bitdo SFC30 as my go-to Retron wireless controller, but I have to do a weird button combo to get into the menu and not all of the buttons are represented on the controller, and I just want something easier.


Initially my first plan was to hotwire the inputs from a different controller to the PCB on the Retron controller. So the first step was to take apart the Retron controller to see what I was working with, and that's when I was met with my first lucky break.

 

 

93hBX11.jpg?1

Half of the work has already been sorta done for me here, with the directional inputs as well as L1 and L2 already set up to be wired to another PCB. All I really have to do is figure out what to do for the other buttons and I'm set, right? Well, maybe not.

 

I needed to find a controller that would fit the PCB inside, or at least would be easy to mod so that it could fit inside. For a while I was looking to the Xbox 360 controller, which has lots of room, but I decided that the subpar d-pad wasn't worth it. For a while I was actually considering the Xbox One controller, but every broken xbone controller I've been able to get my hands on so far has been either easily fixable or there's nothing wrong with them in the first place, and they're too nice for PC gaming to take apart (and besides they have a really weird thing going where one of the face buttons is actually connected to the first PCB and it was a little too complicated for me). That's when I turned to the Dualshock 3 and stumbled across my second lucky break.

 

fQ32N8e.jpg?1

 

The DS3 has a great d-pad, four buttons as well as two sets of shoulder and trigger buttons, and it's set up so that I can easily attach a bunch of ribbon cable to pretty much everything except the analog sticks and L3/R3 (just don't mind the shoddy soldering job). Not only that, but if I take the second DS3 PCB out, everything on the input PCB but the middle area are fully supported and don't need any backing to keep it steady. Unfortunately, I don't have everything going for me, as the space inside the DS3 controller is still pretty cramped, and I don't think I could fit the Retron controller PCB as is. So, I'm pretty sure I'm going to try to cut the PCB up and remove what I don't really need.

 

Now, this is a bit of a tall order for me, as I have no idea what almost all of these little metal components on the Retron PCB are supposed to do, and I couldn't find a schematic of the board online, but I think I've got a way to make it quite a bit smaller. I couldn't find a schematic for this piece of hot garbage online (not that I know much about reading schematics anyway), so I had to improvise.

 

gjb2I2I.png?1

 

I pulled some of the pictures I took into photoshop and started mapping out what connects to what, with particular emphasis on the inputs. The red lines are paths I found on the front, and the blue lines are paths that I found on the back. The small green dots are the holes where I'm pretty sure the paths are passing through to one side or the other. The purple circles are surface leads, mostly located on the back. I've highlighted where I believe the paths from the button inputs come from in yellow, and right now my initial plan is to cut the PCB where those yellow lines end, up and down the board. As for the bluetooth antenna, I'll either cut around it or remove it and connect it to the PCB again with a wire. In theory this should slim up the PCB quite a bit, but not enough to be able to fit in the DS3 (especially if I want the USB cable to be in the right place) so I'm still a bit stuck there, and I may have to make a bit of a modification to the controller. I feel like I might be able to cut off the bit with the indicator lights and rewire them so that they're near the USB port like they are on the controller, but I'm getting too far ahead of myself, because while testing out the DS3's PCB I came across a potential problem.

 

I have a cheap, dinky continuity tester that I've been using to poke around and see what connects to what, and up until this point I've been able to get a good idea of which lead sends signals and which do not. I've tested a bunch of the surface leads to make sure I knew where the ground was, I've tested the buttons to make sure I know which prong sends the signal when it's pressed, but when I tried to test the DS3's inputs to make sure that pressing buttons actually sends a signal to the wires, I get nothing. On the shoulders and triggers, there's a very basic circuit, one path splits off and connects to the pads that the other two leads connect to, and pressing down the little rubber contact pad onto it gives me nothing for any of these buttons, left or right, even after extensive cleaning.

 

So to sum up, I'm trying to take a Retron 5 controller and connect it to the button pad PCBs from a Dualshock 3. I'm planning on cutting up the Retron PCB around where the yellow lines on the above diagram end, but unfortunately I've been testing the DS3 PCB and pressing buttons doesn't connect a circuit between either the ground or the "ADCC" or "ADCD" lines (no idea what those mean, and google doesn't reveal anything, but I suspect it has something to do with power) and what I'm wondering now is if the button inputs work differently between these two PCBs (in which case, this project may be screwed unless I can figure out a workaround), or if maybe every button in this DS3 PCB is broken (I doubt it, but it's possible). I've checked the continuity between the solder joints and the wires and everything. It doesn't make sense to me.

 

There are some other concerns I have, including the fact that there's a symbol on the Retron board that looks like the symbol underneath one of the capacitors (a circle with a bunch of lines on one side) and I'm wondering if there's supposed to be a capacitor there. I'm also wondering if I need to make sure that the blue line running along the diagonal line on the side of it needs to be connected to something (I'm guessing it's supposed to have power coming through it, so I might be able to connect it to where the power's supposed to go on the DS3, either "ADCC" or "ADCD").

 

Here's a link to all the pictures I've taken so far in case there's some info I'm missing. Even if you don't feel like offering advice, I'm sure I'll figure things out myself in time. If I end up screwing up and breaking everything here, I'll at least have learned something (I hope). If you have any suggestions for me, though it would really help. Thank you!

  • Sign in to reply
  • Cancel
Parents
  • spannerspencer
    0 spannerspencer over 9 years ago

    Okay, I think I've found it. I know this isn't exactly what you're wanting to do, but I think it might be your best option for swapping out the awful RetroN wireless controller with something better.

     

    A company called 8BitDo makes retro-styled wireless controllers for iOS and Android (primarily, but they're bluetooth -- you can use them for pretty much anything). A little while ago they released a variation on the controllers' firmware, that makes then compatible with the RetroN5.

     

    From what I've read, it can be a bit of a headache getting them set up, and you have to install new firmware on the controller itself before it'll work, but these are seriously nice devices! I like the NES30 Pro, especially:

    image

     

    Here's a bit more reading on the subject of updating the firmware for these controllers, in case that's a route you think you might try. Keep us posted!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mistsonata
    0 mistsonata over 9 years ago in reply to spannerspencer

    Hi Spencer! Thanks so much for taking the time to help.

     

    I actually already knew about the 8bitdo controllers and their ability to function in Retron5 mode, I even mentioned in my original post that my SFC30 is my go-to wireless controller for the Retron. This project was just something I wanted to do, because I had the Retron controller lying around and I wanted to try to do something with it, so if I ended up with a controller that no longer worked it wouldn't be a big deal. Never practice on something you're not ready to throw away and all that. I had no idea that the NES30 pro had so many buttons though, so I might actually be getting one of those for the future just for the extra buttons on the bottom.

     

    Unfortunately, it looks like shabaz was right. I managed to get everything hooked up and working really well, but the moment I tried to cut it, rewire it, and fit it into the controller (an ordeal unto itself) there was a lot of lag and most of the buttons weren't really responsive. It DID work, though, even if the performance was now just too poor to play with. I may come back to it in the future, but for now I think I'll set it aside until I've got some more experience under my belt.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • spannerspencer
    0 spannerspencer over 9 years ago in reply to mistsonata

    Ah, that's a shame about the lag. Another thought did occur in the meantime, that you could pretty easily build an arcade controller much like those on the PIK3A and PIK3A Mk II, as the microswitches for the joystick and buttons could simply piggyback onto the RetroN controller's PCB. That'd be a fairly simple, and pretty cool project, and it'd be way better than the RetroN's controller!

     

    And apologies for totally missing that you'd already had a go with 8BitDo's stuff! image  How did it go with that, by the way? Did you have to update the controller's firmware and re-pair it with the RetroN5?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mistsonata
    0 mistsonata over 9 years ago in reply to spannerspencer

    Yeah, I kind of wish I were more into the arcade style controllers so that space was less of an issue. Unfortunately I didn't frequent the arcades, and a home console controller is more familiar to my hands. If I feel like it in the future I might try to make something small like something akin to the SNES/NES Advantage controller, so I'll probably bookmark those links for future reference. I'm thinking of doing a retropie project next, though.

     

    As for the 8bitdo controllers, I love them (I have multiple), and they work really well with the Retron 5, you just have to hold down the L button while pressing start to put it into Retron mode. You don't really have to update the firmware more than once I've found, but thinking about it now I probably should. You also have to adjust to the weird switch between button mappings on your games and the button mappings that the Retron 5 forces you to use in the menus (I think there might be a way to fix that on the 8bitdo end, though now that I think of it).

     

    If you're into playing with the original retro console hardware, by the way, 8bitdo has wireless bluetooth receivers for both the NES and SNES that work with their controllers, it's pretty amazing stuff. They can even act as bluetooth dongles for your PC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mistsonata
    0 mistsonata over 9 years ago in reply to spannerspencer

    Yeah, I kind of wish I were more into the arcade style controllers so that space was less of an issue. Unfortunately I didn't frequent the arcades, and a home console controller is more familiar to my hands. If I feel like it in the future I might try to make something small like something akin to the SNES/NES Advantage controller, so I'll probably bookmark those links for future reference. I'm thinking of doing a retropie project next, though.

     

    As for the 8bitdo controllers, I love them (I have multiple), and they work really well with the Retron 5, you just have to hold down the L button while pressing start to put it into Retron mode. You don't really have to update the firmware more than once I've found, but thinking about it now I probably should. You also have to adjust to the weird switch between button mappings on your games and the button mappings that the Retron 5 forces you to use in the menus (I think there might be a way to fix that on the 8bitdo end, though now that I think of it).

     

    If you're into playing with the original retro console hardware, by the way, 8bitdo has wireless bluetooth receivers for both the NES and SNES that work with their controllers, it's pretty amazing stuff. They can even act as bluetooth dongles for your PC.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer