• Products and Partners
    Products and Partners
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
Member's Forum I think this is a buck converter, but I'm not entirely sure.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 3 answers
  • Subscribers 632 subscribers
  • Views 2573 views
  • Users 0 members are here
Related

I think this is a buck converter, but I'm not entirely sure.

capacitance_incarnate
capacitance_incarnate over 9 years ago

So I have this little chip here from a cigarette lighter psu, but there isn't a voltage regulator any where in it. If this is indeed a buck converter, that would explain the lack of a regulator, but I'm new to this kind of stuff, (I first got into it  while creating a project for school last year) so I would appreciate any help I can get.

imageimageimage

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Jake,

     

    That is a voltage regulator, also known as a DC-DC converter or a Buck converter when it uses an inductor and switching and steps down the voltage.

    You could confirm by examining the part code on the integrated circuit, and obtain the datasheet for the part online. It is extremely likely to be MC34063 (or similar) because that is common in low-cost USB car chargers (and from the photo, the pinout looks about right for that).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • capacitance_incarnate
    0 capacitance_incarnate over 9 years ago in reply to shabaz

    Thanks so much! I'm assuming the input voltage would be 12v, yes? Also, is there anyway i can change the output voltage? I'd like to lower it to around 4.7 volts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to capacitance_incarnate

    Take a look at the datasheet for the controller here (assuming it is the one Shabaz is referring to): http://www.farnell.com/datasheets/1723944.pdf?_ga=1.226316314.1698039299.1446112257

     

    If you look at Figure 15 on page 11 this is the circuit for a step down converter. In the circuit in this drawing R1 and R2 are the feedback resistors which are used to set the output voltage. The CII input feeds into a comparator inside the device, the other input being a 1.25V reference. The device will try and adjust the output such that the voltage on the CII input matches the reference voltage so if you want to change your output voltage then select values of R1 and R2 such that CII is at 1.25V for your desired output voltage.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • capacitance_incarnate
    0 capacitance_incarnate over 9 years ago in reply to rachaelp

    whoops. yea i meant  kohms. I found what I belive to be r1, its a .43 kohm and a 3.3 kohm in series, so if at all possible i want to try to only mess with r1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to capacitance_incarnate

    I hope it's not 1.2 ohm. Do you mean Kohm? You can do as you said to calculate the two resistor values. You might need to replace both to get the output you need as you will be restricted to standard values which can be easily obtained.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • capacitance_incarnate
    0 capacitance_incarnate over 9 years ago in reply to rachaelp

    ok so I've located r1. its 1.2Ω. Im still working on r2. once i find that, ill plug it into that equation that Texas instruments has, and I'll replace r1. and issues in doing that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • capacitance_incarnate
    0 capacitance_incarnate over 9 years ago in reply to rachaelp

    ok so I've located r1. its 1.2Ω. Im still working on r2. once i find that, ill plug it into that equation that Texas instruments has, and I'll replace r1. and issues in doing that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • capacitance_incarnate
    0 capacitance_incarnate over 9 years ago in reply to rachaelp

    whoops. yea i meant  kohms. I found what I belive to be r1, its a .43 kohm and a 3.3 kohm in series, so if at all possible i want to try to only mess with r1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to capacitance_incarnate

    I hope it's not 1.2 ohm. Do you mean Kohm? You can do as you said to calculate the two resistor values. You might need to replace both to get the output you need as you will be restricted to standard values which can be easily obtained.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer