• Products and Partners
    Products and Partners
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
Member's Forum Help: Am I crazy or is this chip dead?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 2 answers
  • Subscribers 633 subscribers
  • Views 2741 views
  • Users 0 members are here
Related

Help: Am I crazy or is this chip dead?

pathfider1998
pathfider1998 over 9 years ago

Hello people, I need some help with this issue.

(The chip that was supposed to be in the socket is SAB0600, from Siemens.)

I assembled the circuit "textbook style", EXACTLY replicating the circuit shown in the datasheet.

Circuit both assembled as-is on both breadboard and perfboard.

But it doesn't produce any sound when the switch is engaged (it should produce three chimes)

On breadboard, the circuit did make DC clicking noise when 100 microfarad capacitor was inserted backwards.

 

I do not have a multimeter yet that could reliably check the voltage, but using a trusted 5V power source and tuned analog multimeter, I verified that the power supply is outputting 9V, which is in-spec.

 

All chips bought from eBay, none of them came in static-safe packaging, not even the pink foam.

I had one sound chip that was not working and UM3482A Melody IC that didn't emit literally ANY noise even with all the components in the right place.

 

Am I crazy and killed all the chips, or am I stupid and I did something wrong, or was the chip faulty?

Any help is greatly appreciated, please tell me your opinions.

 

(Image mirrored to provide visual aid)

image

image

image

Sorry for the drunken soldering job, I still have problems with my hands.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Phil,

     

    It may be good to closely examine the IC, it could be fake. The SAB0600 could likely be obsolete (it is several decades old), so parts have a strong likelihood of being fake or reused parts. The same could apply to the other part you mention. I don't buy ICs from ebay for this reason.

    Fake and Re-used Electronic Parts and Components

     

    There is a photo of what the SAB 0600 should look like here:

    SAB 0600, Tube SAB0600; Röhre SAB 0600 ID61903, IC - Integra

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • pathfider1998
    0 pathfider1998 over 9 years ago in reply to shabaz

    It does have some questionable markings, as shown in the picture:

    image

    The chip has lasered on markings and has no date codes.

    The chip has what looks like sloppily written letter "F" on it, shown here:

    image

    The top stroke goes all over the place.

    image

    The legs have some suspicious scores on it too.

     

    Also, the other chip is COB with small circuit board, and UM3482A chip is shown below:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to pathfider1998

    Hi Phil,

     

    I can't be sure but it it likely a fake since there seem to be several suspicious things about it as you say.

     

    I'm not sure on the UM.. chip, that may be fine, a lot of these types of ICs were sold for COB applications for greetings cards etc., as well as the DIP package.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago in reply to pathfider1998

    Hi Phil,

     

    I can't be sure but it it likely a fake since there seem to be several suspicious things about it as you say.

     

    I'm not sure on the UM.. chip, that may be fine, a lot of these types of ICs were sold for COB applications for greetings cards etc., as well as the DIP package.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • pathfider1998
    0 pathfider1998 over 9 years ago in reply to shabaz

    I think that would work (as this chip outputs square wave anyway, only finely tuned to sound pleasing), but I now wonder how to make such thing happen.

     

    According to the datasheet, it should produce three harmonically tuned tones, one at a time, with the amplitude tapering off in around 1 to 2 seconds.

    (I have tons of 555 compatible chips lying around here, so it's okay to use as many as possible)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to pathfider1998

    Yes, I agree.

    A better option is the 555 (you've probably already used that), it is far more popular. It only generates one tone, but there are many circuits that can manipulate it in special ways, to generate (say) siren type sounds. You can combine two 555's to make even more interesting sounds.

    Check out this link for 50 ideas: 50 - 555 Circuits

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • pathfider1998
    0 pathfider1998 over 9 years ago in reply to shabaz

    I think I should ask for refund.