• Products and Partners
    Products and Partners
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
Member's Forum Bistable/latching solenoid valve control circuit. Please help!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 17 answers
  • Subscribers 634 subscribers
  • Views 9552 views
  • Users 0 members are here
  • change polarity
  • solenoid valve
Related

Bistable/latching solenoid valve control circuit. Please help!

sim.parkin
sim.parkin over 8 years ago

Hi there.

 

This is my first time posting and it's about my first electronics project since school image. So no need to say that i apologise if what I am asking is very simple but still I hope some one can help me.

 

So here's the situ... I want to be able to remotely switch a hose pipe on, but the thing is, the system is fixed into my vehicle so the whole thing has to be portable and run off batteries. I have a remote switch that at the press of a button (on the remote) can momentarily (or it can be set to self lock also) connect the battery to the solenoid valve and switch it on but the valve needs the polarity to be reversed and pulsed to switch it off again. For love nor money can I figure out a way of doing this? My head is in a whirl from all the h-bridge... dpdt relays... flipflops... etc.... every time I research something it seems I need something else to make it work. (if that makes sense) I am lost.

 

In short what I want to do is: Press the button on the remote control once and it turn the water flow on, and press it again and the water turn off. Basically its a momentary push button input that alternates between a +6v output and a -6v output. If that is possible.

 

I want to use this latching type relay because you can get low power ones of this type, but they also save battery power by only requiring a pulse of electricity to change state, rather than energising a coil for longer periods of time. Oh and I also want to avoid using microcontrollers if possible because I can't code.

 

Really hope someone out there can help. I also hope I remembered everything, if I missed something just let me know.

 

Thanks for reading.

 

 

Simon.

 

p.s. I found one other post like this with a guy with my exact problem but he gave up and used a non-latching type. image

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Hi Simon,

    I was back in the shop playing with this idea. I have changed the capacitors to 1000 uF and I have changed  R10 and R11 to 390 ohms. I hooked up a small 6 volt DC relay with a 100 ohm coil to see if it could be actuated. Here is the relay:

     

    image

     

    I put my analog ohmmeter across the NO contacts in parallel with my scope probes. This should give me about 3 volts on the scope when the contacts are open and zero volts when they close. Here is the scope image of the relays contacts.

     

    image

     

    As you can see the pulse was strong enough to close the relay contacts for 200 mSec. This relay is fairly easy to actuate so I am not sure that it is a good model for your solenoid. You will have to do some experimentation. I am calculating that we had a peak of about 70 mA to the relay coil and dropping from there as the capacitor charged.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sim.parkin
    0 sim.parkin over 8 years ago in reply to jw0752

    Hi John.

     

    This is very positive image. I am looking forward to having a tinker myself when the parts all arrive.

     

    Over and out for now.

     

     

    Simon.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sim.parkin
    0 sim.parkin over 8 years ago in reply to jw0752

    Hi John.

     

    This is very positive image. I am looking forward to having a tinker myself when the parts all arrive.

     

    Over and out for now.

     

     

    Simon.