• Products and Partners
    Products and Partners
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
Member's Forum I am looking for some help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 5 answers
  • Subscribers 632 subscribers
  • Views 2171 views
  • Users 0 members are here
Related

I am looking for some help

jlusco
jlusco over 8 years ago

I am newer to DIY electronics and I am working on a project. I have a project that I am building and I am stuck on this one part. I have an Adafruit Mono 2.5W Class D Audio Amplifier - PAM8302 and I want to bring teh Speaker out to another board that will have a Speaker and headphone jack on it. I want to wire it so when the headphones are plugged in the speaker is off and the sound comes through the headphones but when unplugged the sound comes out the speaker. Below is a basic mock up of what I want and I am just stuck on how to accomplish it.

I have tried to Google the answer but have had no luck. Orange dots are the thru hole solder points for each component any help will be appreciated.

 

 

MockUp

  • Sign in to reply
  • Cancel
  • ifish
    0 ifish over 8 years ago in reply to jlusco

    Hi Jacob,

     

    I think your misinterpreting that table as only GPIO0-27 are available by way of the 40 pin header, its a bit confusing but there are two ways of referencing the pins on the 40 pin header.  If you look at the schematic symbol you have posted each pin has a pin number and a description associated to it, pin 40 is in fact GPIO 21.

     

    image

    Which if we look at your table you have linked to isn't capable of being used for PWM

    image

     

    After looking the link you posted I get the feeling the guy used a USB audio device rather then the IO, but if you don't need two sets of triggers you could use GPIO 18 (pin 12) and wire you amplifier to this pin and ground.  You'll need to make some software modification, according to Step 7 of the projects setup (https://github.com/32teeth/Gameboy-Zero-Kickstarter/blob/master/INSTALL.md ) you have to edit the control setup anyways.  You'll want to free up gpio 18, so delete the following two lines from the config file

     

    A 18  # Left shoulder button

     

    OR

     

    change

    A 18  # Left shoulder button

    to

    A 21  # Left shoulder button

     

    but doing this will require you to lift the tact switch from being connected to GPIO_18 and run a wire from the tact switch to the GPIO_21.

     

    Hope this helps

    Chris

     

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jlusco
    0 jlusco over 8 years ago in reply to shabaz

    I thought about the schematic right after I asked. I took a look and now I am confused there are a hand full of pins not used but from the link you provided and looking at the GPIO Alt functions the only PWM pin free is 40. The designer has a PWN board as well that looks a lot like the circuit in the Pi Zero Adafruit page you provided. So Pins 3,5,7,8,16,27,28, and 40 are all free if I am reading it correctly but based on what I see here https://elinux.org/RPi_BCM2835_GPIOs only Pin 40 is PWM and it looks like you have to use a PWM1 and PWM0 pin am I understanding this correctly. I have also reached out to teh Designer to see how he suggests wiring his PWM board to the device.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to jlusco

    Hi Jacob,

    You originally stated that all GPIO pins were in use, is the question now if some are actually free?

    If so, it is really better if you check (good learning experience). The way to do it is to either find the circuit diagram of this gameboy project if you can, or visually inspect the circuit board if you have purchased it, to see which of the GPIO pins are in use. You could also use a multimeter to probe pins if you really don't wish to find the circuit diagram or if it is not available (if you don't have a multimeter, it is highly recommended).

    If the GPIO pins are just soldered but really are not going anywhere, then those GPIO pins are free. However, as you can see from the adafruit audio link sent earlier, the audio available on the GPIO pins are on _specific_ pins. You can't interchange. So you'd need to see if those specific pins are free and unused on that gameboy project board.

    And as mentioned, all you have is an audio amplifier. It can't directly connect to GPIO pins anyway, even if the GPIO pins are free. You need to also assemble the small circuit described on the adafruit page (a total of 4 resistors and 4 capacitors).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jlusco
    0 jlusco over 8 years ago in reply to shabaz

    So I am building a Gameboyzero (Link Below) and you mount the Raspberry Pi Zero W onto the PCB. I am not sure if I can use the GPIO PWM. Here is an image with the pins numbered maybe you can tell if I can do what I want to this way.

     

    image

     

     

     

     

     

    https://www.tindie.com/products/thirtytwoteeth/game-boy-zero-handheld-edition/

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jlusco
    0 jlusco over 8 years ago in reply to shabaz

    Thanks for your help you got me half way to what I am trying to do. image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jlusco
    0 jlusco over 8 years ago

    SoI guess the question is can I, and if I can, hook up a Adafruit Mono 2.5W Class D Audio Amplifier - PAM8302 to a raspberry pi zero without using the GPIO since in the project I am doing they are all used. If it can be done I would like to know how.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to jlusco

    Hi Jacob,

     

    It's not possible in the way you mention, without additional hardware (a USB sound card effectively). Otherwise GPIO can be used.

    If you don't want to use GPIO connections, then a USB sound card is needed.

    If you do eventually decide to use GPIO, see here for the circuit you need (in additional to the amplifier which you have already got).

    https://learn.adafruit.com/introducing-the-raspberry-pi-zero/audio-outputs

    Or you could connect a digital audio card to the GPIO pins. But it uses GPIO pins.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to jlusco

    Jacob,

     

    Well then you might need another person who is smarter than me for this one.  I have no experience with the Raspberry Pi, even though I recently purchased a Pi zero.  I can see how a GPIO could be used to generate an audio signal, but I am not sure if I have heard of the USB port being used in this way.

     

    Any ideas from the more experienced Raspberry Pi people here?

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jlusco
    0 jlusco over 8 years ago in reply to genebren

    I want to connect the amp to a raspberry pi zero without using the GPIO and being new to this I am not sure if I can do it with this or not so figured I would ask people who were smarter then me when it comes to this. I know you can wire a USB sound card to teh pads on the bottom of the Pi but not sure If I can do the same with amp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to jlusco

    Jacob,

     

    Not quite sure that I know what you are trying to do here. Best I can tell, Vin and Gnd are your power supply connections (2.5V to 5.5V), SD is used to turn the amp 'on' (Vin) or 'off' (gnd).  A+ and A- are your inputs (differential, if single-ended use A+ and tie A- to gnd.

    How this relates to the USB Test Pads is where I am getting lost.

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>